Projects
Need inspiration? Find it here! These tutorials feature special projects broken down into steps to illustrate how you can use various concepts, skills, and technologies to build awesome stuff.
How to Run a 5V Device On a 3.3V System With Qwiic
Power up your 5V I2C devices on the Qwiic system! This tutorial shows you how to use the SparkFun Qwiic 5V Boost to integrate power-hungry sensors like the SEN55 seamlessly.
Calibrating Your Odometry Sensor
In this tutorial, we will cover how to calibrate your Qwiic Optical Tracking Odometry Sensor (or "OTOS") with Arduino and Python Examples.
Moving Beyond the Ordinary With the Qwiic Alphanumeric Display
More than just numbers, more than just letters, with a little creative coding you can do teach your alphanumeric display lots of new tricks.
IMU Data to Motion: Tutorial for Translating Sensor Data into Real-World Movement
Sometimes we want to do more with our data than just watch the values roll by on a screen. In this tutorial, we'll take a look at one way we can translate that data to movement.
How to Play Multiple Buzzers at Once
This tutorial demonstrates the SparkFun Qwiic Buzzer's ability to control multiple buzzers simultaneously by playing a 3-part arrangement of a segment of the Super Mario Bros Theme!
GeoFence Treasure Hunt With Artemis Global Tracker
Follow along with an engineering student as he creates a distance-based game using the Artemis Global Tracker!
Connecting Thing Plus Matter to Google Nest Hub
Connect your Thing Plus Matter board to a Google Nest Hub, as well as the Google Home app, and set up as a light device!
Qwiic Kit for Raspberry Pi V2 Hookup Guide
Get started with the SGP40, BME280, VCNL4040, and microOLED via I2C using the Qwiic system and Python on a Raspberry Pi! Measure VOC Index, light, temperature, humidity, and pressure from the environment. Then display them on the microOLED, serial terminal, or the cloud with Cayenne!
Sending Sensor Data over LoRa
This tutorial will show you how setup a simple peer-to-peer connection to send and receive sensor data using LoRa.
MicroMod Qwiic Pro Kit Project Guide
The MicroMod Qwiic Pro Kit was designed to allow users to get started with Arduino without the need for soldering or a breadboard. We've included three inputs (a joystick, accelerometer, and proximity sensor) and one display that can be daisy chained to the MicroMod SAMD51 Processor Board.
Measuring Height with Atmospheric Pressure
Measure height using atmospheric pressure with your Qwiic MicroPressure breakout board!
Wireless Timing Project
Time for racing, let's make a wireless timing device using ESP32 wireless communication.
Monitor Sensor Data from Anywhere
Using WiFi to send sensor data from an ESP32 to a WiFi network and be able to read it from an IoT Dashboard from anywhere in the world.
The 970-HA-JOKES Payphone Project
A payphone turned into a bit of fun.
Qwiic Digital Desk Sign with MicroMod
Make a Qwiic-enabled digital desk sign with a MicroMod SAMD51 Processor Board's USB Host and a USB keyboard!
Sending Sensor Data Over WiFi
This tutorial will show you how setup a simple peer-to-peer connection to send and receive sensor data between two ESP32 WiFi boards.
How to Build a DIY GNSS Reference Station
Learn how to affix a GNSS antenna, use PPP to get its ECEF coordinates and then broadcast your own RTCM data over the internet and cellular using NTRIP to increase rover reception to 10km!
Setting up a Rover Base RTK System
Getting GNSS RTCM correction data from a base to a rover is easy with a serial telemetry radio! We'll show you how to get your high precision RTK GNSS system setup and running.
The ClockClock Project
Tell the time with this fantastic Alchitry project using clocks to make a clock!
Qwiic GPS Clock
What time is it? Time for you to... Qwiic-ly build a GPS clock and output it to a display! This project provides you with the current date and time using GPS satellites. Read the date and time as a digital or analog clock. Or even configure the clock for military, your time zone, or automatically adjust the time for daylight savings time!
Jetson Nano + Sphero RVR Mash-up (PART 2)
We took two of our biggest robotics partnerships from the previous year and shazamed them together into one robot to rule them all!
Qwiic Digital Indoor Thermometer
Qwiic-ly build a digital indoor thermometer to measure the ambient temperature of the room and display it using an OLED on an I2C bus!
Nintendo Switch Macro Recording on the Raspberry Pi
Learn how to record and playback controller 'macros' for your Nintendo Switch using a Raspberry Pi, SparkFun Top pHAT, and Joycontrol.
ESP32 OTA Updates over BLE from a React Web Application
Learn how to flash firmware Over-the-Air using a BLE React WebApp and ESP32
How to Make a Magic Mirror with Raspberry Pi
Need a great project for your Raspberry Pi 4 kit? Use it to create a command center to display the weather, clock, your calendar, or even a news feed!
RFID Beginners Tutorial
Make a remote work logger using an RFID reader and a GPS module. Scan a card and get ID, location, and time. All the perfect data to punch in and punch out from the middle of Nowhere!
Wireless Remote Weather Station with micro:bit
Monitor the weather without being exposed to it through wireless communication between two micro:bits using the radio blocks! This is useful if your weather station is installed in a location that is difficult to retrieve data from the OpenLog. We will also explore a few different ways to send and receive data.
Jetson Nano + Sphero RVR Mash-up (PART 1)
We took two of our biggest robotics partnerships from the previous year and shazamed them together into one robot to rule them all!
Raspberry Pi Safe Reboot and Shutdown Button
Safely reboot or shutdown your Raspberry Pi to avoid corrupting the microSD card using the built-in general purpose button on the Qwiic pHAT v2.0!
Temperature Sensor Comparison
A comparison of analog and digital temperature sensors. Which is better?
Secure DIY Garage Door Opener
Did you know that most garage doors are at risk of a roll jam attack? Here we make a DIY garage door remote-control system that is much more secure than most commercial-ready products using the latest in ECC cryptography.
Getting Started with the Autonomous Kit for the Sphero RVR
Want to get started in robotics? Look no further than the SparkFun autonomous kit for the Sphero RVR! Whether you purchased the Basic or Advanced kit, this tutorial will get you rolling...
Magnetic Levitation
This tutorial will show you how to build a magnetic levitation circuit using common parts.
Qwiic Pro Kit Project Guide
The Qwiic Pro Kit was designed to allow users to get started with Arduino without the need for soldering or a breadboard. We've included three inputs (a joystick, accelerometer, and proximity sensor) and one display that can be daisy chained to the RedBoard Turbo (SAMD21) Development Board.
Wireless Controlled Wearable EL Wire Dance Suit
In this tutorial, we will build an EL wire dance suit that can be controlled by a wireless glove controller!
Fuse Breakout Board Hookup Guide
Protect your project by adding a fuse in your circuit to save it from molten destruction.
GPS Geo-Mapping at the Push of a Button
Let's ramp up our GPS tracking skills with KML files and Google Earth. We'll make a tracker that logs location and allows us to visualize our steps with Google Earth.
ESP32 Relay Web Server
The goal of this project is to have a website hosted on an ESP32 that controls any relay controlled device connected to a local network and keeps a dynamically updated state of those devices.
EL Wire Pants
In this tutorial, we will sew standard electroluminescent (EL) wire to a pair of pants.
Modifying Your EL Wire Inverter
In this tutorial, we will modify the 12V EL wire inverter to power the EL Sequencer/EL Escudo Dos off a single power supply.
Using Home Assistant to Expand Your Home Automations
An introduction to Home Assistant, an open source home automation hub.
Displaying Your Coordinates with a GPS Module
This Arduino tutorial will teach you how to pinpoint and display your GPS coordinates with a press of a button using hardware from our Qwiic Connect System (I2C).
Wireless Gesture Controlled Robot
Control the RedBot wirelessly based on the movement of your hand using an accelerometer, Arduino, and XBees!
Keyboard Shortcut, Qwiic Keypad
A simple project using the Qwiic Keypad and the RedBoard Turbo to create your own custom hotkey-pad.
Wireless Glove Controller
Build a wireless glove controller with Arduinos to trigger an LED using XBees!
LED Gumball Machine
Hacking gumball machines to make the world a happier, blinkier place.
Build a Qwiic Jukebox that is Toddler Approved!
Follow this tutorial to build your own custom jukebox. Note, this is designed simple and tough for use primarily with toddlers. It's also a great introduction to SparkFun's Qwiic products!
Wireless RC Robot with Arduino and XBees
In this tutorial, we will expand on the SIK for RedBot to control the robot wirelessly with XBee radios! We'll explore a different microcontroller and wirelessly control the RedBot at a distance.
Computer Vision and Projection Mapping in Python
Use computer vision to detect faces and project images on top of them.
Motion Controlled Wearable LED Dance Harness
Control LEDs based on your movement using an accelerometer! Make your LEDs breathe by fading in and out when laying on the floor, turn off the LEDs when moving to your side, or make the LEDs blink in a headstand!
Wireless Remote Control with micro:bit
In this tutorial, we will utilize the MakeCode radio blocks to have the one micro:bit transmit a signal to a receiving micro:bit on the same channel. Eventually, we will control a micro:bot wirelessly using parts from the arcade:kit!
3D Printed Illuminated Wand Prop
In this tutorial, we will learn about how to create a theatrical prop for a performance by 3D printing a wand and adding an LED.
How to Make a Custom EL Wire Extension Cable
In this tutorial, we will make a custom EL Wire extension cable as an alternative to splicing wire.
EL Wire Hoodie
In this tutorial, we will sew standard electroluminescent (EL) wire to a hoodie.
Python GUI Guide: Introduction to Tkinter
Tkinter is the standard graphical user interface package that comes with Python. This tutorial will show you how to create basic windowed applications as well as complete full-screen dashboard examples complete with live graph updates from matplotlib.
Graph Sensor Data with Python and Matplotlib
Use matplotlib to create a real-time plot of temperature data collected from a TMP102 sensor connected to a Raspberry Pi.
Light Up Your 3D Printer's Bed
Having issues viewing your print in a dark lit room? In this tutorial, we will be using LED strips to light up a print bed's area on a LulzBot 3D printer!
IoT Power Relay
Using the ESP32 to make a web-configured timed relay.
IoT Weight Logging Scale
This tutorial will show you how to make a scale that logs your weight to a custom website on the Internet. The principles can be extrapolated to any type of data.
WiFi Controlled Robot
This tutorial will show you how to make a robot that streams a webcam to a custom website that can be remotely controlled.
Headless Raspberry Pi Setup
Configure a Raspberry Pi without a keyboard, mouse, or monitor.
Setting up a Raspberry Pi 3 as an Access Point
This guide will show you how to configure a Raspberry Pi as an access point and connect it to your local Ethernet network to share Internet to other WiFi devices.
Interactive 3D Printed LED Diamond Prop
In this tutorial, we will learn about how to create an interactive theatrical prop for a performance by 3D printing a translucent diamond prop using a non-addressable RGB LED strip and AT42QT1011 capacitive touch sensing.
Using Artnet DMX and the ESP32 to Drive Pixels
In this tutorial, we'll find out how to use Resolume Arena, a popular video jockey software, to control custom-made ArtNet DMX fixtures.
Craft a Holiday Greeting with Love to Code
Craft your own paper circuit holiday greeting using the LEDs, a Chibi Chip, Love to Code!
Tech Prank: Hardware Mouse Jiggler
Create an innocuous-looking USB stick with an Arduino Pro Micro and a 3D printed case that moves your mouse pointer randomly every few seconds. Sure to anger your coworkers and friends!
Raspberry Pi Zero Helmet Impact Force Monitor
How much impact can the human body handle? This tutorial will teach you how to build your very own impact force monitor using a helmet, Raspberry Pi Zero, and accelerometer!
MIDI BLE Tutorial
Developing a bidirectional MIDI-BLE link with the nRF52832 Breakout.
Prototype Wearable LED Dance Harness
A project tutorial to add an extra effect for dancers performing a choreographed piece. The harness can be added quickly under a costume.
DIY Heated Earmuffs
Embedded with heating pads and four Neopixel rings, these earmuffs do more than your average winter accessory to keep you warm while still looking good.
Wireless Audio Bluetooth Adapter w/ BC127
Build a custom wireless audio Bluetooth adapter using BlueCreation's BC127 and add it to your old speaker system!
Light-Seeking Robot
We use parts from the SparkFun Inventor's Kit v4.0 to create a light-seeking robot that mimics the behavior of single-celled organisms.
Clap On Lamp
Modify a simple desk lamp to respond to a double clap (or other sharp noise) using parts from the SparkFun Inventor's Kit v4.0.
Vibe-O-Matic 3000
We attempt to emulate a car seat to ease a baby to sleep.
Endless Runner Game
We make a simple side-scrolling endless runner game using parts from the SparkFun Inventor's Kit v4.0.
LilyPad Safety Scarf
This scarf is embedded with a ribbon of LEDs that illuminate when it gets dark out, making yourself more visible to vehicle and other pedestrians.
Lumenati Alien Garden
Use Lumenati LED boards to add glow to your own alien garden.
Night Sky Halloween Costume
Make a beautiful night sky costume using the LilyPad LEDs and the LilyTiny.
DIY Light-Up Shoes
This tutorial provides everything you need to know to make your own light up high top sneakers!
LED Crystal Goddess Crown
Follow this tutorial to make your own Crystal Goddess Crown with LEDs!
Twinkle Zodiac Constellation
Create a quick and easy piece of e-textile art based on a Zodiac sign using a LilyTiny, LilyPad LEDs, battery holder, conductive thread, and coin cell battery.
Fairy LED Bracelet
Light up the world - and your wrist - with this quick and easy rechargeable firefly LED bracelet.
LED PomPom Headbands
Follow this tutorial to make your own light up PomPom headband! Try the beginner version if you are new to electronics or the advanced version if you have some more experience!
Marquee Party Bag
This tutorial provides everything you need to know to make your own Marquee Party Bag!
Spectacle Example: Super Mario Bros. Diorama
A study in building an animated diorama (with sound!) using Spectacle electronics.
Building a Safe Cracking Robot
How to crack an unknown safe in under an hour.
Hack Your Roshamglo Badge
Learn how to customize and program your Roshamglo badge.
Roshamglo Project: TV-B-Gone
Turn your Roshamglo board into a (nearly) universal TV power button.
Bark Back Interactive Pet Monitor
Monitor and interact with pets through this dog bark detector project based on the Raspberry Pi!
Light-Up Plush
Craft a light-up plush with LilyPad LEDs controlled by pressing a button and sliding a switch in the creature's hands.
Illuminated Mask
Use LilyPad LEDs, a switched battery holder, and coin cell battery to make a fun light up mask for your next costume party.
Glowing Pin
Create a quick and easy piece of e-textile art using a LilyPad LED, battery holder, conductive thread, and coin cell battery.
Night-Light Pennant with LilyMini ProtoSnap
Use the pre-programmed LilyMini ProtoSnap to make an interactive pennant that reacts to ambient light levels.
Logging Data to Google Sheets with the Tessel 2
This project covers how to log data to Google Sheets two ways: using IFTTT with a web connection or a USB pen drive and "sneakernet" without.
Building an Autonomous Vehicle: The Batmobile
Documenting a six-month project to race autonomous Power Wheels at the SparkFun Autonomous Vehicle Competition (AVC) in 2016.
Vox Imperium: Stormtrooper Voice Changer
Add some flair to your Imperial uniform by changing your voice using a Teensy 3.2 and Prop Shield.
MicroView Digital Compass
Build a portable digital compass using the SparkFun MicroView and the MAG3110 Magnetometer Breakout.
Sunrise Machine with the Tessel 2
Are you to sleepy to enjoy a sunrise on a brisk morning? Yeah...us too! No worries, with a Webcam, a Tessel 2 and a bit of code you can sleep in and catch the sunrise at your leisure with the Sunrise Machine.
Environmental Monitoring with the Tessel 2
Build an air-conditioner monitoring device to collect environment information and store it in the cloud.
ReconBot with the Tessel 2
Build a robot with the Tessel 2 that you can control from a browser on your phone or laptop.
IoT Industrial Scale
What does a baby elephant weigh? How much impact force does a jump have? Answer these questions and more by building your very own IoT industrial scale using the SparkFun OpenScale.
TB6612FNG Hookup Guide
Basic hookup guide for the TB6612FNG H-bridge motor driver to get your robot to start moving!
Proto Pedal Example: Analog Equalizer Project
Building a gyrator-based analog equalizer using the Proto Pedal.
Proto Pedal Example: Programmable Digital Pedal
Building a pedal around the Teensy 3.2 and Teensy Audio shield. Changing the effect in the pedal is as easy as uploading a new sketch!
Pokémon Go Patches with EL Panels
Add a cloth stencil over EL panels to create glowing logos and designs.
OpenScale Applications and Hookup Guide
OpenScale allows you to have a permanent scale for industrial and biological applications. Learn how to use the OpenScale board to read and configure load cells.
Electret Mic Breakout Board Hookup Guide
An introduction to working with the Electret Mic Breakout Board.
Hazardous Gas Monitor
Build a portable gas monitor to check for dangerous levels of hazardous gases.
Photon Remote Water Level Sensor
Learn how to build a remote water level sensor for a water storage tank and how to automate a pump based off the readings!
Interactive LED Music Visualizer
Use an Arduino and the SparkFun Sound Detector to create visualizations on Addressable RGB LED strips.
How to Build a Remote Kill Switch
Learn how to build a wireless controller to kill power when things go... sentient.
GPS Differential Vector Pointer
Use GPS to have two objects, a base and a target, point towards one another. This can be used to aim a directional antenna (or in the case of this project, a laser) from one object to the other object at a distance that is only limited by your ability to provide the base station with the target's GPS location.
Sparcade: Edison as a Web Server for Browser Games
Turn the Intel® Edison into an access point that serves a simple browser-based game. High scores from the game are displayed on a character LCD.
Measuring Internal Resistance of Batteries
Classroom STEM activity that has students build a battery from a lemon, measure the open and closed circuit voltages, and determine the battery's internal resistance.
SIK Keyboard Instrument
We can use the parts and concepts in the SparkFun Invetor's Kit to make a primitive keyboard instrument.
Paper Circuit Pin
This quick craft project shows you how to create a circuit using copper tape instead of wire to light up an LED and make a wearable piece of e-craft art.
Blynk Board Washer/Dryer Alarm
How to configure the Blynk Board and app to notify you when your washer or dryer is done shaking.
Boss Alarm
Build a Boss Alarm that alerts you of anyone walking into your office and automatically changes your computer screen.
Blynk Board Bridge Widget Demo
A Blynk project that demonstrates how to use the Bridge widget to get two (or more) Blynk Boards to communicate.
Blynk Board Project Guide
A series of Blynk projects you can set up on the Blynk Board without ever re-programming it.
ESP8266 Powered Propane Poofer
Learn how Nick Poole built a WiFi controlled fire-cannon using the ESP8266 Thing Dev Board!
LED Cloud-Connected Cloud
Make an RGB colored cloud light! You can also control it from your phone, or hook up to the weather!
BadgerHack: Sensor Add-On Kit
Turn your Badger or Redstick into a temperature and soil moisture sensing display with the BadgerHack Sensor Add-On Kit
BadgerHack: Synth Add-On Kit
Make a tiny synth with BadgerStick.
BadgerHack: Gaming Add-On Kit
Make a Breakout clone with the BadgerHack Gaming Add-On Kit.
Interactive Smart Mirror
Build a smart mirror that displays weather data using the Intel® Edison.
Using an LCD on the Edison
How to connect an LCD controlled by an ILI9341 driver to the Intel® Edison.
Electronic E-craft Terrarium
A guest tutorial on an Electronic Terrarium from the Performative Sculpture class of Parsons DT.
Sound Reactive EL Wire Costume
Learn how to make your EL wire costumes sound reactive in this project tutorial.
Shapeoko Coaster Project
A step-by-step guide to cutting and engraving a coaster with the Shapeoko.
EL Wire Light-Up Dog Harness
Learn how to create a light-up dog harness using EL wire for when you need to take your four-legged friend for a walk in the dark.
Light Up Pennant with E-Textiles
Show your school spirit, geek pride, or fandom with a light up pennant using the LilyTwinkle or LilyPad Arduino.
LED Butterfly Pop Up Card
Craft an illuminated butterfly pop up card with copper tape, two LEDs, and a battery.
LED Robot Pop Up Card
Craft a paper circuit pop up card with a cycling RGB LED, battery, and copper tape.
Making Music with the FreeSoC2
Create a synth keyboard with the FreeSoC2 from SparkFun.
Planning a Wearable Electronics Project
Tips and tricks for brainstorming and creating a wearables project.
Adding a Timed Button to a Project
This tutorial will walk you through making a timed power controller for interactive projects. You will learn how to add an on button that will provide power to your project for an amount of time and then turn off again.
Building Large LED Installations
Learn what it takes to build large LED installations from planning to power requirements to execution.
Large Digit Driver Hookup Guide
Getting started guide for the Large Digit display driver board. This tutorial explains how to solder the module (backpack) onto the back of the large 7-segment LED display and run example code from an Arduino.
Origami Paper Circuits
A quick tutorial to get you started in the world of light up origami flowers.
Sound Page Guide
How to use the Lilypad MP3 Player and some Bare Conductive Paint to make a fandom silhouette sound trigger page.
Hackers in Residence: The Sound Visualizer Pt. 2
An addition to a previous project, this time using a PC and a custom Java app to create your own music visualizer using a RGB LED matrix.
Bare Conductive Musical Painting
Learn how to make a musical painting using the Bare Conductive Touch Board and Conductive Paint.
Light Up Silk Flower Corsage
Combine a silk flower with a built-in RGB LED and some LilyPad Switches to create a customizable accessory.
Hackers in Residence: The Sound Visualizer
A fun project that uses a Raspberry Pi and a custom Java app to create your own sound visualizer using a RGB LED matrix.
LilyTiny Plush Monster
Craft a stuffed monster while exploring the LilyTiny preprogrammed microcontroller. This is a project based on the Plush Monster Activity created at MIT's High-Low Tech Lab by Emily Lovell, Jie Qi, and Natalie Freed.
Hacker in Residence: The Harmonic Skew Zoetrope
Check out Hacker in Residence, Jesse's awesome Harmonic Skew Zoetrope in this project tutorial.
Light-Up Valentine Cards
Light up your love with paper circuits - no soldering required!
Alphanumeric GPS Wall Clock
This is a GPS controlled clock - a clock you truly never have to set! Using GPS and some formulas, we figure out what day of the week and if we are in or out of daylight savings time.
RedBoard Santa Trap
A fun holiday project to try for anyone looking to catch Santa on Christmas!
Actobotics Basic Differential Platform
Get started with Actobotics with this simple vehicle. Then expand and customize it for your own evil robot empire.
21st Century Fashion Kit: Inflation
Learn how to use a blower and thin sheet plastic to create designs that change shape and volume!
Let It Glow Holiday Cards
Craft a glowing card for friends and family this holiday season with paper circuits - no soldering required!
21st Century Fashion Kit: Electrochromatic Circuits
Diana Eng walks you through a magically appearing design made with an thermochromatic pigment.
Cackling Apple Head Witch
Make your own cackling apple head witch to scare all of the trick or treaters this Halloween!
Humidity-sensing LED Flower
How about that humidity? This tutorial shows how to add sensing capability to the 21st Century Fashion Kit's RGB flower project.
Hackers in Residence - Sound and Motion Reactivity for Wearables
How to consciously wear light-up and and sound reactive clothing.
Twinkling Trick or Treat Bag
Make a light up goodie bag with conductive thread, LEDs, and the LilyTwinkle!
Hacking Your Maker Faire Badge
How to hook-up, program, and modify your Maker Faire Badge for electronic fun.
Hackers in Residence - Cosmic Ray Detector
Learn how to detect cosmic rays with this simple and cheap detector, built by Hacker in Residence Pete Marchetto.
RGB Panel Jumbotron
This tutorial will show you how to combine a webcam, a 32x32 RGB LED panel, and a Teensy 3.1 to stream video from the webcam, pixelate it, and display it on the LED panel - LIVE.
Hackers in Residence - The ElectricBone
Drum machines and keyboards have been the standard for making digital music, but how do you make electronic music if you're trained to play the trombone? One of our Hackers in Residence, Carlos Mello, took it upon himself to find a solution to that very question.
Soil moisture-sensing by hacking a solar light
How to take a solar powered pathway light from a hardware store and make it into a crude soil moisture sensor.
Light-Up Father's Day Card
Light up your dad's day with this electronic pop-up card!
Are You Okay? Widget
Use an Electric Imp and accelerometer to create an "Are You OK" widget. A cozy piece of technology your friend or loved one can nudge to let you know they're OK from half-a-world away.
Customizing LilyPad LED Colors
A short guide to creating a rainbow of new LilyPad LED colors at home!
ELasto-Nightlight
Fear the dark no longer with this ELastoLite nightlight.
Interactive Hanging LED Array
Learn how we converted 72 lightbulbs into an interactive LED array for our conference room.
Arduino Wireless Communication via the Electric Imp
How to communicate between an Electric Imp and Arduino using serial.
MYST Linking Book
Create your own Linking Book from the classic computer game, MYST
HID Control of a Web Page
Learn how to move a slider on a webpage and make a motor spin. We connect HTML and HID to read sensors and interface with the physical world.
Build an Auduino Step Sequencer
Make a Step Sequencer using an Arduino, the Auduino firmware, and a handful of hardware.
Hackers in Residence - Hacking MindWave Mobile
Review, teardown, and hacking tutorial for the MindWave Mobile, a $99 commercial grade EEG sensor.
Wireless Arduino Programming with Electric Imp
Reprogram your Arduino from anywhere in the world using the Tomatoless Boots wireless bootloader with the Electric Imp.
Simon Splosion Wireless
This is a tutorial demonstrating one of many techniques to "hack" the Simon Says. We will highlight the technique to take your Simon Says Wireless.
Das Blinken Top Hat
A top hat decked out with LED strips makes for a heck of a wedding gift.
Reaction Timer
Demonstrate mental chronometry with this simple reaction timer!
Recreating Classic Electronics Kits
100-in-1? 500-in-1? It's up to you when you build your own Science Fair style experiment board!
pcDuino Crowdsource Kiosk
Getting People to do your job for you (badly) with some chocolate and a pcDuino!
Vernier Photogate
Vernier Photogate Timer -- using the Serial Enabled LCD Kit.
Quick Illuminated Boxes
A quick tutorial to show you how to add LEDs to gift or holiday bags or boxes.
Raspberry Pi Twitter Monitor
How to use a Raspberry Pi to monitor Twitter for hashtags and blink an LED.
Hackers In Residence - The Tethered Quad
Our first-ever "Hackers in Residence" Tara Tiger Brown and Sean Bonner created a quadcopter that stays tethered to the ground. Here's how they did it!
My Drunk Kitchen Apron
A fun project that uses the LilyPad MP3 trigger. This apron will dispense helpful kitchen advice and humor from the host of My Drunk Kitchen, Hannah Harto!
Dungeons and Dragons Dice Gauntlet
A playful, geeky tutorial for a leather bracer that uses a LilyPad Arduino, LilyPad accelerometer, and seven segment display to roll virtual 4, 6, 8, 10, 12, 20, and 100 side dice for gaming.
Mario the Magician's Magical Lapel Flower
A guest tutorial from the astonishingly talented Mario the Magician showing how to put together your own servo-controlled lapel flower.
Creating a Humidor Control Box
Because some of our boards need to be re-humidified after reflow, we decided to make our own humidor. This tutorial will focus on how to model a project in 3D and then fabricate it using a CNC routing machine.
The Uncertain 7-Cube
The Uncertain 7-Cube is a non-committal, less-than-helpful, but also entirely honest fortune teller. Simply ask it a yes or no question, give it a nudge, and the 7-Cube will dutifully inform you that it doesn’t have all the facts and doesn’t feel comfortable making a guess.
Soft Circuits: LED Feelings Pizza
Here we will learn how to say how you feel with pizza. Electric pizza.
Heating Pad Hand Warmer Blanket
DIY Project Idea: Create a custom hand warmer blanket using heating pads.
MP3 Player Shield Music Box
Music Box Project based on the Dr. Who TARDIS.
Heartbeat Straight Jacket
An EL project that displays one person's heartbeat on another person's costume.