Using an LCD on the Edison

≡ Pages
Contributors: Shawn Hymel

Introduction

One of the requests we often hear for the Intel® Edison is the ability to use an LCD. While the Edison does not have a display driver, we can use the onboard SPI port to control simple LCDs.

ReplaceMeOpen

ReplaceMeClose

For this particular tutorial, we will rely on a recent version of Intel's UPM library. In it is a module capable of calling the necessary functions to control an ILI9341 driver chip, which is a popular controller for 320x240, 2"-3" LCDs.

NOTE: The UPM driver used in this tutorial is a library that works in user space. That means we can make function calls to draw simple shapes and text on the LCD. Because it is not in kernel space we cannot do things like run X on it.
ALSO NOTE: The SPI driver on the Edison is currently quite slow. A full-screen refresh takes around 20 seconds, so don't expect any video or fast cycling images. If the SPI driver is updated in a future Edison image, you can ignore this message.

Required Materials

You will need an LCD with a ILI9341 controller. These can be found from a variety of sources, such as PJRC and Adafruit. Additionally, you will need the following:

NOTE: If you are using the LCD from PJRC, you will also need a 100Ω resistor.

Suggested Readings

Before getting started, you may find some of the tutorials below helpful.

Hardware Hookup

Build the Block Stack

Using the Edison Hardware Pack, attach the Edison to the Base Block.

Attaching the Edison to the Base Block

Attach the Base Block to the Pi Block. Secure them in place using screws and standoffs.

Attach the Pi Block

Connect the LCD

We need to connect the LCD to the Edison via the Pi Block. Solder headers to the LCD (if necessary), and follow the Fritzing diagram below to connect it to the Edison.

NOTE: If you are using an LCD from PJRC, a 100Ω resistor is needed between the LED and VCC pins on the LCD.
NOTE: If you are using an LCD from Adafruit, you will need to solder the jumpers IM1, IM2, IM3 on the back of the board in order to use SPI.

Connect the LCD to the Edison

Click on the image to view a larger version

Install the ILI9341 Module

NOTE: At the time of this writing, the ILI9341 module is included in UPM but not as part of the Edison image. As a result, we will need to build UPM from source. If, in the future, it is included in the default Edison image, you can skip this section.

Flash and Configure the Edison

If this is your first time using the Edison, it is recommended that you update to the latest firmware and connect to WiFi.

Build MRAA

MRAA is Intel's set of libraries used to control the low-level hardware. Because UPM relies on MRAA, we need to install it first.

Connect to the Edison over Serial or SSH. Once logged in, enter the following commands to download MRAA:

wget https://github.com/intel-iot-devkit/mraa/archive/master.zip
unzip master.zip
mv mraa-master mraa

Then, build MRAA with:

cd mraa
mkdir build
cd build
cmake ..
make

Install the newly built libraries, and update the pkg-config path, which is needed by UPM.

make install
export PKG_CONFIG_PATH=$PKG_CONFIG_PATH:/usr/local/lib/pkgconfig

Build ili9341 in UPM

Next, we need to download the latest version of UPM and install the ili9341 module. Download UPM with:

cd ~
rm master.zip
wget https://github.com/intel-iot-devkit/upm/archive/master.zip
unzip master.zip
mv upm-master upm

Prepare to build:

cd upm
mkdir build
cd build
cmake ..

Build and install the ili9341 module:

make ili9341
cd src/ili9341
make install

And that's it! We'll use this installed library to make an example program that draws some basic shapes on the LCD. Choose whether you want to write the example program in C++, JavaScript, or Python, and skip to that section below.

NOTE: Each of the C++, JavaScript, and Python examples can be found in ~/upm/examples.

Example Program: C++

If you are used to writing C/C++, then this is the way to go. Go back to your home directory and create a C++ file:

cd ~
vi ili9341.cpp

Press 'i' to type text. Copy and paste the code below into vi (if you are using an SSH client like PuTTY, simply right-click in the window to paste).

language:cpp
#include <unistd.h>

#include "ili9341.h"

int main(int argc, char **argv) {

    // Pins (Edison)
    // CS_LCD   GP44 (MRAA 31)
    // CS_SD    GP43 (MRAA 38) unused
    // DC       GP12 (MRAA 20)
    // RESEST   GP13 (MRAA 14)
    upm::ILI9341 * lcd = new upm::ILI9341(31, 38, 20, 14);

    // Fill the screen with a solid color
    lcd->fillScreen(lcd->color565(0, 40, 16));

    // Draw some shapes
    lcd->drawFastVLine(10, 10, 100, ILI9341_RED);
    lcd->drawFastHLine(20, 10, 50, ILI9341_CYAN);
    lcd->drawLine(160, 30, 200, 60, ILI9341_GREEN);
    lcd->fillRect(20, 30, 75, 60, ILI9341_ORANGE);
    lcd->drawCircle(70, 50, 20, ILI9341_PURPLE);
    lcd->fillCircle(120, 50, 20, ILI9341_PURPLE);
    lcd->drawTriangle(50, 100, 10, 140, 90, 140, ILI9341_YELLOW);
    lcd->fillTriangle(150, 100, 110, 140, 190, 140, ILI9341_YELLOW);
    lcd->drawRoundRect(20, 150, 50, 30, 10, ILI9341_RED);
    lcd->drawRoundRect(130, 150, 50, 30, 10, ILI9341_RED);
    lcd->fillRoundRect(75, 150, 50, 30, 10, ILI9341_RED);

    // Write some text
    lcd->setCursor(0, 200);
    lcd->setTextColor(ILI9341_LIGHTGREY);
    lcd->setTextWrap(true);
    lcd->setTextSize(1);
    lcd->print("Text 1\n");
    lcd->setTextSize(2);
    lcd->print("Text 2\n");
    lcd->setTextSize(3);
    lcd->print("Text 3\n");
    lcd->setTextSize(4);
    lcd->print("Text 4\n");

    // Test screen rotation
    for(int r = 0; r < 4; r++) {
        lcd->setRotation(r);
        lcd->fillRect(0, 0, 5, 5, ILI9341_WHITE);
        sleep(1);
    }

    // Invert colors, wait, then revert back
    lcd->invertDisplay(true);
    sleep(2);
    lcd->invertDisplay(false);

    // Don't forget to free up that memory!
    delete lcd;

    return 0;
}

Save and exit ('esc', type ':wq', and press 'enter'). Append the UPM modules location to our linker PATH, and compile the program:

export LD_LIBRARY_PATH=$LD_LIBRARY_PATH:/usr/local/lib
g++ ili9341.cpp -o ili9341 -lupm-ili9341 -lmraa -I/usr/local/include/upm

Run the program:

./ili9341

The screen will fill with a color and draw some basic shapes!

Example Program: JavaScript

If you would like to write a Node.JS program that uses the ILI9341 module, you can do that, too!

cd ~
vi ili9341.js

Press ‘i’ to type text. Copy and paste the code below into vi (if you are using an SSH client like PuTTY, simply right-click in the window to paste).

language:javascript
var ili9341 = require('jsupm_ili9341');

// Pins (Edison)
// CS_LCD   GP44 (MRAA 31)
// CS_SD    GP43 (MRAA 38) unused
// DC       GP12 (MRAA 20)
// RESEST   GP13 (MRAA 14)
var lcd = new ili9341.ILI9341(31, 38, 20, 14);

// Fill the screen with a solid color
lcd.fillScreen(lcd.color565(0, 40, 16));

// Draw some shapes
lcd.drawFastVLine(10, 10, 100, ili9341.ILI9341_RED);
lcd.drawFastHLine(20, 10, 50, ili9341.ILI9341_CYAN);
lcd.drawLine(160, 30, 200, 60, ili9341.ILI9341_GREEN);
lcd.fillRect(20, 30, 75, 60, ili9341.ILI9341_ORANGE);
lcd.drawCircle(70, 50, 20, ili9341.ILI9341_PURPLE);
lcd.fillCircle(120, 50, 20, ili9341.ILI9341_PURPLE);
lcd.drawTriangle(50, 100, 10, 140, 90, 140, ili9341.ILI9341_YELLOW);
lcd.fillTriangle(150, 100, 110, 140, 190, 140, ili9341.ILI9341_YELLOW);
lcd.drawRoundRect(20, 150, 50, 30, 10, ili9341.ILI9341_RED);
lcd.drawRoundRect(130, 150, 50, 30, 10, ili9341.ILI9341_RED);
lcd.fillRoundRect(75, 150, 50, 30, 10, ili9341.ILI9341_RED);

// Write some text
lcd.setCursor(0, 200);
lcd.setTextColor(ili9341.ILI9341_LIGHTGREY);
lcd.setTextWrap(true);
lcd.setTextSize(1);
lcd.print("Text 1\n");
lcd.setTextSize(2);
lcd.print("Text 2\n");
lcd.setTextSize(3);
lcd.print("Text 3\n");
lcd.setTextSize(4);
lcd.print("Text 4\n");

// Test screen rotation
function rotateScreen(r) {
    lcd.setRotation(r);
    lcd.fillRect(0, 0, 5, 5, ili9341.ILI9341_WHITE);
    if (r < 4) {
        r++;
        setTimeout(function() { rotateScreen(r); }, 1000);
    }
}
rotateScreen(0);

// Invert colors, wait, then revert back
setTimeout(function() { lcd.invertDisplay(true); }, 4000);
setTimeout(function() { lcd.invertDisplay(false); }, 6000);

Save and exit (‘esc’, type ‘:wq’, and press ‘enter’). Append the UPM modules location to our Node PATH:

export NODE_PATH=$NODE_PATH:/usr/local/lib/node_modules/

Run the program:

node ili9341.js

The screen will fill with a color and draw some basic shapes!

Example Program: Python

We can also use Python to make calls to the UPM module. Create a Python script:

cd ~
vi ili9341.py

Press ‘i’ to type text. Copy and paste the code below into vi (if you are using an SSH client like PuTTY, simply right-click in the window to paste).

language:python
#!/usr/bin/python

import time
import pyupm_ili9341 as ili9341

# Pins (Edison)
# CS_LCD   GP44 (MRAA 31)
# CS_SD    GP43 (MRAA 38) unused
# DC       GP12 (MRAA 20)
# RESEST   GP13 (MRAA 14)
lcd = ili9341.ILI9341(31, 38, 20, 14)

# Fill the screen with a solid color
lcd.fillScreen(lcd.color565(0, 40, 16))

# Draw some shapes
lcd.drawFastVLine(10, 10, 100, ili9341.ILI9341_RED)
lcd.drawFastHLine(20, 10, 50, ili9341.ILI9341_CYAN)
lcd.drawLine(160, 30, 200, 60, ili9341.ILI9341_GREEN)
lcd.fillRect(20, 30, 75, 60, ili9341.ILI9341_ORANGE)
lcd.drawCircle(70, 50, 20, ili9341.ILI9341_PURPLE)
lcd.fillCircle(120, 50, 20, ili9341.ILI9341_PURPLE)
lcd.drawTriangle(50, 100, 10, 140, 90, 140, ili9341.ILI9341_YELLOW)
lcd.fillTriangle(150, 100, 110, 140, 190, 140, ili9341.ILI9341_YELLOW)
lcd.drawRoundRect(20, 150, 50, 30, 10, ili9341.ILI9341_RED)
lcd.drawRoundRect(130, 150, 50, 30, 10, ili9341.ILI9341_RED)
lcd.fillRoundRect(75, 150, 50, 30, 10, ili9341.ILI9341_RED)

# Write some text
lcd.setCursor(0, 200)
lcd.setTextColor(ili9341.ILI9341_LIGHTGREY)
lcd.setTextWrap(True)
lcd.setTextSize(1)
lcd._print("Text 1\n")
lcd.setTextSize(2)
lcd._print("Text 2\n")
lcd.setTextSize(3)
lcd._print("Text 3\n")
lcd.setTextSize(4)
lcd._print("Text 4\n")

# Test screen rotation
for r in range(0, 4):
    lcd.setRotation(r)
    lcd.fillRect(0, 0, 5, 5, ili9341.ILI9341_WHITE)
    time.sleep(1)

# Invert colors, wait, then revert back
lcd.invertDisplay(True)
time.sleep(2)
lcd.invertDisplay(False)

# Don't forget to free up that memory!
del lcd

Save and exit (‘esc’, type ‘:wq’, and press ‘enter’). Append the UPM modules location to our Python PATH:

export PYTHONPATH=$PYTHONPATH:/usr/local/lib/python2.7/site-packages/

Run the script with:

python ili9341.py

The screen will fill with a color and draw some basic shapes!

Resources and Going Further

If you successfully ran one of the example programs, your LCD should look like this:

Edison with an ILI9341 LCD

Feel free to take a closer look at the examples, as they will show you how to draw basic shapes on the LCD.

Resources

Want to make a smart mirror using the Edison and an LCD? Check out the following tutorial:

Interactive Smart Mirror

February 8, 2016
Build a smart mirror that displays weather data using the Intel® Edison.