Displays

Turn a Qwiic Ultrasonic Distance Sensor into a Garage Distance Sensor

January 31, 2025
This tutorial will take your SparkFun Qwiic Ultrasonic Distance Sensor to the next level by turning it into a parking distance sensor!

Display Distance Measurements On an OLED

July 2, 2024
This tutorial will take your SparkFun Qwiic Ultrasonic Distance Sensor to the next level by adding a cool little OLED display.

Fading with the MOSFET Power Switch and Buck Regulator

July 1, 2024
In this tutorial, we will slowly turn on the load and then slowly turn it off using the N-channel MOSFET.

SparkFun Arduino UNO R4 WiFi Qwiic Kit Hookup Guide

July 11, 2023
The SparkFun Arduino UNO R4 WiFi Qwiic Kit is a great way to get started with Arduino and the Qwiic-connect system - use this guide to get started!

Displaying Sensor Data with Bluetooth

March 28, 2023
In our previous Bluetooth tutorial called Sending Sensor Data Via Bluetooth, we showed how to display data from a triple axis accelerometer over the Arduino IDE’s serial monitor. Continuing off of the first tutorial, we are going to expand this project to include more capabilities for visualizing and interacting with your accelerometer data.

LiPo Fuel Gauge (MAX1704X) Hookup Guide

February 23, 2023
Monitor your LiPo battery with the LiPo fuel gauge! In this tutorial, we will be using the MAX17043 and MAX17048 to monitor a single cell, LiPo battery over the Arduino Serial Monitor. We will also connect a display to view the output without the need to connect the microcontroller to a computer.

Qwiic Kit for Raspberry Pi V2 Hookup Guide

December 29, 2022
Get started with the SGP40, BME280, VCNL4040, and microOLED via I2C using the Qwiic system and Python on a Raspberry Pi! Measure VOC Index, light, temperature, humidity, and pressure from the environment. Then display them on the microOLED, serial terminal, or the cloud with Cayenne!

Sending Sensor Data over LoRa

November 4, 2022
This tutorial will show you how setup a simple peer-to-peer connection to send and receive sensor data using LoRa.

MicroMod Qwiic Pro Kit Project Guide

September 29, 2022
The MicroMod Qwiic Pro Kit was designed to allow users to get started with Arduino without the need for soldering or a breadboard. We've included three inputs (a joystick, accelerometer, and proximity sensor) and one display that can be daisy chained to the MicroMod SAMD51 Processor Board.

Qwiic Digital Desk Sign with MicroMod

June 30, 2022
Make a Qwiic-enabled digital desk sign with a MicroMod SAMD51 Processor Board's USB Host and a USB keyboard!

Sending Sensor Data Over WiFi

January 16, 2022
This tutorial will show you how setup a simple peer-to-peer connection to send and receive sensor data between two ESP32 WiFi boards.

SparkFun Qwiic Alphanumeric Display Hookup Guide

October 21, 2021
A Hookup Guide to get you started with the Qwiic Alphanumeric Display.

Qwiic SHIM Kit for Raspberry Pi Hookup Guide

February 16, 2021
Get started with the Serial LCD with RGB backlight and 9DoF IMU (ICM-20948) via I2C using the Qwiic system and Python on a Raspberry Pi! Take sensor readings and display them in the serial terminal or SerLCD.

SparkFun MicroMod Input and Display Carrier Board Hookup Guide

October 21, 2020
A short Hookup Guide to get started with the SparkFun MicroMod Input and Display Carrier Board

The ClockClock Project

October 8, 2020
Tell the time with this fantastic Alchitry project using clocks to make a clock!

Qwiic GPS Clock

September 14, 2020
What time is it? Time for you to... Qwiic-ly build a GPS clock and output it to a display! This project provides you with the current date and time using GPS satellites. Read the date and time as a digital or analog clock. Or even configure the clock for military, your time zone, or automatically adjust the time for daylight savings time!

Qwiic Digital Indoor Thermometer

July 15, 2020
Qwiic-ly build a digital indoor thermometer to measure the ambient temperature of the room and display it using an OLED on an I2C bus!

Working with Qwiic on a Jetson Nano through Jupyter Notebooks

April 23, 2020
We created a few Jupyter Notebooks to make using our Qwiic boards with your Jetson Nano even easier!

SparkFun Top pHAT Hookup Guide

April 16, 2020
The pHAT to sit above your other HATs. Does that make it the "king" of the pHATs? This guide will help you get started using the Top pHAT with the Raspberry Pi.

Qwiic Pro Kit Project Guide

November 7, 2019
The Qwiic Pro Kit was designed to allow users to get started with Arduino without the need for soldering or a breadboard. We've included three inputs (a joystick, accelerometer, and proximity sensor) and one display that can be daisy chained to the RedBoard Turbo (SAMD21) Development Board.

SparkFun Inventor's Kit Experiment Guide - v4.1

August 8, 2019
The SparkFun Inventor's Kit (SIK) Experiment Guide contains all of the information needed to build all five projects, encompassing 16 circuits, in the latest version of the kit, v4.1.2 and v4.1.

Basic Character LCD Hookup Guide

May 28, 2019
Liquid crystal displays (LCDs) are a great way to output a string of words or sensor data to a display for visual feedback. In this tutorial, we'll learn about LCDs, how to print a string of words to a 16x2 basic character LCD and create custom characters.

Displaying Your Coordinates with a GPS Module

April 30, 2019
This Arduino tutorial will teach you how to pinpoint and display your GPS coordinates with a press of a button using hardware from our Qwiic Connect System (I2C).

TFT LCD Breakout 1.8in 128x160 Hookup Guide

April 11, 2019
This TFT LCD Breakout is a versatile, colorful, and easy way to experiment with graphics or create a user interface for your project.
Viewing 76 Displays Tutorials. View All Tutorials.