Wireless

Transfer data between two or more devices without the use of wires! Some of these technologies include WiFi, cellular, Bluetooth, BLE, Zigbee, RFID, NFC, and GPS. Check out the following tutorials below to get started sending data into the air waves!

Connecting Thing Plus Matter to Google Nest Hub

March 30, 2023
Connect your Thing Plus Matter board to a Google Nest Hub, as well as the Google Home app, and set up as a light device!

Displaying Sensor Data with Bluetooth

March 28, 2023
In our previous Bluetooth tutorial called Sending Sensor Data Via Bluetooth, we showed how to display data from a triple axis accelerometer over the Arduino IDE’s serial monitor. Continuing off of the first tutorial, we are going to expand this project to include more capabilities for visualizing and interacting with your accelerometer data.

SparkFun Thing Plus Matter - MGM240P Hookup Guide

March 2, 2023
Get started with the SparkFun Thing Plus Matter - MGM240P with this Hookup Guide. This guide covers the hardware on this development board along with a quick intro to using the board with Silicon Labs' Simplicity Studio IDE.

SparkFun NanoBeacon Board - IN100 Hookup Guide

February 16, 2023
A quick guide to show how to configure and use your own 2.4Ghz wireless beacon with the SparkFun NanoBeacon Board - IN100.

Audio Codec Breakout - WM8960 Hookup Guide

January 26, 2023
The SparkFun Audio Codec Breakout - WM8960 is a low power, high quality stereo codec chock full of features. In this tutorial, some of these features by using an Arduino microcontroller to configure the audio codec and pass audio to the headphone or speaker channels.

Getting Started with u-blox Thingstream and PointPerfect

January 23, 2023
Interested in high precision GNSS without setting up a base station?

Cellular Function Board - Blues Wireless Notecarrier

January 5, 2023
Add a global cellular module to your MicroMod project with the SparkFun Cellular Function Board - Blues Wireless Notecarrier. With this Function board you can not only send data to and from your MicroMod project, you can even update the firmware on the STM32 MicroMod Processor.

Qwiic Kit for Raspberry Pi V2 Hookup Guide

December 29, 2022
Get started with the SGP40, BME280, VCNL4040, and microOLED via I2C using the Qwiic system and Python on a Raspberry Pi! Measure VOC Index, light, temperature, humidity, and pressure from the environment. Then display them on the microOLED, serial terminal, or the cloud with Cayenne!

SparkFun Satellite Transceiver Kit - Swarm M138 Hookup Guide

December 1, 2022
A hookup guide for the SparkFun Satellite Transceiver - Swarm M138 (KIT-21287)

Sending Sensor Data over LoRa

November 4, 2022
This tutorial will show you how setup a simple peer-to-peer connection to send and receive sensor data using LoRa.

GNSS Correction Data Receiver (NEO-D9S) Hookup Guide

October 27, 2022
Add GNSS correction data to your high precision GNSS (HPG) receiver with the u-blox NEO-D9S! This tutorial will get you started with the ZED-F9P, NEO-D9S, and the ESP32 IoT RedBoard.

Wireless Timing Project

September 29, 2022
Time for racing, let's make a wireless timing device using ESP32 wireless communication.

AzureWave Thing Plus (AW-CU488) Hookup Guide

September 22, 2022
The SparkFun AzureWave Thing Plus is a Feather form-factor development board equipped with the AW-CU488. We'll highlight key features of the board and show you to get started with the development board. A few Arduino examples will be highlighted to connect to a WiFi router, calculate the Fast Fourier Transform (FFT) from an input microphone, output an analog signal to a speaker, and connect an Qwiic-enabled device.

Getting Started with the DA16200 FreeRTOS SDK

September 15, 2022
Interested in the DA16200 FreeRTOS SDK? This guide covers setting up the SDK in the Eclipse IDE and how to program our boards with the DA16200 module.

ESP32 Thing Plus (USB-C) Hookup Guide

August 18, 2022
Meet the updated ESP32 Thing Plus (USB-C) development board. We have included some extra bells and whistles that users will appreciate, so check out out hookup guide for all the details!

IoT RedBoard ESP32 Development Board Hookup Guide

August 18, 2022
Delve into the functionality-rich world of the IoT RedBoard ESP32 Development Board!

MicroMod GNSS Function Board - NEO-M9N Hookup Guide

August 11, 2022
The u-blox NEO-M9N is a powerful GPS unit that now comes populated on a MicroMod Function Board! In this tutorial, we will quickly get you set up using it with the MicroMod ecosystem and Arduino so that you can start reading the output.

Monitor Sensor Data from Anywhere

August 10, 2022
Using WiFi to send sensor data from an ESP32 to a WiFi network and be able to read it from an IoT Dashboard from anywhere in the world.

Getting Started with the MyoWare® 2.0 Muscle Sensor Ecosystem

April 1, 2022
The MyoWare® 2.0 Muscle Sensor, an Arduino-compatible, all-in-one electromyography (EMG) sensor from Advancer Technologies. In this tutorial, we will go over the features and related shields to connect the sensor to a muscle group.

Getting Started with the Raspberry Pi Zero 2 W

December 22, 2021
Learn how to setup, configure and use the latest version of the smallest Raspberry Pi out there, the Raspberry Pi Zero 2 W.

Artemis Global Tracker Hookup Guide

December 9, 2021
The SparkFun Artemis Global Tracker combines the Artemis processor with an Iridium 9603N satellite transceiver, ZOE-M8Q GNSS transceiver, and MS8607 PHT sensor. With a clear view of the sky, this board allows you to send and receive short data messages from anywhere in the world including remote locations far beyond the reach of WiFi and GSM networks. Follow this guide to get started with the Artemis Global Tracker.

ARGOS (ARTIC R2) Satellite Communication Guide

November 18, 2021
A guide describing the ARGOS satellite network - as used by our ARTIC R2 satellite communication products

MicroMod WiFi Function Board - DA16200 Hookup Guide

November 11, 2021
Add IoT functionality to any MicroMod project with the MicroMod WiFi function Board - DA16200!
Viewing 140 Wireless Tutorials. View All Tutorials.