Thing Plus
The Thing Plus is a footprint that is used for a board. Each board uses the same specifications (e.g. pin location, common peripherals, board dimensions, etc.) so you can easily switch between different development boards and stack shields that use the same footprint. The Thing Plus footprint is also Feather-compatible, so you can take advantage of existing shield options.
        Sort by:
        
          Recently Added          
        
        
      
    
  
    
          Viewing 19 Thing Plus Tutorials.
      
        View All Tutorials.
      
        
          
        
        
      
      
Sending Sensor Data via Bluetooth
      In this tutorial, we will show you how to get started on incorporating Bluetooth into your electronics projects. This project uses a SparkFun Thing Plus ESP32 Wroom USB-C to display data from a Triple Axis Accelerometer over Bluetooth.    
  
  SparkFun Thing Plus - NINA-B306 Hookup Guide
      A quick guide to get started using the SparkFun Thing Plus - NINA-B306. This Thing Plus is loaded with the Arm Cortex-M4 processor in the NINA-B306 along with on-board motion and environmental sensors in the ISM330DHCX 6DoF and BME280 pressure and temperature sensor.    
  
  AzureWave Thing Plus (AW-CU488) Hookup Guide
      The SparkFun AzureWave Thing Plus is a Feather form-factor development board equipped with the AW-CU488. We'll highlight key features of the board and show you to get started with the development board. A few Arduino examples will be highlighted to connect to a WiFi router,  calculate the Fast Fourier Transform (FFT) from an input microphone, output an analog signal to a speaker, and connect an Qwiic-enabled device.     
  
  DA16200 Thing Plus Hookup Guide
      A guide to get started with the DA16200 Thing Plus.    
  
  ESP32 Thing Plus (USB-C) Hookup Guide
      Meet the updated ESP32 Thing Plus (USB-C) development board. We have included some extra bells and whistles that users will appreciate, so check out out hookup guide for all the details!    
  
  Thing Plus Dual-Port Logging Shield Hookup Guide
      This tutorial shows you how to hook up and use the SparkFun Thing Plus Dual-Port Logging Shield.    
  
  ARGOS ARTIC R2 Satellite Transceiver Shield Hookup Guide
      A hookup guide for the ARGOS Satellite Transceiver Shield - ARTIC R2 (SPX-17236)    
  
  QuickLogic Thing Plus (EOS S3) Hookup Guide
      This guide provides users with functional descriptions, configuration options for the QuickLogic Thing Plus EOS S3. It also serves as a “Getting Started” and “How To” guide.    
  
  STM32 Thing Plus Hookup Guide
      Get started with the STM32 Thing Plus!     
  
  nRF9160 Thing Plus Hookup Guide
      Getting started with the nRF9160 from Circuit Dojo and SparkFun!    
  
  ESP32-S2 Thing Plus Hookup Guide
      Looking to use the more secure ESP32-S2? Follow this hookup guide to get started.    
  
  RP2040 Thing Plus Hookup Guide
      Want to take a stab at advancing your programming skills? Check out the Thing Plus - RP2040, with the first microcontroller from the Raspberry Pi Foundation. This guide will get you started working with the RP2040 and programming in MicroPython and C/C++.    
  
  SparkFun Qwiic Shield for Thing Plus Hookup Guide
      A short guide for assembling and using the SparkFun Qwiic Shield for Thing Plus.    
  
  RED-V Thing Plus Hookup Guide
      This guide will go over the hardware of the RED-V Thing Plus.     
  
  Hookup Guide for the SparkFun Artemis Thing Plus
      Get started with our SparkFun Artemis Thing Plus - our popular Thing Plus footprint with the powerful Artemis module for ultimate functionality.    
  
  XBee3 Thing Plus Hookup Guide
      Get started with SparkFun's XBee3 Thing Plus - both the u.FL as well as the PCB antenna versions.     
  
  SAMD51 Thing Plus Hookup Guide
      This tutorial covers the basic functionality of the SAMD51 Thing Plus and highlights the features of the new ARM Cortex-M4F development board.    
  
  SparkFun ESP32 DMX to LED Shield
      Learn how to utilize your DMX to LED Shield in a variety of different ways.    
  
  ESP32 Thing Plus Hookup Guide
      Hookup guide for the ESP32 Thing Plus (Micro-B) using the ESP32 WROOM's WiFi/Bluetooth system-on-chip in Arduino.    
  
  
        Sort by:
        
          Recently Added          
        
        
      
    
  
    
          Viewing 19 Thing Plus Tutorials.
      
        View All Tutorials.