ESP32
Setup and Using MicroPython for Beginners
In this tutorial, our goal is to help guide you through using MicroPython on a microcontroller unit or Linus SBC, setting up and running mpremote, and getting started with three different development environments
SparkFun Arduino UNO R4 WiFi Qwiic Kit Hookup Guide
The SparkFun Arduino UNO R4 WiFi Qwiic Kit is a great way to get started with Arduino and the Qwiic-connect system - use this guide to get started!
SparkFun RTK Reference Station Hookup Guide
Setup the RTK Reference Station in minutes and start sending RTCM NTRIP corrections to your favourite caster.
Displaying Sensor Data with Bluetooth
In our previous Bluetooth tutorial called Sending Sensor Data Via Bluetooth, we showed how to display data from a triple axis accelerometer over the Arduino IDE’s serial monitor. Continuing off of the first tutorial, we are going to expand this project to include more capabilities for visualizing and interacting with your accelerometer data.
LiPo Fuel Gauge (MAX1704X) Hookup Guide
Monitor your LiPo battery with the LiPo fuel gauge! In this tutorial, we will be using the MAX17043 and MAX17048 to monitor a single cell, LiPo battery over the Arduino Serial Monitor. We will also connect a display to view the output without the need to connect the microcontroller to a computer.
Analog MEMS Microphone (VM2020) Hookup Guide
Get started with the SparkFun analog MEMS microphone breakout board! In this tutorial, we will be connecting the differential MEMS microphone to an Arduino using the WM8960 audio codec.
Audio Codec Breakout - WM8960 Hookup Guide
The SparkFun Audio Codec Breakout - WM8960 is a low power, high quality stereo codec chock full of features. In this tutorial, some of these features by using an Arduino microcontroller to configure the audio codec and pass audio to the headphone or speaker channels.
Getting Started with u-blox Thingstream and PointPerfect
Interested in high precision GNSS without setting up a base station?
GNSS Correction Data Receiver (NEO-D9S) Hookup Guide
Add GNSS correction data to your high precision GNSS (HPG) receiver with the u-blox NEO-D9S! This tutorial will get you started with the ZED-F9P, NEO-D9S, and the ESP32 IoT RedBoard.
Measuring Height with Atmospheric Pressure
Measure height using atmospheric pressure with your Qwiic MicroPressure breakout board!
Wireless Timing Project
Time for racing, let's make a wireless timing device using ESP32 wireless communication.
ESP32 Thing Plus (USB-C) Hookup Guide
Meet the updated ESP32 Thing Plus (USB-C) development board. We have included some extra bells and whistles that users will appreciate, so check out out hookup guide for all the details!
IoT RedBoard ESP32 Development Board Hookup Guide
Delve into the functionality-rich world of the IoT RedBoard ESP32 Development Board!
MicroMod GNSS Function Board - ZED-F9P Hookup Guide
Add millimeter precision location data to your MicroMod project with this guide for the SparkFun MicroMod GNSS Function Board - ZED-F9P.
Monitor Sensor Data from Anywhere
Using WiFi to send sensor data from an ESP32 to a WiFi network and be able to read it from an IoT Dashboard from anywhere in the world.
SparkFun RTK Facet L-Band Hookup Guide
Setup the RTK Facet L-Band in minutes to begin gathering millimeter level geospatial coordinates.
Getting Started with the MyoWare® 2.0 Muscle Sensor Ecosystem
The MyoWare® 2.0 Muscle Sensor, an Arduino-compatible, all-in-one electromyography (EMG) sensor from Advancer Technologies. In this tutorial, we will go over the features and related shields to connect the sensor to a muscle group.
Qwiic ToF Imager - VL53L5CX Hookup Guide
Hookup Guide for the Qwiic ToF Imager - VL53L5CX
Sending Sensor Data Over WiFi
This tutorial will show you how setup a simple peer-to-peer connection to send and receive sensor data between two ESP32 WiFi boards.
SparkFun RTK Facet Hookup Guide
Setup the RTK Facet in minutes to begin gathering millimeter level geospatial coordinates.
MicroMod GNSS Carrier Board (ZED-F9P) Hookup Guide
Easily switch between Processor Boards using the MicroMod ecosystem and get precision down to the diameter of a dime with the ZED-F9P from u-blox using the MicroMod GNSS Carrier Board!
MicroMod WiFi Function Board - ESP32 Hookup Guide
The MicroMod ESP32 Function Board adds additional wireless options to MicroMod Processor Boards that do not have that capability. This special function board acts as a coprocessor that takes advantage of Espressif's ESP32 WROOM to add WiFi and Bluetooth® to your applications.
smôl ESP32 Hookup Guide
Small in size, small on current draw. It's a smôl world! This guide will get you up and running with the smôl ESP32 Processor Board.
smôl Hookup Guide
Small in size, small on current draw. It's a smôl world! This guide will get you up and running with the smôl ecosystem.