Biometrics
The following tutorials use biometric sensors to measure biological signatures. Some of these measurements include fingerprints, voice, muscle (EMG), brainwaves (EEG), or heart rate (ECG)!
Sort by:
Recently Added
Viewing 10 Biometrics Tutorials.
View All Tutorials.
SparkFun Photodetector (MAX30101) Hookup Guide
June 25, 2020
The SparkFun Photodetector - MAX30101 (Qwiic) is the successor to the MAX30105 particle sensor, a highly sensitive optical sensor. This tutorial will get you started on retrieving the raw data from the MAX30101 sensor.
SparkFun Pulse Oximeter and Heart Rate Monitor Hookup Guide
September 12, 2019
Find out your oxygen saturation level or check out your heart rate using the MAX30101 biometric sensor and MAX32664 Biometric Hub via I2C!
SparkFun gator:particle Hookup Guide
June 13, 2019
The gator:particle is an I2C heart-rate monitor and pulse oximeter that can be used as a particle sensor. This tutorial will get you started using the gator:particle with the micro:bit platform.
Fingerprint Scanner (GT-521Fxx) Hookup Guide
March 1, 2018
This tutorial provides information about how to connect to ADH-Tech's fingerprint scanner (GT-521F32) and how to use it with Hawley's FPS_GT511C3 library for Arduino.
Getting Started with Walabot
February 15, 2018
See through walls, track objects, monitor breathing patterns, and more using the power of radio frequency with the Walabot! In this tutorial, we will explore Walabot’s features using the Software Demo Kit (SDK) on Windows and the Application Programming Interface (API) on Linux-based distributions for embedded projects.
MAX30105 Particle and Pulse Ox Sensor Hookup Guide
December 1, 2016
The SparkFun MAX30105 Particle Sensor is a flexible and powerful sensor enabling sensing of distance, heart rate, particle detection, even the blinking of an eye. Get ready. Set. Shine!
MyoWare Muscle Sensor Kit
March 17, 2016
Line of products to work with the MyoWare muscle sensor from Advancer Technologies
AD8232 Heart Rate Monitor Hookup Guide
July 17, 2014
Learn how to create your very own heart rate monitor.
Teardown: Misfit Shine Activity Tracker
April 3, 2014
A quick tear down of the popular fitness tracking device, the Misfit Shine.
Hackers in Residence - Hacking MindWave Mobile
February 26, 2014
Review, teardown, and hacking tutorial for the MindWave Mobile, a $99 commercial grade EEG sensor.
Sort by:
Recently Added
Viewing 10 Biometrics Tutorials.
View All Tutorials.
Old Tutorials
Looking for the old, archived tutorials? Head on over to the
archived tutorials on the main
SparkFun site.
Please be aware that the tutorials you find there are no longer
actively maintained.