Internet of Things
MicroMod Single Pair Ethernet Function Board - ADIN1110 Hookup Guide
May 12, 2022
With the SparkFun MicroMod Single Pair Ethernet Function Board - ADIN1110 you can prototype and create 10BASE-T1L Ethernet connections that work in noisy environments and over exceptionally long distances of over 1 kilometer! Follow this guide to get started with this Function Board.
Satellite Transceiver Breakout - Swarm M138 - Hookup Guide
April 22, 2022
A hookup guide for the Satellite Transceiver Breakout - Swarm M138 (SPX-19236)
MicroMod Ethernet Function Board - W5500 Hookup Guide
March 10, 2022
Add Ethernet and PoE capabilities to your MicroMod project using the Ethernet Function Board - W5500.
Qwiic ToF Imager - VL53L5CX Hookup Guide
January 27, 2022
Hookup Guide for the Qwiic ToF Imager - VL53L5CX
Getting Started with the Raspberry Pi Zero 2 W
December 22, 2021
Learn how to setup, configure and use the latest version of the smallest Raspberry Pi out there, the Raspberry Pi Zero 2 W.
IOTA (ARTIC R2) Satellite Communication Module Hookup Guide
November 18, 2021
A hookup guide for the SparkFun IOTA - Satellite Communication Module (ARTIC R2) (SPX-17984)
ARGOS ARTIC R2 Satellite Transceiver Shield Hookup Guide
November 18, 2021
A hookup guide for the ARGOS Satellite Transceiver Shield - ARTIC R2 (SPX-17236)
ARGOS (ARTIC R2) Satellite Communication Guide
November 18, 2021
A guide describing the ARGOS satellite network - as used by our ARTIC R2 satellite communication products
MicroMod WiFi Function Board - DA16200 Hookup Guide
November 11, 2021
Add IoT functionality to any MicroMod project with the MicroMod WiFi function Board - DA16200!
MicroMod WiFi Function Board - ESP32 Hookup Guide
November 11, 2021
The MicroMod ESP32 Function Board adds additional wireless options to MicroMod Processor Boards that do not have that capability. This special function board acts as a coprocessor that takes advantage of Espressif's ESP32 WROOM to add WiFi and Bluetooth® to your applications.
smôl ESP32 Hookup Guide
October 20, 2021
Small in size, small on current draw. It's a smôl world! This guide will get you up and running with the smôl ESP32 Processor Board.
smôl Hookup Guide
October 19, 2021
Small in size, small on current draw. It's a smôl world! This guide will get you up and running with the smôl ecosystem.
Dialog ULP WiFi DA16200 R3 Shield Hookup Guide
October 7, 2021
Add WiFi to your project with this hookup guide for our Dialog's Ultra Low Power DA16200 R3 shield!
LTE GNSS Breakout - SARA-R5 Hookup Guide
July 8, 2021
A guide to get you started with the SparkFun LTE GNSS Breakout - SARA-R5. This breakout features the SARA-R5 module from u-blox.
ESP32-S2 Thing Plus Hookup Guide
April 8, 2021
Looking to use the more secure ESP32-S2? Follow this hookup guide to get started.
MicroMod Asset Tracker Carrier Board Hookup Guide
February 25, 2021
Get started with the SparkFun MicroMod Asset Tracker Carrier Board following this Hookup Guide. The Asset Tracker uses the u-blox SARA-R510M8S LTE-M / NB-IoT module to provide a host of data communication options.
MicroMod Update Tool Hookup Guide
February 25, 2021
Follow this guide to learn how to use the MicroMod Update Tool to interact directly with the UART on the MicroMod Asset Tracker's SARA-R5. Using this board you can talk directly to the module using u-blox's m-center software as well as update the firmware using EasyFlash.
MicroMod nRF52840 Processor Hookup Guide
January 14, 2021
Get started with the MicroMod nRF52840 Processor following this guide.
How to Build a DIY GNSS Reference Station
October 15, 2020
Learn how to affix a GNSS antenna, use PPP to get its ECEF coordinates and then broadcast your own RTCM data over the internet and cellular using NTRIP to increase rover reception to 10km!
How to Make a Magic Mirror with Raspberry Pi
June 17, 2020
Need a great project for your Raspberry Pi 4 kit? Use it to create a command center to display the weather, clock, your calendar, or even a news feed!
Raspberry Pi 4 Kit Hookup Guide
March 14, 2020
Guide for hooking up your Raspberry Pi 4 Model B basic, desktop, or hardware starter kit together.
Cryptographic Co-Processor ATECC508A (Qwiic) Hookup Guide
October 17, 2019
Learn how to use some of the standard features of the SparkFun Cryptographic Co-processor.
SparkFun Edge Hookup Guide
September 26, 2019
Get to know your Edge board, including both the hardware features for you to utilize as well as how to get talking to it.
Hookup Guide for the SparkFun Artemis Thing Plus
September 19, 2019
Get started with our SparkFun Artemis Thing Plus - our popular Thing Plus footprint with the powerful Artemis module for ultimate functionality.
Old Tutorials
Looking for the old, archived tutorials? Head on over to the
archived tutorials on the main
SparkFun site.
Please be aware that the tutorials you find there are no longer
actively maintained.