GPS
GPS, or Global Positioning System, is accessible from almost everywhere on Earth and provides exact coordinates of your current location so that you can figure out where you are. Combine that information with a good map and there's nothing you can't find. Check out our GPS Buying Guide to compare the current GPS modules available in the catalog. We recommend looking at the GPS Basics tutorial to get started.
Getting Started with u-blox Thingstream and PointPerfect
January 23, 2023
Interested in high precision GNSS without setting up a base station?
GNSS Correction Data Receiver (NEO-D9S) Hookup Guide
October 27, 2022
Add GNSS correction data to your high precision GNSS (HPG) receiver with the u-blox NEO-D9S! This tutorial will get you started with the ZED-F9P, NEO-D9S, and the ESP32 IoT RedBoard.
GNSS Receiver Breakout - MAX-M10S (Qwiic) Hookup Guide
September 1, 2022
Get started using the SparkFun GNSS Receiver Breakout - MAX-M10S (Qwiic), a ultra-low power, GNSS receiver module for your asset tracking needs!
MicroMod GNSS Function Board - ZED-F9P Hookup Guide
August 11, 2022
Add millimeter precision location data to your MicroMod project with this guide for the SparkFun MicroMod GNSS Function Board - ZED-F9P.
MicroMod GNSS Function Board - NEO-M9N Hookup Guide
August 11, 2022
The u-blox NEO-M9N is a powerful GPS unit that now comes populated on a MicroMod Function Board! In this tutorial, we will quickly get you set up using it with the MicroMod ecosystem and Arduino so that you can start reading the output.
SparkFun RTK Facet L-Band Hookup Guide
June 9, 2022
Setup the RTK Facet L-Band in minutes to begin gathering millimeter level geospatial coordinates.
GNSS Timing Breakout - ZED-F9T (Qwiic) Hookup Guide
January 20, 2022
Follow this guide to add up to 5 nanosecond timing accuracy under clear skies with no external GNSS correction with the GNSS Timing Breakout - ZED-F9T (Qwiic).
SparkFun GPS-RTK Dead Reckoning ZED-F9K Hookup Guide
January 6, 2022
The u-blox ZED-F9K is a powerful GPS-RTK unit that uses a fusion of IMU, wheel ticks, a vehicle dynamics model, correction data, and GNSS measurements to provide highly accurate and continuous position for navigation in the difficult conditions. We will quickly get you set up using the Qwiic ecosystem through Arduino so that you can start reading the output!
SparkFun RTK Facet Hookup Guide
December 16, 2021
Setup the RTK Facet in minutes to begin gathering millimeter level geospatial coordinates.
Artemis Global Tracker Hookup Guide
December 9, 2021
The SparkFun Artemis Global Tracker combines the Artemis processor with an Iridium 9603N satellite transceiver, ZOE-M8Q GNSS transceiver, and MS8607 PHT sensor. With a clear view of the sky, this board allows you to send and receive short data messages from anywhere in the world including remote locations far beyond the reach of WiFi and GSM networks. Follow this guide to get started with the Artemis Global Tracker.
MicroMod GNSS Carrier Board (ZED-F9P) Hookup Guide
December 9, 2021
Easily switch between Processor Boards using the MicroMod ecosystem and get precision down to the diameter of a dime with the ZED-F9P from u-blox using the MicroMod GNSS Carrier Board!
smôl ZOE-M8Q Hookup Guide
October 21, 2021
Small in size, small on current draw. It's a smôl world! This guide will get you up and running with the smôl ZOE-M8Q GNSS Peripheral Board.
LTE GNSS Breakout - SARA-R5 Hookup Guide
July 8, 2021
A guide to get you started with the SparkFun LTE GNSS Breakout - SARA-R5. This breakout features the SARA-R5 module from u-blox.
SparkFun RTK Express Hookup Guide
June 21, 2021
Learn how to use the enclosed RTK Express product to achieve millimeter level geospatial coordinates.
nRF9160 Thing Plus Hookup Guide
May 6, 2021
Getting started with the nRF9160 from Circuit Dojo and SparkFun!
How to Upgrade Firmware of a u-blox GNSS Receiver
March 26, 2021
A few steps and you'll upgrade to the latest features on a u-blox GNSS receiver.
MicroMod Update Tool Hookup Guide
February 25, 2021
Follow this guide to learn how to use the MicroMod Update Tool to interact directly with the UART on the MicroMod Asset Tracker's SARA-R5. Using this board you can talk directly to the module using u-blox's m-center software as well as update the firmware using EasyFlash.
MicroMod Asset Tracker Carrier Board Hookup Guide
February 25, 2021
Get started with the SparkFun MicroMod Asset Tracker Carrier Board following this Hookup Guide. The Asset Tracker uses the u-blox SARA-R510M8S LTE-M / NB-IoT module to provide a host of data communication options.
SparkFun RTK Surveyor Hookup Guide
December 3, 2020
Learn how to use the enclosed RTK Surveyor product to achieve millimeter level geospatial coordinates.
How to Build a DIY GNSS Reference Station
October 15, 2020
Learn how to affix a GNSS antenna, use PPP to get its ECEF coordinates and then broadcast your own RTCM data over the internet and cellular using NTRIP to increase rover reception to 10km!
Setting up a Rover Base RTK System
October 14, 2020
Getting GNSS RTCM correction data from a base to a rover is easy with a serial telemetry radio! We'll show you how to get your high precision RTK GNSS system setup and running.
Qwiic GPS Clock
September 14, 2020
What time is it? Time for you to... Qwiic-ly build a GPS clock and output it to a display! This project provides you with the current date and time using GPS satellites. Read the date and time as a digital or analog clock. Or even configure the clock for military, your time zone, or automatically adjust the time for daylight savings time!
OpenLog Artemis Hookup Guide
August 20, 2020
How to use and re-program the OpenLog Artemis, an open source datalogger. The OLA comes preprogrammed to automatically log data. The OLA can also record serial data, analog voltages, or readings from external Qwiic-enabled I2C devices. Some of these Qwiic-enabled devices include GPS/GNSS modules, pressure, altitude, humidity, temperature, air quality, environment, distance, and weight sensors.
SparkFun GPS-RTK Dead Reckoning ZED-F9R Hookup Guide
July 9, 2020
The u-blox ZED-F9R is a powerful GPS-RTK unit that uses a fusion of IMU, wheel ticks, a vehicle dynamics model, correction data, and GNSS measurements to provide highly accurate and continuous position for navigation in the difficult conditions. We will quickly get you set up using the Qwiic ecosystem through Arduino and Python so that you can start reading the output!
Old Tutorials
Looking for the old, archived tutorials? Head on over to the
archived tutorials on the main
SparkFun site.
Please be aware that the tutorials you find there are no longer
actively maintained.