How to Upgrade Firmware of a u-blox GNSS Receiver

≡ Pages
Contributors: Nate

Introduction

For GNSS positioning, u-blox has some of the most incredible receivers available. Over time they will release new versions of the firmware running on those receivers. This tutorial will demonstrate how to upgrade the firmware on the ZED-F9P but can be used for nearly all u-blox receivers including:

Connecting

If you have not already installed u-center, do so now. If this is your first time using u-center, you should be fine, but just now we have a Getting started with u-center tutorial that can be helpful.

Note: For these products, please download and use u-center (original version) and not u-center 2 (latest version). These products are not compatible with u-center 2.


software compatibility

Connecting the ZED-F9P over USB

Connecting the RTK Surveyor over USB

For many modules like the ZED-F9P (shown inside the RTK Surveyor above) or NEO-M8P, a USB connection is as simple as plugging in a USB cable.

SAM-M8Q connected to USB

A USB adapter providing the serial connection

For modules that do not have USB built in, you will need to use a serial to USB adapter and solder in a 6-pin right angle header. Note how the GRN and BLK labels align on both the serial adapter and the SAM-M8Q evaluation board.

COM power menu list

Open u-center and connect to the appropriate COM port. Not sure what COM port to use? The easiest method is to view the listed COM ports, then unplug your device from USB. Now re-open the list. Which COM disappeared? That’s the one you want.

Alternatively, you can Open Device Manager (press the Windows button then type ‘device’).

Device Manager list of COM ports

In the image above COM3 is a COM port on my computer that never goes away. COM11 disappears when I unplug my ZED-F9P so COM11 is the port I need to connect to from u-center.

Backup Device Settings

Updating the firmware will overwrite the device configuration. If you use stock settings or tweak just a few features then you can skip this step. If you have a highly configured receiver that you don’t want to manually configure again, read on.

Receiver configuration sub menu

Open the Receiver Configuration window. It’s under Tools.

Receiver configuration tool

We want to transfer from the receiver to a file. Give the configuration file an easy to remember name. Once complete, the receiver’s settings will be committed to the file.

Loading a configuration to a u-blox receiver

And just as easily, you can load a configuration file back onto the receiver. This is a handy tool for having a handful of different configurations or if you have a batch of receivers that all need to have the same settings applied.

Identifying Current Firmware Version

This is perhaps the most difficult step of the process! Click on the Messages window button.

Messages window

Within the Messages window, you will see a tremendous number of subtrees. Close them all so you only see NMEA, RTCM3, and UBX

All subtress collapsed

Now expand UBX. We need to locate and expand MON, and finally locate VER.

VER message located

Your device’s firmware will be listed in the right window pane. In this example the Firmware Version is 1.13 and the module is the ZED-F9P.

Getting Latest Firmware

Now that you know your current firmware, it’s time to find out if there is anything more recent. SparkFun will generally not host the binary files that u-blox releases. This is because we want you to have the latest and greatest version directly from u-blox. You can usually find the firmware for a given product under the ‘Documents and resources’ tab for that given product. Here’s the ZED-F9P as an example.

Documents tab

Scroll or search this page for ‘firmware’

Download firmware link

Download this binary to a folder where you can easily find it.

Upgrading Firmware

Firmware update sub-menu

Select Firmware Update from the Tools menu. Note that while the menu says that Ctrl+U is the shortcut, it is not! Ctrl+U will open the legacy firmware update tool. Be careful and use your mouse.

Firmware update tool window

Press the button with three dots '...' and locate the firmware image you just downloaded. When you’re ready, press the green dot button labeled ‘GO’ in the lower left corner.

Loading new firmware

Sit back and wait. This upgrade took about 60s but your mileage may vary.

Firmware update success

Upon completion, you should see the ‘Firmware Update Success’ message. The GNSS receiver will reset and re-enumerate over USB (if it has USB built-in). On the ZED-F9P all device settings and configurations were overwritten so if you previously saved your device’s configuration now is a good time to reload them.

Further Reading

Thanks for reading! We hope this makes the firmware upgrade process a bit less daunting. If you're unsure about the changes and advantages to each firmware release, be sure to checkout the 'Release Notes' listed on a given u-blox receiver's documents page.

Want more GNSS goodness? Checkout some of these great tutorials:

Building an Autonomous Vehicle: The Batmobile

Documenting a six-month project to race autonomous Power Wheels at the SparkFun Autonomous Vehicle Competition (AVC) in 2016.

What is GPS RTK?

Learn about the latest generation of GPS and GNSS receivers to get 14mm positional accuracy!

Getting Started with U-Center for u-blox

Learn the tips and tricks to use the u-blox software tool to configure your GPS receiver.

GPS-RTK2 Hookup Guide

Get precision down to the diameter of a dime with the new ZED-F9P from u-blox.

SparkFun GPS Breakout (ZOE-M8Q and SAM-M8Q) Hookup Guide

The SparkFun ZOE-M8Q and SAM-M8Q are three similarly powerful GNSS boards, but with different project applications. We'll compare both GNSS receivers before getting each up and running.

Setting up a Rover Base RTK System

Getting GNSS RTCM correction data from a base to a rover is easy with a serial telemetry radio! We'll show you how to get your high precision RTK GNSS system setup and running.

How to Build a DIY GNSS Reference Station

Learn how to affix a GNSS antenna, use PPP to get its ECEF coordinates and then broadcast your own RTCM data over the internet and cellular using NTRIP to increase rover reception to 10km!

MicroMod Asset Tracker Carrier Board Hookup Guide

Get started with the SparkFun MicroMod Asset Tracker Carrier Board following this Hookup Guide. The Asset Tracker uses the u-blox SARA-R510M8S LTE-M / NB-IoT module to provide a host of data communication options.