micropython

MicroPython is an open source interpreter for the Python programming language developed specifically for microcontrollers. It is a subset of the Python 3 language that has been pared down to run efficiently on several microcontrollers. If you are familiar with Python or looking for a quick way to write code for a microcontroller (that isn't C/C++, Arduino, or assembly), MicroPython is a good option. Depending on the hardware, not all Python modules are available. Make sure to check the documentation.

Setup and Using MicroPython for Beginners

July 23, 2025
In this tutorial, our goal is to help guide you through using MicroPython on a microcontroller unit or Linus SBC, setting up and running mpremote, and getting started with three different development environments

RP2040 Thing Plus Hookup Guide

January 21, 2021
Want to take a stab at advancing your programming skills? Check out the Thing Plus - RP2040, with the first microcontroller from the Raspberry Pi Foundation. This guide will get you started working with the RP2040 and programming in MicroPython and C/C++.

Pro Micro RP2040 Hookup Guide

January 21, 2021
This tutorial covers the basic functionality of the Pro Micro RP2040 and highlights the features of the dual-core ARM Cortex-M0+ processors development board. Get started with the first microcontroller from the Raspberry Pi Foundation!

MicroMod RP2040 Processor Board Hookup Guide

January 21, 2021
This tutorial covers the basic functionality of the MicroMod RP2040 Processor Board and highlights the features of the dual-core ARM Cortex-M0+ processors development board. Get started with the first microcontroller from the Raspberry Pi Foundation!

XBee3 Thing Plus Hookup Guide

August 22, 2019
Get started with SparkFun's XBee3 Thing Plus - both the u.FL as well as the PCB antenna versions.

ARM Programming

May 23, 2019
How to program SAMD21 or SAMD51 boards (or other ARM processors).

SparkFun gator:bit v2 Hookup Guide

January 31, 2019
The gator:bit v2 is a breakout board for the BBC micro:bit. The gator:bit exposes almost every pin on the micro:bit to clippable pad with circuit protection. It also has as built-in addressable LEDs and a built-in buzzer.

MicroPython Programming Tutorial: Getting Started with the ESP32 Thing

September 26, 2018
MicroPython is an implementation and subset of the Python 3 programming language that can be used on microcontrollers. This guide will walk you through writing MicroPython programs for the ESP32 Thing development board.

How to Load MicroPython on a Microcontroller Board

September 4, 2018
This tutorial will show you how to load the MicroPython interpreter onto a variety of development boards.

Pyboard Hookup Guide

September 7, 2017
Getting started with the Pyboard using MicroPython.

Exploring XBees and XCTU

March 12, 2015
How to set up an XBee using your computer, the X-CTU software, and an XBee Explorer interface board.