Projects

Need inspiration? Find it here! These tutorials feature special projects broken down into steps to illustrate how you can use various concepts, skills, and technologies to build awesome stuff.

How to Run a 5V Device On a 3.3V System With Qwiic

June 5, 2025
Power up your 5V I2C devices on the Qwiic system! This tutorial shows you how to use the SparkFun Qwiic 5V Boost to integrate power-hungry sensors like the SEN55 seamlessly.

Calibrating Your Odometry Sensor

December 2, 2024
In this tutorial, we will cover how to calibrate your Qwiic Optical Tracking Odometry Sensor (or "OTOS") with Arduino and Python Examples.

Moving Beyond the Ordinary With the Qwiic Alphanumeric Display

November 7, 2024
More than just numbers, more than just letters, with a little creative coding you can do teach your alphanumeric display lots of new tricks.

IMU Data to Motion: Tutorial for Translating Sensor Data into Real-World Movement

November 3, 2024
Sometimes we want to do more with our data than just watch the values roll by on a screen. In this tutorial, we'll take a look at one way we can translate that data to movement.

How to Play Multiple Buzzers at Once

October 18, 2024
This tutorial demonstrates the SparkFun Qwiic Buzzer's ability to control multiple buzzers simultaneously by playing a 3-part arrangement of a segment of the Super Mario Bros Theme!

GeoFence Treasure Hunt With Artemis Global Tracker

July 31, 2024
Follow along with an engineering student as he creates a distance-based game using the Artemis Global Tracker!

Connecting Thing Plus Matter to Google Nest Hub

March 30, 2023
Connect your Thing Plus Matter board to a Google Nest Hub, as well as the Google Home app, and set up as a light device!

Qwiic Kit for Raspberry Pi V2 Hookup Guide

December 29, 2022
Get started with the SGP40, BME280, VCNL4040, and microOLED via I2C using the Qwiic system and Python on a Raspberry Pi! Measure VOC Index, light, temperature, humidity, and pressure from the environment. Then display them on the microOLED, serial terminal, or the cloud with Cayenne!

Sending Sensor Data over LoRa

November 4, 2022
This tutorial will show you how setup a simple peer-to-peer connection to send and receive sensor data using LoRa.

MicroMod Qwiic Pro Kit Project Guide

September 29, 2022
The MicroMod Qwiic Pro Kit was designed to allow users to get started with Arduino without the need for soldering or a breadboard. We've included three inputs (a joystick, accelerometer, and proximity sensor) and one display that can be daisy chained to the MicroMod SAMD51 Processor Board.

Measuring Height with Atmospheric Pressure

September 29, 2022
Measure height using atmospheric pressure with your Qwiic MicroPressure breakout board!

Wireless Timing Project

September 29, 2022
Time for racing, let's make a wireless timing device using ESP32 wireless communication.

Monitor Sensor Data from Anywhere

August 10, 2022
Using WiFi to send sensor data from an ESP32 to a WiFi network and be able to read it from an IoT Dashboard from anywhere in the world.

The 970-HA-JOKES Payphone Project

July 11, 2022
A payphone turned into a bit of fun.

Qwiic Digital Desk Sign with MicroMod

June 30, 2022
Make a Qwiic-enabled digital desk sign with a MicroMod SAMD51 Processor Board's USB Host and a USB keyboard!

Sending Sensor Data Over WiFi

January 16, 2022
This tutorial will show you how setup a simple peer-to-peer connection to send and receive sensor data between two ESP32 WiFi boards.

How to Build a DIY GNSS Reference Station

October 15, 2020
Learn how to affix a GNSS antenna, use PPP to get its ECEF coordinates and then broadcast your own RTCM data over the internet and cellular using NTRIP to increase rover reception to 10km!

Setting up a Rover Base RTK System

October 14, 2020
Getting GNSS RTCM correction data from a base to a rover is easy with a serial telemetry radio! We'll show you how to get your high precision RTK GNSS system setup and running.

The ClockClock Project

October 8, 2020
Tell the time with this fantastic Alchitry project using clocks to make a clock!

Qwiic GPS Clock

September 14, 2020
What time is it? Time for you to... Qwiic-ly build a GPS clock and output it to a display! This project provides you with the current date and time using GPS satellites. Read the date and time as a digital or analog clock. Or even configure the clock for military, your time zone, or automatically adjust the time for daylight savings time!

Jetson Nano + Sphero RVR Mash-up (PART 2)

July 29, 2020
We took two of our biggest robotics partnerships from the previous year and shazamed them together into one robot to rule them all!

Qwiic Digital Indoor Thermometer

July 15, 2020
Qwiic-ly build a digital indoor thermometer to measure the ambient temperature of the room and display it using an OLED on an I2C bus!

Nintendo Switch Macro Recording on the Raspberry Pi

July 8, 2020
Learn how to record and playback controller 'macros' for your Nintendo Switch using a Raspberry Pi, SparkFun Top pHAT, and Joycontrol.

ESP32 OTA Updates over BLE from a React Web Application

July 2, 2020
Learn how to flash firmware Over-the-Air using a BLE React WebApp and ESP32
Viewing 191 Projects Tutorials. View All Tutorials.