Time
Time is of the essence. Keep track of the date or time using a GPS module, Real Time Clock (RTC), or even grabbing the current time from the Internet. Whatever your preference, start making your own clock, timers, generating a signal, or adding a timestamp with your sensor data. Check out the tutorials below for ideas!
Wireless Timing Project
Time for racing, let's make a wireless timing device using ESP32 wireless communication.
Dialog ULP WiFi DA16200 R3 Shield Hookup Guide
Add WiFi to your project with this hookup guide for our Dialog's Ultra Low Power DA16200 R3 shield!
The ClockClock Project
Tell the time with this fantastic Alchitry project using clocks to make a clock!
Qwiic GPS Clock
What time is it? Time for you to... Qwiic-ly build a GPS clock and output it to a display! This project provides you with the current date and time using GPS satellites. Read the date and time as a digital or analog clock. Or even configure the clock for military, your time zone, or automatically adjust the time for daylight savings time!
OpenLog Artemis Hookup Guide
How to use and re-program the OpenLog Artemis, an open source datalogger. The OLA comes preprogrammed to automatically log data. The OLA can also record serial data, analog voltages, or readings from external Qwiic-enabled I2C devices. Some of these Qwiic-enabled devices include GPS/GNSS modules, pressure, altitude, humidity, temperature, air quality, environment, distance, and weight sensors.
How to Make a Magic Mirror with Raspberry Pi
Need a great project for your Raspberry Pi 4 kit? Use it to create a command center to display the weather, clock, your calendar, or even a news feed!
RFID Beginners Tutorial
Make a remote work logger using an RFID reader and a GPS module. Scan a card and get ID, location, and time. All the perfect data to punch in and punch out from the middle of Nowhere!
Wireless Remote Weather Station with micro:bit
Monitor the weather without being exposed to it through wireless communication between two micro:bits using the radio blocks! This is useful if your weather station is installed in a location that is difficult to retrieve data from the OpenLog. We will also explore a few different ways to send and receive data.
Real Time Clock Module - RV-8803 (Qwiic) Hookup Guide
A Hookup Guide for the SparkFun Real Time Clock Module - RV-8803 (Qwiic). Learn how to integrate the RV-8803 into your next time-keeping project.
SparkFun Clock Generator 5P49V60 (Qwiic) Hookup Guide
The SparkFun Clock Generator 5P49V60 (Qwiic) breakout board offers a wide range of customizable frequencies in a wide range of different signal types using a single reference clock. This hookup guide will go over all of the many available functions and gives the hardware rundown on what exactly is on this board.
SparkFun Qwiic Micro (SAMD21E) Hookup Guide
An introduction to the Qwiic Micro SAMD21E. Level up your Arduino-skills with the powerful SAMD21 ARM Cortex M0+ processor!
SparkFun gator:RTC Hookup Guide
The gator:RTC is an I2C based, real-time clock (RTC) for keeping time while your micro:bit isn't powered. This tutorial will get you started using the gator:RTC with the micro:bit platform.
RedBoard Turbo Hookup Guide
An introduction to the RedBoard Turbo. Level up your Arduino-skills with the powerful SAMD21 ARM Cortex M0+ processor!
Getting Started with the SmartLED Shield for Teensy
In this tutorial, we will connect different RGB LED matrix panels to PixelMatix's SmartLED shield and Teensy.
Qwiic Real Time Clock Module (RV-1805) Hookup Guide
Find out what time it is, even after the power's been out on your project for a while with the Qwiic Real Time Clock (RTC) module.
IoT Power Relay
Using the ESP32 to make a web-configured timed relay.
Sunrise Machine with the Tessel 2
Are you to sleepy to enjoy a sunrise on a brisk morning? Yeah...us too! No worries, with a Webcam, a Tessel 2 and a bit of code you can sleep in and catch the sunrise at your leisure with the Sunrise Machine.
DeadOn RTC Breakout Hookup Guide
An introduction to the DS3234 real-time clock (RTC), example wiring diagrams, and an Arduino library!
Real Time Clock Module Hookup Guide
A quick introduction to the DS1307 RTC module and a hookup guide for the SparkFun Breakout.
Experiment Guide for the Johnny-Five Inventor's Kit
Use the Tessel 2 and the Johnny Five Inventors kit to explore the world of JavaScript enabled hardware through 14 awesome experiments!
Blynk Board Project Guide
A series of Blynk projects you can set up on the Blynk Board without ever re-programming it.
SAMD21 Mini/Dev Breakout Hookup Guide
An introduction to the Atmel ATSAMD21G18 microprocessor and our Mini and Pro R3 breakout boards. Level up your Arduino-skills with the powerful ARM Cortex M0+ processor.
SparkFun Inventor's Kit for Photon Experiment Guide
Dive into the world of the Internet of Things with the SparkFun Inventor's Kit for Photon.
Adding a Timed Button to a Project
This tutorial will walk you through making a timed power controller for interactive projects. You will learn how to add an on button that will provide power to your project for an amount of time and then turn off again.