ESP8266

Installing Board Definitions in the Arduino IDE

September 9, 2020

How do I install a custom Arduino board/core? It's easy! This tutorial will go over how to install an Arduino board definition using the Arduino Board Manager. We will also go over manually installing third-party cores, such as the board definitions required for many of the SparkFun development boards.

LuMini 8x8 Matrix Hookup Guide

January 24, 2019

The LuMini 8x8 Matrix (APA102-2020) are the highest resolution LED matrix available.

LuMini Ring Hookup Guide

January 17, 2019

The LuMini Rings (APA102-2020) are the highest resolution LED rings available.

SparkFun WiFi IR Blaster Hookup Guide

December 6, 2018

How to assemble the WiFi IR Blaster and program it using Arduino. You'll be controlling IR devices from the web in no time!

Introduction to MQTT

November 7, 2018

An introduction to MQTT, one of the main communication protocols used with the Internet of Things (IoT).

Using Flask to Send Data to a Raspberry Pi

November 9, 2017

In this tutorial, we'll show you how to use the Flask framework for Python to send data from ESP8266 WiFi nodes to a Raspberry Pi over an internal WiFi network.

Internet of Things Experiment Guide

November 23, 2016

The SparkFun ESP8266 Thing Dev Board is a powerful development platform that lets you connect your hardware projects to the Internet. In this guide, we show you how to combine some simple components to remotely log temperature data, send yourself texts and control lights from afar.

Blynk Board Washer/Dryer Alarm

March 31, 2016

How to configure the Blynk Board and app to notify you when your washer or dryer is done shaking.

Blynk Board Arduino Development Guide

March 25, 2016

How to get your computer set up with Arduino and the Blynk Board hardware definitions -- so you can start creating Blynk projects of your own!

Blynk Board Bridge Widget Demo

March 25, 2016

A Blynk project that demonstrates how to use the Bridge widget to get two (or more) Blynk Boards to communicate.

Blynk Board Project Guide

March 25, 2016

A series of Blynk projects you can set up on the Blynk Board without ever re-programming it.

Getting Started with the SparkFun Blynk Board

March 25, 2016

How to provision a Blynk Board - get it connected to Wi-Fi and Blynk, so you can start Blynking!

ESP8266 Powered Propane Poofer

March 15, 2016

Learn how Nick Poole built a WiFi controlled fire-cannon using the ESP8266 Thing Dev Board!

LED Cloud-Connected Cloud

February 22, 2016

Make an RGB colored cloud light! You can also control it from your phone, or hook up to the weather!

ESP8266 Thing Development Board Hookup Guide

November 5, 2015

An overview of SparkFun's ESP8266 Thing Development Board - a development board for the Internet of Things.

ESP8266 WiFi Shield Hookup Guide

July 16, 2015

Interface your Arduino with an ESP8266 to give it inexpensive access to your WiFi network and the Internet!

ESP8266 Thing Hookup Guide

May 21, 2015

An overview of SparkFun's ESP8266 Thing - a development board for the Internet of...Things. This tutorial explains the circuitry driving the board, and how to get it up and running in an Arduino environment.

Old Tutorials

Looking for the old, archived tutorials? Head on over to the archived tutorials on the main SparkFun site.
Please be aware that the tutorials you find there are no longer actively maintained.