Sensors

Build Your Own High-Concentration CO2 Detector

September 23, 2025
The SparkFun STC31 CO2 Sensor can accurately measure CO2 concentrations up to 100% with high repeatability and long-term stability, thanks to humidity and temperature compensation provided by the built-in SHTC3. This tutorial will show you how!

How to Run a 5V Device On a 3.3V System With Qwiic

June 5, 2025
Power up your 5V I2C devices on the Qwiic system! This tutorial shows you how to use the SparkFun Qwiic 5V Boost to integrate power-hungry sensors like the SEN55 seamlessly.

Turn a Qwiic Ultrasonic Distance Sensor into a Garage Distance Sensor

January 31, 2025
This tutorial will take your SparkFun Qwiic Ultrasonic Distance Sensor to the next level by turning it into a parking distance sensor!

Calibrating Your Odometry Sensor

December 2, 2024
In this tutorial, we will cover how to calibrate your Qwiic Optical Tracking Odometry Sensor (or "OTOS") with Arduino and Python Examples.

IMU Data to Motion: Tutorial for Translating Sensor Data into Real-World Movement

November 3, 2024
Sometimes we want to do more with our data than just watch the values roll by on a screen. In this tutorial, we'll take a look at one way we can translate that data to movement.

Detecting Colors with the SparkFun Tristimulus Color Sensor

August 22, 2024
Detect and classify colors based on their CIE XYZ color space values.

Display Distance Measurements On an OLED

July 2, 2024
This tutorial will take your SparkFun Qwiic Ultrasonic Distance Sensor to the next level by adding a cool little OLED display.

Fading with the MOSFET Power Switch and Buck Regulator

July 1, 2024
In this tutorial, we will slowly turn on the load and then slowly turn it off using the N-channel MOSFET.

SparkFun Arduino UNO R4 WiFi Qwiic Kit Hookup Guide

July 11, 2023
The SparkFun Arduino UNO R4 WiFi Qwiic Kit is a great way to get started with Arduino and the Qwiic-connect system - use this guide to get started!

Sending Sensor Data via Bluetooth

April 14, 2023
In this tutorial, we will show you how to get started on incorporating Bluetooth into your electronics projects. This project uses a SparkFun Thing Plus ESP32 Wroom USB-C to display data from a Triple Axis Accelerometer over Bluetooth.

Displaying Sensor Data with Bluetooth

March 28, 2023
In our previous Bluetooth tutorial called Sending Sensor Data Via Bluetooth, we showed how to display data from a triple axis accelerometer over the Arduino IDE’s serial monitor. Continuing off of the first tutorial, we are going to expand this project to include more capabilities for visualizing and interacting with your accelerometer data.

SparkFun Thing Plus - NINA-B306 Hookup Guide

March 23, 2023
A quick guide to get started using the SparkFun Thing Plus - NINA-B306. This Thing Plus is loaded with the Arm Cortex-M4 processor in the NINA-B306 along with on-board motion and environmental sensors in the ISM330DHCX 6DoF and BME280 pressure and temperature sensor.

Analog MEMS Microphone (VM2020) Hookup Guide

February 9, 2023
Get started with the SparkFun analog MEMS microphone breakout board! In this tutorial, we will be connecting the differential MEMS microphone to an Arduino using the WM8960 audio codec.

SparkFun Temperature Sensor - STTS22H (Qwiic) Hookup Guide

January 19, 2023
Get started with the ultralow-power, high-accuracy, qwiic-enabled SparkFun Temperature Sensor - STTS22H!

Qwiic Kit for Raspberry Pi V2 Hookup Guide

December 29, 2022
Get started with the SGP40, BME280, VCNL4040, and microOLED via I2C using the Qwiic system and Python on a Raspberry Pi! Measure VOC Index, light, temperature, humidity, and pressure from the environment. Then display them on the microOLED, serial terminal, or the cloud with Cayenne!

SparkFun Triple Axis Accelerometer Breakout - BMA400 (Qwiic) Hookup Guide

December 8, 2022
Add low power triple axis motion monitoring to your Qwiic project using the SparkFun Triple Axis Accelerometer Breakout - BMA400 (Qwiic).

SparkFun Absolute Digital Barometer - LPS28DFW (Qwiic) Hookup Guide

December 8, 2022
Get started adding water-resistant pressure sensing using the SparkFun Absolute Digital Barometer - LPS28DFW (Qwiic) following this guide.

SparkFun Indoor Air Quality Sensor - ENS160 (Qwiic) Hookup Guide

November 11, 2022
Is your air safe? Check your eCO2, TVOC, and AQI levels with the new SparkFun Indoor Air Quality Sensor - ENS160!

Sending Sensor Data over LoRa

November 4, 2022
This tutorial will show you how setup a simple peer-to-peer connection to send and receive sensor data using LoRa.

Getting Started with Machinechat

October 7, 2022
Organize and display your data with SparkFun's Artemis OpenLog and MachineChat's JEDIOne!

Wireless Timing Project

September 29, 2022
Time for racing, let's make a wireless timing device using ESP32 wireless communication.

MicroMod Qwiic Pro Kit Project Guide

September 29, 2022
The MicroMod Qwiic Pro Kit was designed to allow users to get started with Arduino without the need for soldering or a breadboard. We've included three inputs (a joystick, accelerometer, and proximity sensor) and one display that can be daisy chained to the MicroMod SAMD51 Processor Board.

Measuring Height with Atmospheric Pressure

September 29, 2022
Measure height using atmospheric pressure with your Qwiic MicroPressure breakout board!

Monitor Sensor Data from Anywhere

August 10, 2022
Using WiFi to send sensor data from an ESP32 to a WiFi network and be able to read it from an IoT Dashboard from anywhere in the world.
Viewing 236 Sensors Tutorials. View All Tutorials.