micro:bit


The BBC micro:bit is a pocket-sized computer that lets you get creative with digital technology. You can code, customize, and control your micro:bit from anywhere! You can use your micro:bit for all sorts of unique creations, from robots to musical instruments and more. We recommend looking at our Getting Started with the micro:bit or tutorials tagged with micro:bit to start.

Getting Started with the micro:bit

September 2, 2021
The BBC micro:bit is a compact, powerful programming tool that requires no software installation. Read on to learn how to use it YOUR way!

micro:bit Breakout Board Hookup Guide

June 17, 2021
How to get started with the micro:bit breakout board.

Wireless Remote Weather Station with micro:bit

May 11, 2020
Monitor the weather without being exposed to it through wireless communication between two micro:bits using the radio blocks! This is useful if your weather station is installed in a location that is difficult to retrieve data from the OpenLog. We will also explore a few different ways to send and receive data.

micro:bot Kit Experiment Guide

February 20, 2020
Get started with the moto:bit, a carrier board for the micro:bit that allows you to control motors, and create your own robot using this experiment guide for the micro:bot kit.

SparkFun gator:RTC Hookup Guide

September 5, 2019
The gator:RTC is an I2C based, real-time clock (RTC) for keeping time while your micro:bit isn't powered. This tutorial will get you started using the gator:RTC with the micro:bit platform.

SparkFun gator:UV Hookup Guide

September 5, 2019
The gator:UV is an I2C based UV sensor. This tutorial will get you started using the gator:UV with the micro:bit platform.

SparkFun gator:log Hookup Guide

September 5, 2019
The gator:log is a serial communication based data logger. This tutorial will get you started using the gator:log with the micro:bit platform.

SparkFun gator:soil Hookup Guide

June 13, 2019
The gator:soil is analog soil moisture sensor. This tutorial will get you started using the gator:soil with the micro:bit platform.

SparkFun gator:microphone Hookup Guide

June 13, 2019
The gator:microphone is an I2C sensor for detecting sound with an electret microphone. This tutorial will get you started using the gator:microphone with the micro:bit platform.

SparkFun gator:environment Hookup Guide

June 13, 2019
The gator:environment combines two I2C sensors for temperature, humidity, pressure, eCO2, and eTVOC values. This tutorial will get you started using the gator:environment with the micro:bit platform.

SparkFun gator:particle Hookup Guide

June 13, 2019
The gator:particle is an I2C heart-rate monitor and pulse oximeter that can be used as a particle sensor. This tutorial will get you started using the gator:particle with the micro:bit platform.

How to Create a MakeCode Package for Micro:Bit

April 16, 2019
Learn how to develop code blocks for the Micro:bit in Microsoft MakeCode!

SparkFun gator:bit v2 Hookup Guide

January 31, 2019
The gator:bit v2 is a breakout board for the BBC micro:bit. The gator:bit exposes almost every pin on the micro:bit to clippable pad with circuit protection. It also has as built-in addressable LEDs and a built-in buzzer.

Wireless Remote Control with micro:bit

January 21, 2019
In this tutorial, we will utilize the MakeCode radio blocks to have the one micro:bit transmit a signal to a receiving micro:bit on the same channel. Eventually, we will control a micro:bot wirelessly using parts from the arcade:kit!

Gator:starter ProtoSnap Hookup Guide

October 18, 2018
Get started clipping sensors and lights to the micro:bit with the gator:starter gator:board from SparkFun!

Gator:color ProtoSnap Hookup Guide

October 18, 2018
Clip some LED's onto your gator:bit with the gator:color.

Gator:control ProtoSnap Hookup Guide

October 17, 2018
Buttons and switches and inputs oh my! Start adding more control to your gator:bit with the SparkFun gator:control.

How to Load MicroPython on a Microcontroller Board

September 4, 2018
This tutorial will show you how to load the MicroPython interpreter onto a variety of development boards.

micro:bit Educator Lab Pack Experiment Guide

May 8, 2018
A quickstart guide for the micro:bit educator lab pack.

micro:arcade Kit Experiment Guide

July 21, 2017
We love games! We love writing games, building games and yes, even building game consoles. So we want to introduce to you the micro:arcade kit for the micro:bit!

SparkFun Inventor's Kit for micro:bit Experiment Guide

July 21, 2017
This guide contains all the information you will need to explore the twelve circuits of the SparkFun Inventors Kit for micro:bit.

micro:climate Kit Experiment Guide

July 21, 2017
A weather station kit that is built on top of the inexpensive, easy-to-use micro:bit and Microsoft MakeCode.