ESP32
SparkFun RTK Express Hookup Guide
Learn how to use the enclosed RTK Express product to achieve millimeter level geospatial coordinates.
ESP32-S2 Thing Plus Hookup Guide
Looking to use the more secure ESP32-S2? Follow this hookup guide to get started.
SparkFun RTK Surveyor Hookup Guide
Learn how to use the enclosed RTK Surveyor product to achieve millimeter level geospatial coordinates.
MicroMod All The Pins (ATP) Carrier Board
Access All The Pins (ATP) of the MicroMod Processor Board with the Carrier Board!
MicroMod ESP32 Processor Board Hookup Guide
A short hookup guide to get started with the SparkFun MicroMod ESP32 Processor Board.
Getting Started with MicroMod
Dive into the world of MicroMod - a compact interface to connect a microcontroller to various peripherals via the M.2 Connector!
How to Build a DIY GNSS Reference Station
Learn how to affix a GNSS antenna, use PPP to get its ECEF coordinates and then broadcast your own RTCM data over the internet and cellular using NTRIP to increase rover reception to 10km!
Installing Board Definitions in the Arduino IDE
How do I install a custom Arduino board/core? It's easy! This tutorial will go over how to install an Arduino board definition using the Arduino Board Manager. We will also go over manually installing third-party cores, such as the board definitions required for many of the SparkFun development boards.
ESP32 OTA Updates over BLE from a React Web Application
Learn how to flash firmware Over-the-Air using a BLE React WebApp and ESP32
ESP32 Relay Web Server
The goal of this project is to have a website hosted on an ESP32 that controls any relay controlled device connected to a local network and keeps a dynamically updated state of those devices.
Using Home Assistant to Expand Your Home Automations
An introduction to Home Assistant, an open source home automation hub.
TFT LCD Breakout 1.8in 128x160 Hookup Guide
This TFT LCD Breakout is a versatile, colorful, and easy way to experiment with graphics or create a user interface for your project.
SparkFun ESP32 DMX to LED Shield
Learn how to utilize your DMX to LED Shield in a variety of different ways.
ESP32 Thing Plus Hookup Guide
Hookup guide for the ESP32 Thing Plus (Micro-B) using the ESP32 WROOM's WiFi/Bluetooth system-on-chip in Arduino.
Transparent Graphical OLED Breakout Hookup Guide
The future is here! Our Qwiic Transparent Graphical OLED Breakout allows you to display custom images on a transparent screen using either I2C or SPI connections.
LuMini 8x8 Matrix Hookup Guide
The LuMini 8x8 Matrix (APA102-2020) are the highest resolution LED matrix available.
LuMini Ring Hookup Guide
The LuMini Rings (APA102-2020) are the highest resolution LED rings available.
SparkFun LoRa Gateway 1-Channel Hookup Guide
How to setup and use the LoRa Gateway 1-Channel in Arduino.
Introduction to MQTT
An introduction to MQTT, one of the main communication protocols used with the Internet of Things (IoT).
MicroPython Programming Tutorial: Getting Started with the ESP32 Thing
MicroPython is an implementation and subset of the Python 3 programming language that can be used on microcontrollers. This guide will walk you through writing MicroPython programs for the ESP32 Thing development board.
I2S Audio Breakout Hookup Guide
Hookup guide for the MAX98357A I2S audio breakout board.
How to Load MicroPython on a Microcontroller Board
This tutorial will show you how to load the MicroPython interpreter onto a variety of development boards.
ESP32 LoRa 1-CH Gateway, LoRaWAN, and the Things Network
Using the ESP32 LoRa 1-CH Gateway as a gateway and device, and pushing data to The Things Network.
IoT Power Relay
Using the ESP32 to make a web-configured timed relay.