Wireless
Transfer data between two or more devices without the use of wires! Some of these technologies include WiFi, cellular, Bluetooth, BLE, Zigbee, RFID, NFC, and GPS. Check out the following tutorials below to get started sending data into the air waves!
MicroMod WiFi Function Board - DA16200 Hookup Guide
Add IoT functionality to any MicroMod project with the MicroMod WiFi function Board - DA16200!
MicroMod WiFi Function Board - ESP32 Hookup Guide
The MicroMod ESP32 Function Board adds additional wireless options to MicroMod Processor Boards that do not have that capability. This special function board acts as a coprocessor that takes advantage of Espressif's ESP32 WROOM to add WiFi and Bluetooth® to your applications.
smôl ZOE-M8Q Hookup Guide
Small in size, small on current draw. It's a smôl world! This guide will get you up and running with the smôl ZOE-M8Q GNSS Peripheral Board.
smôl ARTIC R2 Hookup Guide
Small in size, small on current draw. It's a smôl world! This guide will get you up and running with the smôl ARTIC R2 satellite communication Peripheral Board.
Dialog ULP WiFi DA16200 R3 Shield Hookup Guide
Add WiFi to your project with this hookup guide for our Dialog's Ultra Low Power DA16200 R3 shield!
SparkFun RTK Express Hookup Guide
Learn how to use the enclosed RTK Express product to achieve millimeter level geospatial coordinates.
nRF9160 Thing Plus Hookup Guide
Getting started with the nRF9160 from Circuit Dojo and SparkFun!
MicroMod Update Tool Hookup Guide
Follow this guide to learn how to use the MicroMod Update Tool to interact directly with the UART on the MicroMod Asset Tracker's SARA-R5. Using this board you can talk directly to the module using u-blox's m-center software as well as update the firmware using EasyFlash.
MicroMod Asset Tracker Carrier Board Hookup Guide
Get started with the SparkFun MicroMod Asset Tracker Carrier Board following this Hookup Guide. The Asset Tracker uses the u-blox SARA-R510M8S LTE-M / NB-IoT module to provide a host of data communication options.
SparkFun RTK Surveyor Hookup Guide
Learn how to use the enclosed RTK Surveyor product to achieve millimeter level geospatial coordinates.
Getting Started with the 8BitDo Bluetooth GamePads
Getting up and running with the sweet new 8BitDo game controllers!
MicroMod ESP32 Processor Board Hookup Guide
A short hookup guide to get started with the SparkFun MicroMod ESP32 Processor Board.
How to Build a DIY GNSS Reference Station
Learn how to affix a GNSS antenna, use PPP to get its ECEF coordinates and then broadcast your own RTCM data over the internet and cellular using NTRIP to increase rover reception to 10km!
Setting up a Rover Base RTK System
Getting GNSS RTCM correction data from a base to a rover is easy with a serial telemetry radio! We'll show you how to get your high precision RTK GNSS system setup and running.
How to Make a Magic Mirror with Raspberry Pi
Need a great project for your Raspberry Pi 4 kit? Use it to create a command center to display the weather, clock, your calendar, or even a news feed!
Wireless Remote Weather Station with micro:bit
Monitor the weather without being exposed to it through wireless communication between two micro:bits using the radio blocks! This is useful if your weather station is installed in a location that is difficult to retrieve data from the OpenLog. We will also explore a few different ways to send and receive data.
Assembly Guide for SparkFun JetBot AI Kit V2.0
Assembly Guide for the SparkFun JetBot AI Kit v2.0. This tutorial includes photos & comments to assemble the two-layer chassis & additional components unique to the JetBot kit.
Raspberry Pi 4 Kit Hookup Guide
Guide for hooking up your Raspberry Pi 4 Model B basic, desktop, or hardware starter kit together.
Secure DIY Garage Door Opener
Did you know that most garage doors are at risk of a roll jam attack? Here we make a DIY garage door remote-control system that is much more secure than most commercial-ready products using the latest in ECC cryptography.
SparkFun GPS NEO-M9N Hookup Guide
The u-blox NEO-M9N is a powerful GPS unit that comes with a chip antenna, SMA connector, and u.FL connector. We will quickly get you set up using the Qwiic ecosystem and Arduino so that you can start reading the output!
Getting Started with the Autonomous Kit for the Sphero RVR
Want to get started in robotics? Look no further than the SparkFun autonomous kit for the Sphero RVR! Whether you purchased the Basic or Advanced kit, this tutorial will get you rolling...
Advanced Autonomous Kit for Sphero RVR Assembly Guide
Get your Advanced Autonomous Kit for the Sphero RVR built up with this hookup guide!
Basic Autonomous Kit for Sphero RVR Assembly Guide
Get your Basic Autonomous Kit for Sphero RVR all hooked up with this guide!
Wireless Controlled Wearable EL Wire Dance Suit
In this tutorial, we will build an EL wire dance suit that can be controlled by a wireless glove controller!