Wireless

Transfer data between two or more devices without the use of wires! Some of these technologies include WiFi, cellular, Bluetooth, BLE, Zigbee, RFID, NFC, and GPS. Check out the following tutorials below to get started sending data into the air waves!

HX1 APRS Transmitter Hookup Guide

June 7, 2018
The HX1 is a low-power amateur radio transmitter that can be used to send data to the Automatic Packet Reporting System (APRS) network.

SparkFun Arduino ProtoShield Hookup Guide

May 17, 2018
The SparkFun Arduino ProtoShield PCB and ProtoShield kit lets you customize your own Arduino shield using whatever custom circuit you can come up with! This tutorial will go over its features, hardware assembly, and how to use the shield with an Arduino R3 footprint.

WiFi Controlled Robot

May 2, 2018
This tutorial will show you how to make a robot that streams a webcam to a custom website that can be remotely controlled.

Setting up a Raspberry Pi 3 as an Access Point

April 23, 2018
This guide will show you how to configure a Raspberry Pi as an access point and connect it to your local Ethernet network to share Internet to other WiFi devices.

Using Artnet DMX and the ESP32 to Drive Pixels

March 29, 2018
In this tutorial, we'll find out how to use Resolume Arena, a popular video jockey software, to control custom-made ArtNet DMX fixtures.

MIDI BLE Tutorial

February 22, 2018
Developing a bidirectional MIDI-BLE link with the nRF52832 Breakout.

Getting Started with Walabot

February 15, 2018
See through walls, track objects, monitor breathing patterns, and more using the power of radio frequency with the Walabot! In this tutorial, we will explore Walabot’s features using the Software Demo Kit (SDK) on Windows and the Application Programming Interface (API) on Linux-based distributions for embedded projects.

Using the PSoC 6 Pioneer Board with the Pioneer IoT Add-on Shield

February 1, 2018
Cypress's PSoC 6 Pioneer Board is a development tool for the powerful PSoC 6 processor. In this tutorial, we'll show you how to use the PSoC 6 Pioneer Board along with the SparkFun/Digi-Key Pioneer IoT Add-on Shield to send data to a Raspberry Pi via BLE or WiFi.

Wireless Audio Bluetooth Adapter w/ BC127

December 14, 2017
Build a custom wireless audio Bluetooth adapter using BlueCreation's BC127 and add it to your old speaker system!

Using Flask to Send Data to a Raspberry Pi

November 9, 2017
In this tutorial, we'll show you how to use the Flask framework for Python to send data from ESP8266 WiFi nodes to a Raspberry Pi over an internal WiFi network.

Wireless Motor Driver Shield Hookup Guide

August 17, 2017
Get started with the SparkFun Wireless Motor Driver Shield!

Getting Started with the Raspberry Pi Zero Wireless

July 13, 2017
Learn how to setup, configure and use the smallest Raspberry Pi yet, the Raspberry Pi Zero - Wireless.

ESP32 Thing Power Control Shield Hookup Guide

June 9, 2017
This tutorial shows you how to get started with the ESP32 Thing Power Control Shield.

Simultaneous RFID Tag Reader Hookup Guide

February 23, 2017
A basic guide to getting started with the RFID Tag Reader breakout and how to read and write multiple RFID tags over multiple feet!

RFID Basics

February 23, 2017
Dive into the basics of Radio Frequency Identification (RFID) technology.

Wireless Joystick Hookup Guide

January 5, 2017
A hookup guide for the SparkFun Wireless Joystick Kit.

Logging Data to Google Sheets with the Tessel 2

December 12, 2016
This project covers how to log data to Google Sheets two ways: using IFTTT with a web connection or a USB pen drive and "sneakernet" without.

Internet of Things Experiment Guide

November 23, 2016
The SparkFun ESP8266 Thing Dev Board is a powerful development platform that lets you connect your hardware projects to the Internet. In this guide, we show you how to combine some simple components to remotely log temperature data, send yourself texts and control lights from afar.

Serial Controlled Motor Driver Hookup Guide

November 17, 2016
Hookup guide for the Serial Controlled Motor Driver

nRF52832 Breakout Board Hookup Guide

November 17, 2016
How to hookup and program (in Arduino!) the nRF52832 Breakout -- a development board for Nordic's BLE/ANT/2.4GHz system on chip.

ESP32 Thing Hookup Guide

October 27, 2016
An introduction to the ESP32 Thing's hardware features, and a primer on using the WiFi system-on-chip in Arduino.

ReconBot with the Tessel 2

October 13, 2016
Build a robot with the Tessel 2 that you can control from a browser on your phone or laptop.

Environmental Monitoring with the Tessel 2

October 13, 2016
Build an air-conditioner monitoring device to collect environment information and store it in the cloud.

Sunrise Machine with the Tessel 2

October 13, 2016
Are you to sleepy to enjoy a sunrise on a brisk morning? Yeah...us too! No worries, with a Webcam, a Tessel 2 and a bit of code you can sleep in and catch the sunrise at your leisure with the Sunrise Machine.
Viewing 141 Wireless Tutorials. View All Tutorials.