Getting Started with the 8BitDo Bluetooth GamePads

≡ Pages
Contributors: Ell C

Introduction

One of the best things about this job is that I get to play with all the new products that come in. If you have a gamer in your family, listen up. The SN30 Pro Bluetooth Gamepad and the Lite Bluetooth Gamepad (which also comes in yellow) from 8BitDo are REALLY cool. They are after market game controllers that work on a variety of platforms, including the Switch, Windows, Linux, Raspberry Pi and possibly even on the iOS. Let's check 'em out!

8BitDo Lite Bluetooth Gamepad - Blue

WIG-17266
Retired

8BitDo Lite Bluetooth Gamepad - Yellow

WIG-17265
Retired

8BitDo SN30 Pro Bluetooth Gamepad

WIG-17264
Retired

Suggested Reading

MetaWatch Teardown and Arduino Hookup

Tearing down the nifty Bluetooth-enabled MetaWatch. Then building an Arduino sketch to control it.

Bluetooth Basics

An overview of the Bluetooth wireless technology.

Connectivity of the Internet of Things

An overview of the different protocols that can be used for the development of Internet of Things (IoT)-based projects.

Lite Hardware Overview

8BitDo's Lite Controller is a D-pad extravaganza. Who needs extra D-pads? I mean, who doesn't? They do have the "push button" functionality of the joystick but you have to press all four direction buttons down at the same time and it's hit or miss. That said, this controller is great for my kiddos - it extremely low profile, so it fits better into their smaller hands and thus it's easier for them to maneuver on. Let's have a look at some of the specs:

  • Compatibility: Windows, Steam, Switch
  • Dimension / Weight: 12066.216.2mm / 84g
  • Special Features:
    • Dual D-pads
    • Mode switch
    • Customizable turbo functionality ( X-input )
  • Connectivity:
    • Wireless Bluetooth®
    • USB-C
  • Battery Type / Battery Life:
    • 480mAh Li-on battery, rechargeable
    • 18 play hours with 1-2 hour charging time
  • Includes:
    • 8BitDo Lite Bluetooth gamepad
    • USB cable
    • Instruction manual

Diagram of 8bitdo Lite buttons

Battery and Charging

The Lite Controller comes with a standard USB-C cable and takes a couple hours to charge up. 8BitDo's documentation boasts about 18 hours of play once charged and while I haven't done any actual benchmarking on that, I will say that my kids have been playing on this thing for a week and I have yet to need to charge it. So it ain't too shabby.

Cons

All this low profile and portability comes at a bit of a cost. The 8BitDo Lite controller does not have an accelerometer or rumble feature, and there is no NFC reader. But! If you're a retro gamer who loves old school Zelda, Mario, etc, this is the controller for you.

Lite Hardware Pairing

Switch

The 8BitDo Lite is designed to work with the Nintendo Switch Lite. In fact, the colors of these controllers match the yellow and turquoise versions of the Switch Lite. If you're not color coordinated, do you even game, bro?

Let's pair. From your main screen, navigate to "Controllers".

Controllers option from the main screen of the switch

Select Change Grip/Order:

Change Grip screen

You'll see the following screen:

Pairing screen

Make sure the S/X button is moved to the "S" position like so:

S and X switch is in the top middle of the controller

Then press the Home button to turn the controller on:

Home button is on the lower right of the controller

On the bottom of the controller, you'll see LEDs turn on. Once the LEDs are lit up, press and hold the Pair button at the top of the controller for 3 seconds to enter pairing mode.

The Pair button is on the top of the controller to the right of the USB C input

The LEDs will run back and forth while pairing. Once pairing is complete, a single LED will light up and you'll see the following screen:

Screen showing controller paired

WOO GAME!

Gif playing Zelda on the Switch Lite with the Lite Controller

Windows

To pair your 8BitDo Lite Controller with Windows, start by navigating to your Bluetooth Settings from your Windows Start menu.

alt text

Click on Add Bluetooth or other device:

alt text

Within this dialog, select Bluetooth:

On windows, search for Bluetooth

Make sure you have the Select switch on the 8BitDo Lite Controller is set to "X".

Select switch is pushed to the right, selecting the X functionality

Press the Home button on the Lite Controller:

Home button on the Lite controller is highlighted

The LEDs on the bottom of the Lite controller will light up. Once you see this, press the "Pair" button on the top of the Lite Controller.

Pair button at the top of the controller is highlighted

In Windows, you should see the 8BitDo Lite show up. Go ahead and click on that.

Once paired, game on.

Playing Legend of Zelda, yo

WOOOOOO

SN30 Pro Hardware Overview

Got drift? The 8BitDo SN30 Pro Controller Gamepad is, in essence, a pro controller for the Nintendo Switch. Instead of going out and buying a new joycon, feel free to pick one of these bad boys up instead. Let's look at all the features!

  • Compatibility: Windows, Android, macOS, Steam, Switch, Raspberry Pi
  • Controller Mode: X-input, D-input, Mac mode, Switch mode
  • Special Features:
    • Rumble vibration
    • Motion controls
    • Turbo function
    • USB-C
  • Dimension / Weight: 14463.533mm / 114g
  • Connectivity:
    • Wireless Bluetooth®4.0
    • USB-C
  • Includes:
    • SN30 Pro G Classic
    • USB-C cable
    • Instruction manual

SN30 Pro Diagram

Battery and Charging

Like all of 8BitDo's controllers, this one uses a Universal USB-C and charges up in a couple of hours. 8BitDo mentions that a single charge can play for 16 hours, but I haven't tested that out. Uh... I'll do that now. BRB...

SN30 Pro Hardware Pairing

Switch

Like it's Lite brethren, the 8BitDo SN30 Pro is designed to work with the Nintendo Switch system. And just as similarly, the pairing process is fairly straightforward.

From your main screen, navigate to "Controllers".

Nintendo Main Screen

Select Change Grip/Order like so:

Change Grip Order screen

On the SN30 Pro Controller, press Y and Start simultaneously.

The Y button and the start button are highlighted

Once the LEDs are lit up, press and hold the Pair button at the top of the controller for 3 seconds to enter pairing mode.

Highlighted pair button

The LEDs will run back and forth while pairing. Once pairing is complete, the LED will light up.

Paired LED

Playtime!

alt text

If you're used to the Nintendo Switch Pro Wireless Controller, the SN30 Pro takes a hot minute to get used to. That said, all the functionality is there, and the price is pretty sweet.

Windows

Got Windoz gamez? Let's pair.

Go to the Start menu and navigate to your "Bluetooth" dialog.

From Start Menu, search up Bluetooth

Once your Bluetooth Dialog is open, click on Add Bluetooth or Other Device.

Windows add bluetooth menu

Choose your Bluetooth Type (top option):

windows add bluetooth dialog

On the SN30 Pro Controller, press X and Start simultaneously

X button and Start button are highlighted

Once the LEDs are lit up, press and hold the Pair button at the top of the controller for 3 seconds to enter pairing mode.

Highlighted pair button

In Windows, you should see the 8BitDo show up. Go ahead and click on that.

Connecting the 8BitDo Pro controller

The LEDs will run back and forth while pairing. Once pairing is complete, the LED will light up.

Paired LED

GAME ON.

Playing Amanita Design's Machinarum

Raspberry Pi

It isn't the goal of this tutorial to get you set up with a RetroPie gaming system. If you aren't already up and running, the documentation at RetroPie's First Installation Webpage is a great start.

Here are all the items I've used here:

That said, I did do a few mods after setup. At a broad stroke, here's where I went:

Initial Setup

For your intial setup of the SN30 Pro Controller, you'll wanna plug that bad boy in. I know, we want to go wireless. This is just the first go around.

  • Using the provided cable, plug the SN30 Pro into your RetriPie and then boot the Pi. You should see a Welcome screen like this:

Welcome screen

  • Press and hold down the "A" button on your Controller. The Welcome Screen should recognize your controller and show you the following:

Welcome screen with SN30 pro recognized

  • Configure your SN30 Pro Controller as prompted. Here's mine in progress:

Configuring SN30

Once you are finished, you should be taken to the RetroPie main window! WOOOOO!

Bluetooth

The easiest way to get gaming is to just leave your controller plugged in. But NO! We want to walk across the room to do something vital while continuing to play our game on the RetroPie! Let's take advantage of that fancy Bluetooth capability, shall we?

  • To start out, make sure you have a keyboard or other controller plugged in and ready to control and push buttons.
  • Get yourself to your RetroPie Main Screen and select "Bluetooth"

RetroPie Main Screen

  • Once you select Bluetooth, you'll see the following show up:

RetroPie Bluetooth Screen

  • On your SN30 Pro controller, hold down X and Start at the same time.

X and Start Buton highlighted

  • Once you see the LED blinking at the bottom, push the "Pair" button on the top.

Pair button highlighted at the top

  • If all goes well, you should have some lovely mac addresses and the 8Bitdo SN30 Pro!

Mac Address for 8BitDo SN30 Pro tutorial

  • Select "OK" and then 1 DisplayYesNo.

Display Yes No hightlighted

  • With any luck, you'll get a happily paired and functional 8Bitdo SN30 controller that you can now wander around the living room with!

Troubleshooting

I had some shenanigans happening with Bluetooth for a bit. I finally tracked it down to a mismatch between some updated vs non-updated dependencies, but I suggest that if you find that you cannot pair, verify the version of your controller's firmware, update all modules on your RetroPie, and if all else fails, uninstall and reinstall RetroPie (make sure you back up your ROMS!!!).

Resources and Going Further

We've covered some of the basics here and we'll add more as we can, but these little controllers have so much potential. Is it feasible to connect them to your other bluetooth devices? Can you drive around a robot? What else can you hack?

8BitDo resources:

Need inspiration for your next project? Check out some of these Bluetooth tutorials!

MIDI BLE Tutorial

Developing a bidirectional MIDI-BLE link with the nRF52832 Breakout.

SparkFun Edge Hookup Guide

Get to know your Edge board, including both the hardware features for you to utilize as well as how to get talking to it.

Nintendo Switch Macro Recording on the Raspberry Pi

Learn how to record and playback controller 'macros' for your Nintendo Switch using a Raspberry Pi, SparkFun Top pHAT, and Joycontrol.

SparkFun RTK Reference Station Hookup Guide

Setup the RTK Reference Station in minutes and start sending RTCM NTRIP corrections to your favourite caster.