Displays
Turn a Qwiic Ultrasonic Distance Sensor into a Garage Distance Sensor
This tutorial will take your SparkFun Qwiic Ultrasonic Distance Sensor to the next level by turning it into a parking distance sensor!
Display Distance Measurements On an OLED
This tutorial will take your SparkFun Qwiic Ultrasonic Distance Sensor to the next level by adding a cool little OLED display.
Fading with the MOSFET Power Switch and Buck Regulator
In this tutorial, we will slowly turn on the load and then slowly turn it off using the N-channel MOSFET.
SparkFun Arduino UNO R4 WiFi Qwiic Kit Hookup Guide
The SparkFun Arduino UNO R4 WiFi Qwiic Kit is a great way to get started with Arduino and the Qwiic-connect system - use this guide to get started!
Displaying Sensor Data with Bluetooth
In our previous Bluetooth tutorial called Sending Sensor Data Via Bluetooth, we showed how to display data from a triple axis accelerometer over the Arduino IDE’s serial monitor. Continuing off of the first tutorial, we are going to expand this project to include more capabilities for visualizing and interacting with your accelerometer data.
LiPo Fuel Gauge (MAX1704X) Hookup Guide
Monitor your LiPo battery with the LiPo fuel gauge! In this tutorial, we will be using the MAX17043 and MAX17048 to monitor a single cell, LiPo battery over the Arduino Serial Monitor. We will also connect a display to view the output without the need to connect the microcontroller to a computer.
Qwiic Kit for Raspberry Pi V2 Hookup Guide
Get started with the SGP40, BME280, VCNL4040, and microOLED via I2C using the Qwiic system and Python on a Raspberry Pi! Measure VOC Index, light, temperature, humidity, and pressure from the environment. Then display them on the microOLED, serial terminal, or the cloud with Cayenne!
Sending Sensor Data over LoRa
This tutorial will show you how setup a simple peer-to-peer connection to send and receive sensor data using LoRa.
MicroMod Qwiic Pro Kit Project Guide
The MicroMod Qwiic Pro Kit was designed to allow users to get started with Arduino without the need for soldering or a breadboard. We've included three inputs (a joystick, accelerometer, and proximity sensor) and one display that can be daisy chained to the MicroMod SAMD51 Processor Board.
Qwiic Digital Desk Sign with MicroMod
Make a Qwiic-enabled digital desk sign with a MicroMod SAMD51 Processor Board's USB Host and a USB keyboard!
Sending Sensor Data Over WiFi
This tutorial will show you how setup a simple peer-to-peer connection to send and receive sensor data between two ESP32 WiFi boards.
SparkFun Qwiic Alphanumeric Display Hookup Guide
A Hookup Guide to get you started with the Qwiic Alphanumeric Display.
Qwiic SHIM Kit for Raspberry Pi Hookup Guide
Get started with the Serial LCD with RGB backlight and 9DoF IMU (ICM-20948) via I2C using the Qwiic system and Python on a Raspberry Pi! Take sensor readings and display them in the serial terminal or SerLCD.
SparkFun MicroMod Input and Display Carrier Board Hookup Guide
A short Hookup Guide to get started with the SparkFun MicroMod Input and Display Carrier Board
The ClockClock Project
Tell the time with this fantastic Alchitry project using clocks to make a clock!
Qwiic GPS Clock
What time is it? Time for you to... Qwiic-ly build a GPS clock and output it to a display! This project provides you with the current date and time using GPS satellites. Read the date and time as a digital or analog clock. Or even configure the clock for military, your time zone, or automatically adjust the time for daylight savings time!
Qwiic Digital Indoor Thermometer
Qwiic-ly build a digital indoor thermometer to measure the ambient temperature of the room and display it using an OLED on an I2C bus!
Working with Qwiic on a Jetson Nano through Jupyter Notebooks
We created a few Jupyter Notebooks to make using our Qwiic boards with your Jetson Nano even easier!
SparkFun Top pHAT Hookup Guide
The pHAT to sit above your other HATs. Does that make it the "king" of the pHATs?
This guide will help you get started using the Top pHAT with the Raspberry Pi.
Qwiic Pro Kit Project Guide
The Qwiic Pro Kit was designed to allow users to get started with Arduino without the need for soldering or a breadboard. We've included three inputs (a joystick, accelerometer, and proximity sensor) and one display that can be daisy chained to the RedBoard Turbo (SAMD21) Development Board.
SparkFun Inventor's Kit Experiment Guide - v4.1
The SparkFun Inventor's Kit (SIK) Experiment Guide contains all of the information needed to build all five projects, encompassing 16 circuits, in the latest version of the kit, v4.1.2 and v4.1.
Basic Character LCD Hookup Guide
Liquid crystal displays (LCDs) are a great way to output a string of words or sensor data to a display for visual feedback. In this tutorial, we'll learn about LCDs, how to print a string of words to a 16x2 basic character LCD and create custom characters.
Displaying Your Coordinates with a GPS Module
This Arduino tutorial will teach you how to pinpoint and display your GPS coordinates with a press of a button using hardware from our Qwiic Connect System (I2C).
TFT LCD Breakout 1.8in 128x160 Hookup Guide
This TFT LCD Breakout is a versatile, colorful, and easy way to experiment with graphics or create a user interface for your project.
Beginner Parts Kit Identification Guide
The essential parts for beginning (or even experienced) hobbyists that gives you all of the basic through-hole components you will need to get started playing with embedded projects. We'll identify a few parts in the kit and provide a few basic circuits to get started!
Transparent Graphical OLED Breakout Hookup Guide
The future is here! Our Qwiic Transparent Graphical OLED Breakout allows you to display custom images on a transparent screen using either I2C or SPI connections.
Qwiic Transparent OLED HUD Hookup Guide
Learn how to connect that sweet transparent OLED.
Everything You Should Know About HyperDisplay
This is a tutorial to go in-depth about the SparkFun HyperDisplay Arduino Library.
Getting Started with the SmartLED Shield for Teensy
In this tutorial, we will connect different RGB LED matrix panels to PixelMatix's SmartLED shield and Teensy.
How to Run a Raspberry Pi Program on Startup
In this tutorial, we look at various methods for running a script or program automatically whenever your Raspberry Pi (or other Linux computer) boots up.
DIY Light Sculpture
In this digital fabrication project featuring 3D printing, laser cutting, and DIY electronics, you will build a beautiful design object for your desktop or night stand.
AVR-Based Serial Enabled LCDs Hookup Guide
The AVR-based Qwiic Serial Enabled LCDs are a simple and cost effective solution to include in your project. These screens are based on the HD44780 controller, and include ATmega328P with an Arduino compatible bootloader. They accept control commands via Serial, SPI and I2C (via PTH headers or Qwiic connector). In this tutorial, we will show examples of a simple setup and go through each communication option.
Flexible Grayscale OLED Hookup Guide
Figure out how to get images displaying on your new flexible OLED screen.
PIC-Based Serial Enabled Character LCD Hookup Guide
The PIC-based serial enabled character LCD backpack is a simple and cost effective solution for interfacing to character Liquid Crystal Displays (LCDs) based on the HD44780 controller. The backpack simplifies the number of wires needed and allows your project to display all kinds of text and numbers.
IoT Power Relay
Using the ESP32 to make a web-configured timed relay.
Qwiic Micro OLED Hookup Guide
Get started displaying things with the Qwiic Micro OLED.
Endless Runner Game
We make a simple side-scrolling endless runner game using parts from the SparkFun Inventor's Kit v4.0.
SparkFun Inventor's Kit Experiment Guide - v4.0
The SparkFun Inventor's Kit (SIK) Experiment Guide contains all of the information needed to build all five projects, encompassing 16 circuits, in the latest version of the kit, v4.0a.
TeensyView Hookup Guide
A guide to using the TeensyView OLED board to display text and graphics.
Wireless Joystick Hookup Guide
A hookup guide for the SparkFun Wireless Joystick Kit.
MicroView Hookup Guide
A quick tutorial to get you up and running with your MicroView Development Board.
Experiment Guide for the Johnny-Five Inventor's Kit
Use the Tessel 2 and the Johnny Five Inventors kit to explore the world of JavaScript enabled hardware through 14 awesome experiments!
Blynk Board Project Guide
A series of Blynk projects you can set up on the Blynk Board without ever re-programming it.
SparkFun LED Array (8x7) Hookup Guide
Getting started with the Charlieplexed 8x7 LED array.
PicoBuck Hookup Guide v12
The PicoBuck board is a high-efficiency three-channel constant-current LED driver.
Using an LCD on the Edison
How to connect an LCD controlled by an ILI9341 driver to the Intel® Edison.
Interactive Smart Mirror
Build a smart mirror that displays weather data using the Intel® Edison.
Button Pad Hookup Guide
An introduction to matrix scanning, using the SparkFun 4x4 Button Pad.
FemtoBuck Constant Current LED Driver Hookup Guide v13
The FemtoBuck board is a high-efficiency, single-channel constant-current LED driver.
MLX90614 IR Thermometer Hookup Guide
How to use the MLX90614 or our SparkFun IR Thermometer Evaluation Board to take temperatures remotely, over short distances.
SparkFun Inventor's Kit for Photon Experiment Guide
Dive into the world of the Internet of Things with the SparkFun Inventor's Kit for Photon.
Photon OLED Shield Hookup Guide
The Photon OLED Shield has everything you need to add a small yet crisp OLED screen to your Photon projects. This hookup guide will show you how to get started.
Large Digit Driver Hookup Guide
Getting started guide for the Large Digit display driver board. This tutorial explains how to solder the module (backpack) onto the back of the large 7-segment LED display and run example code from an Arduino.
SparkFun Inventor's Kit for MicroView
The SparkFun Inventor's Kit for MicroView follows our tried and true inventor's kit model, bringing you 11 simple yet fun experiments to introduce you to the SparkFun MicroView.
SparkFun Blocks for Intel® Edison - OLED Block
A quick overview of the features of the OLED Block for the Edison.
Alphanumeric GPS Wall Clock
This is a GPS controlled clock - a clock you truly never have to set! Using GPS and some formulas, we figure out what day of the week and if we are in or out of daylight savings time.
Micro OLED Breakout Hookup Guide
Learn how to hook up the Micro OLED breakout to an Arduino. Then draw pixels, shapes, text and bitmaps all over it!
RGB Panel Jumbotron
This tutorial will show you how to combine a webcam, a 32x32 RGB LED panel, and a Teensy 3.1 to stream video from the webcam, pixelate it, and display it on the LED panel - LIVE.
Hackers in Residence - The ElectricBone
Drum machines and keyboards have been the standard for making digital music, but how do you make electronic music if you're trained to play the trombone? One of our Hackers in Residence, Carlos Mello, took it upon himself to find a solution to that very question.
ELasto-Nightlight
Fear the dark no longer with this ELastoLite nightlight.
Interactive Hanging LED Array
Learn how we converted 72 lightbulbs into an interactive LED array for our conference room.
MYST Linking Book
Create your own Linking Book from the classic computer game, MYST
Das Blinken Top Hat
A top hat decked out with LED strips makes for a heck of a wedding gift.
Dot/Bar Display Driver Hookup Guide
How to hook up the LM3914 or LM3916 to drive a 10-LED display with a lone analog signal.
Reaction Timer
Demonstrate mental chronometry with this simple reaction timer!
Vernier Photogate
Vernier Photogate Timer -- using the Serial Enabled LCD Kit.
Quick Illuminated Boxes
A quick tutorial to show you how to add LEDs to gift or holiday bags or boxes.
RGB Panel Hookup Guide
Make bright, colorful displays using the 32x16, 32x32, and 32x64 RGB LED matrix panels. This hookup guide shows how to hook up these panels and control them with an Arduino.
Serial Graphic LCD Hookup
Learn how to use the Serial Graphic LCD.
Graphic LCD Hookup Guide
How to add some flashy graphics to your project with a 84x48 monochrome graphic LCD.
ELastoLite Hookup Guide
Everything you need to setup a circuit using ELastoLite super flexible EL Panels from Oryon Technologies.
LED Light Bar Hookup
A quick overview of SparkFun's LED light bars, and some examples to show how to hook them up.
Using the Serial 7-Segment Display
How to quickly and easily set up the Serial 7-Segment Display and the Serial 7-Segment Display Shield.
Dungeons and Dragons Dice Gauntlet
A playful, geeky tutorial for a leather bracer that uses a LilyPad Arduino, LilyPad accelerometer, and seven segment display to roll virtual 4, 6, 8, 10, 12, 20, and 100 side dice for gaming.
WS2812 Breakout Hookup Guide
How to create a pixel string with the WS2812 and WS2812B addressable LEDs!
Using OpenSegment
How to hook up and use the OpenSegment display shield. The OpenSegment is the big brother to the Serial 7-Segment Display. They run on the same firmware, however the OpenSegment is about twice as big.