EL Wire Hoodie

≡ Pages
Contributors: bboyho

Introduction

The design and build time of this project depends on your experience manually sewing, the length of EL wire used, and where you are sewing it to. This can take about ~1 - 3 hours if you are following the edges of a hoodie.

In this tutorial, we will sew standard EL wire onto a hoodie.

EL Hoodie

Required Materials

To follow along with this tutorial, you will need the following materials. We will be using a standard EL wire on the hoodie. You may not need everything, depending on what you have and your setup. Add it to your cart, read through the guide, and adjust the cart as necessary.

Panasonic Alkaline Battery - AA

PRT-15201
$0.60

EL Wire - White 3m

COM-10197
Retired

EL Inverter - Battery Pack

COM-11222
Retired

Tools

At a minimum, you will need a needle. If you are making an extension cable, you will need a soldering iron, solder, and general soldering accessories.

Needle Set

TOL-10405
$2.25

You Will Also Need

  • Hoodie
  • Clear Thread or Fishing Line
  • Binder Clips, Pins, or, Tape
  • Scissors

Suggested Reading

If you aren’t familiar with the following concepts, we recommend checking out these tutorials before continuing.

Getting Started with Electroluminescent (EL) Wire

This guide will help you get started with electroluminescent (EL) wire, tape, panel, chasing wire, and bendable wire to let your project glow!

Planning a Wearable Electronics Project

Tips and tricks for brainstorming and creating a wearables project.

How to Make a Custom EL Wire Extension Cable

In this tutorial, we will make a custom EL Wire extension cable as an alternative to splicing wire.

Prepare the EL Wire

Testing the EL Wire and EL Inverter

Before sewing the EL wire to a piece of clothing, make sure to test it out to see if it is functioning. To test, connect the EL wire to an inverter. In this case, we are using AA batteries and the 3V EL inverter battery pack.

Insert EL Wire's JST Connector into EL Battery Pack

With the battery in the EL inverter battery pack, press the button to test. If the EL wire lights up, both the EL wire and EL inverter are good to go!

EL Wire Lit Up

Planning the Path

Plan out where to add EL wire. While you can sew the EL wire on the arms, it will be harder due to the amount of room available to work with in the arm. The easiest would be to follow the edge of the hoodie. To hold down the EL wire when sewing, we will be using binder clips. Depending on what you have, you could also try to use pins or tape. Place the EL wire into the binder clip and clamp it down against the fabric. Make sure to avoid clamping the EL wire down where the binder clip pinches as this can damage the corona wires.

EL Wire Held to the Hoodie with a Binder Clip

In this case, all 3 meters of EL wire were used starting under the pocket, running up the side of the zipper, around the shoulders, up to the brim of the hood, around the shoulders, down the zipper, and ending at the pocket on the other side. Make sure to avoid sharp bends. If you decide to use a shorter length, you can cut the EL wire. Just make sure to re-seal the cut end with hot glue, otherwise you could end up getting a good jolt..

Front of EL Hoodie with Binder Clips Back of EL Hoodie with Binder Clips

Having a hard time seeing the binder clips and EL wire? Click on the images for a closer look

Prepare the Needle and Thread

For this tutorial, we will double up the clear thread. Prepare your needle and thread by inserting the end of the clear thread through the eye (opening) of the needle and pull it through. Cut about an arms length of thread (approximately 2 feet long) to work with. Tie the two ends of the fishing wires into a knot. You may need to use the needle to help guide the knot close to the end of the thread.

Pulling the Knot Closer To the End Using a Needle

Repeat the steps again for a second knot. Cut of any excess tail left over.

Clear Thread Tied in a Knot

Sewing EL Wire

Start sewing at the EL wire's heat shrink and tie a knot around the EL wire. Continue making a loop around the EL wire to hold it down. When sewing with clear thread, make sure to pull the thread all the way through since the thread is slippery when sewn in certain fabrics. Be careful not to sew the front and back of the hoodie together. Also, ensure that the distance between each stitch is not too long. About 0.5" to 1.0" is a good stitch. Longer stitches can cause the EL wire to snag or become loose when wearing the EL hoodie.

Start Sewing at the Heat Shrink of the EL Wire

After about 5x stitches, loop back through the last stitch with an overhand knot to lock the thread in and prevent it from sliding.

Tying a Knot After 5x Stitches to Prevent the Clear Thread from Sliding

Continue sewing and remove any binder clips holding the EL wire down against the fabric. When sewing EL along the zipper, avoid looping the thread against the zipper.

Sewing EL Wire Beside Zipper

While sewing the EL wire, try holding the EL down against the fabric using your non-dominant hand. Pinch below the area that you are sewing using your thumb and ring finger. Then pinch above the area that you are sewing using your index and middle finger. This keeps the center area (where you will be working with the needle) taut so that it is easier to sew.

Repeat the Steps Outlined Above

Once you begin to run out of thread to work with, tie the clear thread down against the fabric. Then repeat the steps outlined above with another piece of clear thread.

Clear Thread Tied in a Knot

When you are finished sewing the EL wire down, make a loop with the end of the EL wire cable and sew the wire down for strain relief. Make sure this loop is beyond the heat shrink as the connection at the heat shrink is sensitive to bending.

Strain Relief

Plug the EL wire back into the EL inverter to test it out. If it lights up, you are good to go! Place the EL inverter in a pocket or clip to a belt to enjoy! If you are using an EL inverter battery pack, you may want to make an extension cable.

EL Wire in Pocket

Remember, EL wire works best in low light. It may be hard to see in daylight or in rooms with sources of light.

EL Hoodie in Room with Sources of Light

Front EL Wire Hoodie Low Light Back EL Wire Hoodie Low Light
Front EL Wire Hoodie Low Light Back EL Wire Hoodie Low Light

Different Hoodie Sizes

Remember what I said about the size of the hoodie? Different hoodie sizes will require different lengths of EL wire - this variation can cause the EL wire to not start or end where you expect it to. Note the difference in the image in the bottom right.

Youth Medium Hoodie with EL Wire Youth Large Hoodie with EL Wire
Youth Medium with EL Wire Youth Large with EL Wire

Sewing Into The Arms

Looking for a challenge? Sewing EL wire onto the arms can be difficult depending on the fabric being used and the amount of space you have to work with. Three pieces of corrugated cardboard were custom cut to fit inside a hoodie's arm to help with sewing. To assemble, cut half way into the cardboard about 0.5"-1"" away from the edge. It does not have to be perfect. Slide the cardboard pieces together and hot glue the joints.

Front View of Cardboard Braket

Front View of Cardboard Bracket

Trim down the edges as necessary to slide into the arm with ease.

Top-Side View of Cardboard Bracket Front-Side View of Cardboard Bracket
Top-Side View Front-Side View

Once cut and assembled, insert the bracket into an arm.

Cardboard Bracket In Arm

Clamp the fabric material down against the cardboard bracket and ensure that the fabric material is taut. Continue sewing clear thread down/up the arm.

Binder Clips Clipping Down Fabric Against Cardboard Bracket

The following shows standard EL wire sewn into the arms of an adult medium hoodie.

Front View Adult Medium with EL Wire Sewn into Arms Front and Side View Adult Medium with EL Wire Sewn into Arms
Front View with EL Wire Sewn into Arms Front-Side View with EL Wire Sewn into Arms

Resources and Going Further

Need some inspiration for your next project? Check out some of these related tutorials:

EL Wire Light-Up Dog Harness

Learn how to create a light-up dog harness using EL wire for when you need to take your four-legged friend for a walk in the dark.

Heartbeat Straight Jacket

An EL project that displays one person's heartbeat on another person's costume.

Sound Reactive EL Wire Costume

Learn how to make your EL wire costumes sound reactive in this project tutorial.

Prototype Wearable LED Dance Harness

A project tutorial to add an extra effect for dancers performing a choreographed piece. The harness can be added quickly under a costume.

Looking for more ideas, check out these related blog posts: