LED Robot Pop Up Card

≡ Pages
Contributors: Gella

Introduction

Craft a paper circuit pop up card with a cycling RGB LED, battery, and copper tape. If you've built any of our paper circuit pop up cards before, feel free to jump right in to following the template. If this is your first paper circuit, we'll walk you through the process.

alt text

Suggested Reading

If you are brand new to working with electronics, here's some helpful reading to check out:

Materials and Tools

Here is a list of all the materials and tools you'd need to follow along:

Notes:

Additional Materials:

  • Cardstock (2-3 pieces)
  • 3/4" Square of Vellum, wax paper, rice or parchment paper- creates a nice diffused effect for the LED to shine through the robot's heart
  • Clear Tape
  • Gluestick/Glue
  • Scissors/Hobby Knife
  • Needle Nose Pliers
  • Decorating Supplies - stickers, markers, or paints to embellish your designs

Step 1: Print Template

Right-click the images below, and choose “Save Link As” to download the templates to your computer. Each file has a circuit template page and a pop up template page.

Robot Template - 2 pages

alt text

If you have a Silhouette Electronic Cutter, click here to download a Silhouette Studio file for the pop up layer

Print your templates out on cardstock. If needed, adjust your printer's margins, or choose 'Fit to Page' in the print settings. The card template is slightly smaller than the paper, so make sure to cut along the black border for the final card size.

Set the pop up page aside for now. We'll build our circuit first and then assemble the pop up once the electronics are all installed.

Step 2: Create Copper Traces

Time to create a path for our electricity with copper tape. Each template has icons to help guide you in constructing the circuit.

alt text

Line A

Take a look at the template and find the circle marked A. Peel away a few inches of the paper backing from the copper tape and stick down along the grey line.

alt text

Cut when you reach the scissors icon.

Line B

Next we'll place tape along Line B which includes a corner. To keep a solid connection of copper around corners, we'll be using a folding technique to press the tape into shape.

Start by sticking the copper tape down until you reach the corner, then fold the tape backward on itself. Use a fingernail or pen to give it a good crease at the edge.

alt text

Then carefully move the tape down around the corner - you should see the fold forming - and press down flat against the paper. The neatness of the fold doesn't matter that much, it will be covered by your pop up in the end. Finally, cut the tape when you reach the scissors icon.

alt text

alt text

alt text

Line C

The last copper tape line will also form a battery holder. We'll start by folding 1/2" of copper tape onto itself, sticking the adhesive sides together to form a flap.

alt text

This allows the top of the copper to fold down over the coin cell battery - the positive side of the battery is the top and negative side is the bottom, which allows us to create a 'battery sandwich' with copper tape touching each side.

alt text

See the diagrams below to explore how this method works. We won't be installing the battery until the end of our project, so set that aside for now. Fold the card in half along the dotted center line before moving onto the next step.

alt text

alt text

Step 3: Prepare and Place LED

Before prepping the LED, fold the card in half along the dotted line to save the hassle of trying to make a neat fold once there are components sticking up from the paper.

Now that our copper is in place, time to add the LED. The template has an LED symbol which shows shaped wires - we use this method to help us remember which side is positive and negative on the LED.

Read more about LED polarity in our Light-emitting Diodes (LEDs) Tutorial .

alt text

Here are directions for bending a 3mm LED to prepare it for our circuit.

Note: the cycling RGB LEDs have a clear bulb - we used a yellow LED for these photos.

Using pliers (or your finger), bend the longer leg of the LED flat and then form into a zig zag shape. Be careful not to break the wire by bending back and forth over the same joint too many times.

alt text

Next, bend the other leg flat and curl into a spiral. Use the end of the pliers to lightly grab the end of the wire and curl around the tool.

alt text

Once all shaping is complete, place the LED on a table or flat surface to make sure it sits flat and upright. If not, make any adjustments now.

Tape Down LEDs

Line up the positive lead with the copper tape marked + and the negative with -. Use clear tape over the leads to hold down to the copper.

alt text

Step 4: Attach Button

alt text

Next, we'll place the LilyPad button over the oval icon on the template facing up. It doesn't matter which side touches postive and negative. Make sure the conductive pads on the bottom of the button touch the copper tape, then tape down the ends with clear tape. Be careful not to tape directly over the push part of the button, or it may interfere with the ability to press it. You can also use a LilyPad switch instead of a button - the installation is the same.

alt text

Step 5: Insert Battery

Once all the components are installed, it's time to test our circuit by adding a battery. Carefully slip the battery underneath the copper tape flap we made earlier, and center it inside the circle icon. Make sure the positive side of the battery (top, marked with the battery model and +) is facing up. Press the copper over the battery, and tape with clear tape.

alt text

Now, press the button, and the LED should light up!

alt text

alt text

Troubleshooting

  • Check the tape connections - use your nails or a pencil to make sure the tape is firmly adhering the components to the copper tape.
  • Check the battery - make sure it is sandwiched firmly between the top and bottom copper tape lines and that the top copper is not accidentally touching the bottom of the battery.
  • Check the wires of the LED - double check that they weren't accidentally broken while bending them into shapes with pliers.

Here is what the finished circuit should look like:

Step 6: Prepare Pop Up

Use a hobby knife to cut along the lines of the pop up template. Tape or glue a piece of vellum or a semi-transparent paper to the back of robot over the heart to diffuse the light from the RGB LED.

alt text

To pop the robot up from the page, first turn paper over to the front side (the heart should be on the right side of the robot). Carefully fold the robot's feet toward you.

alt text

Rotate the card so the robot's head is facing you and crease the top fold toward you and second fold away from you.

alt text

alt text

To finish the pop up, fold the card in half - making sure not to accidentally fold the legs. The robot should fold up neatly in the card.

alt text

alt text

To attach to your circuit, place the robot pop up page over the copper tape circuit and adjust as necessary so the LED shines through the robot's heart. Trim edges if needed and use glue or tape to fix the corners down. Be careful not to glue under the pop up pieces or they may stick down when closed.

Step 7: Decorate and Customize

After assembling, use a marker or stickers to indicate where the button should be pressed on the top layer. Add extra decorations and embellishments to make your project unique!

alt text

alt text

Resources and Going Further

Things to try:

  • Try these techniques with other pop up designs or create your own - can you figure out how to adapt the copper tape path to fit your card choice?
  • Get crafty with stickers, paint, or markers after you've built your card to customize it even more.

Further Reading: