Heating Pad Hand Warmer Blanket

≡ Pages
Contributors: HelloTechie

What Are Heating Pads Good For?

There are a lot of great projects you can use heating pads (5x10cm and 5x15cm) in, ranging from warming gloves, slippers, a blanket, or anything you want to keep nice and warm. Got a beard mask you want to make toasty? Do beards need to be warmer? Not sure. Would it be a fun project? Definitely.

Heating Pad - 5x10cm

COM-11288
$4.95

Heating Pad - 5x15cm

COM-11289
$5.95

What Parts Should You Consider Getting for Your Project?

You can go as simple as getting the appropriate power supply and a heating pad. One heating pad is rated for 5V, and draws about 600mA. If you want to add a form of logic or control to your circuit, such as interfacing with sensors, the easiest way is to add a microcontroller/development board to your project. You will also need some wire and transistor to control the heating pad if you are using a microcontroller. Check the wishlist in the next section for more details on the products used in this tutorial.

Tools

You will need sewing needles, a soldering iron, solder, and general soldering accessories.

Solder Lead Free - 100-gram Spool

TOL-09325
$24.95

Needle Set

TOL-10405
$2.25

Weller WLC100 Soldering Station

TOL-14228
Retired

Suggested Reading

If you aren’t familiar with the following concepts, we recommend checking out these tutorials before continuing.

DIY Project Idea: Hand Warmer Blanket

A blanket project with two heating pads to keep your hands warm when you are on the computer/notebook/tablet/phone/playing chess/all other activities.

Required Materials

There are a lot of parts on this list that can be exchanged for alternate parts, or that aren't needed at all, depending on what type of setup you want. To follow along with this project, you will need the following materials. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

You could use a 3.7 LiPo battery to power both the LilyPad USB board and the heating pads. Remember: You will still need a MOSFET, because having two heating pads will draw more current then the LilyPad pins can handle. This option is nice, since you can use the LilyPad to charge the LiPo battery when the heating pad isn't in use. The draw back to using a 3.7v LiPo battery is that the heating pads won't get as warm as they would with a 5v (or higher) power supply.

In this setup, we use the LilyPad USB, because you won't have to get an extra FTDI basic for an USB connection.

Directions

The first step is to select your fabric. When picking a fabric, you want to consider the following:

  • Is the pattern on the fabric going to work, or look out of place? If you are going Snuggie style, will you need to add extra fabric for the arms?
  • On what level of awesome is the fabric you are selecting? Meaning, how fast are you going to get sick of looking at it?
  • Is the fabric thick, cozy, and going to keep the rest of your body warm? Sheer, light fabrics don't help to keep you warm during the winter months.

In the video below, you'll see that you can get as weird as you want when customizing your blanket:

For the example in the video, extra fabric and button snaps were sewn on the back of the blanket for easy removal for washing.

Heating pad blanket with sewing snaps

If you don't have a sewing machine, or don't want to sew, you can do a No-Sew blanket and be creative when adding a pouch that holds your heating pads and circuit. No-Sew blanket tutorials

Circuit

Here is a diagram of the circuit setup:

Circuit Heating Pads Arduino LEDs MOSFET

Having a hard time seeing the circuit? Click the image for a closer look.

Example Code

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE.
language:c
  /*

 Heating Pad Hand Warmer Blanket Code Example
  SparkFun Electronics, Pamela, 1/24/2013
  Beerware License

  Hardware Connections:
  -led1 = D9;
  -led2 = D10;
  -led3 = D11;
  -button = D2;
  -Mofset = D3;

  Usage: 
  Hit the switch to power, hit the button to adjust how warm the heating elements get, and three LEDs will indicate low, medium, and high levels. 
 */

int btnPin = 2;
boolean btnPressed = false;
int fetPin = 3;
int led1 = 9;
int led2 = 10;
int led3 = 11;
int mode;

void setup() {                
  // initialize the digital pin as an output.
  pinMode(btnPin, INPUT_PULLUP);  //set internal pull-up resistor for button
  pinMode(fetPin, OUTPUT);  
  pinMode(led1, OUTPUT);  
  pinMode(led2, OUTPUT);  
  pinMode(led3, OUTPUT);  
}

// the loop routine runs over and over again forever:
void loop() {
  //Increment mode on depress, unless mode = 3, then reset to 0
  if (btnPressed && digitalRead(btnPin) == LOW)
    mode = mode == 3 ? 0 : mode + 1;
  //Assign button state
  btnPressed = digitalRead(btnPin);
  switch (mode)
  {
    case 0:
      analogWrite(fetPin, 0); //off
      digitalWrite(led1, LOW);
      digitalWrite(led2, LOW);
      digitalWrite(led3, LOW);
      break;
    case 1:
      analogWrite(fetPin, 85); //33% duty cycle
      digitalWrite(led1, HIGH);
      digitalWrite(led2, LOW);
      digitalWrite(led3, LOW);
      break;
    case 2:
      analogWrite(fetPin, 170); //66% duty cycle
      digitalWrite(led1, HIGH);
      digitalWrite(led2, HIGH);
      digitalWrite(led3, LOW);
      break;
    case 3:
      analogWrite(fetPin, 255); //100% duty cycle
      digitalWrite(led1, HIGH);
      digitalWrite(led2, HIGH);
      digitalWrite(led3, HIGH);
      break;
  }
}

There you go! As with any DIY project, you should always customize and tweak what you want for maximum awesomeness.

Resources and Going Further

For more information about the heating pads, check out the resources below:

Need some inspiration for your next project? Check out some of these related tutorials:

21st Century Fashion Kit: Electrochromatic Circuits

Diana Eng walks you through a magically appearing design made with an thermochromatic pigment.

DIY Heated Earmuffs

Embedded with heating pads and four Neopixel rings, these earmuffs do more than your average winter accessory to keep you warm while still looking good.

Or try controlling thermochromatic pigment with the heating pads.

If you liked this project, we recommend checking out our older tutorials related to e-textiles: