EL Wire Pants
Introduction
In this tutorial, we will sew standard EL wire onto a pair of pants.
Required Materials
To follow along with this tutorial, you will need the following materials. We will be using standard EL wire on the pants. You may not need everything, depending on what you have and your setup. Add it to your cart, read through the guide, and adjust the cart as necessary.
EL Wire - White 3m
COM-10197EL Inverter - Battery Pack
COM-11222
Looking for EL chasing or bendable EL wire? Click on the button below for additional options in the catalog!
EL Chasing, Bendable, & Types of EL Products
Tools
At a minimum, you will need a needle. If you are making an extension cable, you will need a soldering iron, solder, and general soldering accessories.
You Will Also Need
- Pants
- Clear Thread or Fishing Line
- Binder Clips, Pins, or, Tape
- Scissors
Suggested Reading
If you aren’t familiar with the following concepts, we recommend checking out these tutorials before continuing.
Getting Started with Electroluminescent (EL) Wire
Planning a Wearable Electronics Project
How to Make a Custom EL Wire Extension Cable
Prepare the EL Wire
Testing the EL Wire and EL Inverter
Before sewing the EL wire to a piece of clothing, make sure to test it out to see if it is functioning. To test, connect the EL wire to an inverter. In this case, we are using AA batteries and the 3V EL inverter battery pack.
With the battery in the EL inverter battery pack, press the button to test. If the EL wire lights up, both the EL wire and EL inverter are good to go!
Planning the Path
Plan out where to add EL wire. To hold down the EL wire when sewing, we will be using binder clips. Depending on what you have, you could also try to use pins or tape. Place the EL wire into the binder clip and clamp it down against the fabric. Make sure to avoid clamping the EL wire down where the binder clip pinches as this can damage the corona wires.
In this case, all 3 meters of EL wire were used starting by the left pocket, running down the side of the leg, and back up to the waist. The EL wire then followed the waist in the back before running down the right side of the leg and back up to the right pocket. The length along each side was adjusted to be symmetric.
Prepare the Needle and Thread
For this tutorial, we will double up the clear thread. Prepare your needle and thread by inserting the end of the clear thread through the eye (opening) of the needle and pull it through. Cut about an arms length of thread (approximately 2 feet long) to work with. Tie the two ends of the fishing wires into a knot. You may need to use the needle to help guide the knot close to the end of the thread.
Repeat the steps again for a second knot. Cut of any excess tail left over.
Sewing the EL Wire
Start sewing by the EL wire's heat shrink and tie a knot around the EL wire. Continue making a loop around the EL wire to hold it down. When sewing with clear thread, make sure to pull the thread all the way through since the thread is slippery when sewn in certain fabrics. Be careful not to sew the front and back of the pants together. Also, ensure that the distance between each stitch is not too long. About 0.5" to 1.0" is a good stitch. Longer stitches can cause the EL wire to snag or become loose when wearing the EL pants.
After about 5x stitches, loop back through the last stitch with an overhand knot to lock the thread in and prevent it from sliding.
Once you begin to run out of thread to work with, tie the clear thread down against the fabric. Then repeat the steps outlined above with another piece of clear thread.
When you are finished sewing the EL wire down, make a loop with the end of the EL wire and sew the wire down for strain relief. Make sure this loop is beyond the heat shrink as the connection at the heat shrink is sensitive to bending.
Plug the EL wire back into the EL inverter to test it out. If it lights up, you are good to go! Place the EL inverter in a pocket or clip to a belt to enjoy! If you are using an EL inverter battery pack, you may want to make an extension cable.
Remember, EL wire works best in low light. It may be hard to see in daylight or in rooms with sources of light.
![]() |
![]() |
| EL in Light | EL in the Dark |
Different Pant Sizes
Remember what I said about the size of the pants? Different pant sizes will require different lengths of EL wire - this variation can cause the EL wire to not start or end where you expect it to. Note the difference in the the image compared to the youth sized pants.The beginning of the EL wire was sewn further down the pant leg and followed a narrow path as it headed back up toward the waist.
Resources and Going Further
Need some inspiration for your next project? Check out some of these related tutorials:
EL Wire Light-Up Dog Harness
Heartbeat Straight Jacket
Sound Reactive EL Wire Costume
Prototype Wearable LED Dance Harness
EL Wire Hoodie
Looking for more ideas, check out these related blog posts: