Qwiic
The SparkFun Qwiic Connect System is an ecosystem of I2C sensors, actuators, shields, and cables that make prototyping faster and less prone to error. Get it? It's quick Qwiic! The following tutorials tagged takes advantage of the Qwiic system.
Build Your Own High-Concentration CO2 Detector
The SparkFun STC31 CO2 Sensor can accurately measure CO2 concentrations up to 100% with high repeatability and long-term stability, thanks to humidity and temperature compensation provided by the built-in SHTC3. This tutorial will show you how!
Setup and Using MicroPython for Beginners
In this tutorial, our goal is to help guide you through using MicroPython on a microcontroller unit or Linus SBC, setting up and running mpremote, and getting started with three different development environments
How to Run a 5V Device On a 3.3V System With Qwiic
Power up your 5V I2C devices on the Qwiic system! This tutorial shows you how to use the SparkFun Qwiic 5V Boost to integrate power-hungry sensors like the SEN55 seamlessly.
How to Add Audio to Your Embedded Project Using SparkFun's Qwiic Twist and Audio Player Breakout
Looking to bring sound into your next embedded project? In this tutorial, we'll walk you through using the SparkFun Audio Player Breakout in combination with the Qwiic Twist to let you select and play tracks from a microSD card.
Smart Plant Care! Build a Qwiic Soil Moisture Sensor System
See whether your plants are happy or not with their soil moisture level in this Qwiic Circuit Creation!
Turn a Qwiic Ultrasonic Distance Sensor into a Garage Distance Sensor
This tutorial will take your SparkFun Qwiic Ultrasonic Distance Sensor to the next level by turning it into a parking distance sensor!
Calibrating Your Odometry Sensor
In this tutorial, we will cover how to calibrate your Qwiic Optical Tracking Odometry Sensor (or "OTOS") with Arduino and Python Examples.
Moving Beyond the Ordinary With the Qwiic Alphanumeric Display
More than just numbers, more than just letters, with a little creative coding you can do teach your alphanumeric display lots of new tricks.
IMU Data to Motion: Tutorial for Translating Sensor Data into Real-World Movement
Sometimes we want to do more with our data than just watch the values roll by on a screen. In this tutorial, we'll take a look at one way we can translate that data to movement.
How to Play Multiple Buzzers at Once
This tutorial demonstrates the SparkFun Qwiic Buzzer's ability to control multiple buzzers simultaneously by playing a 3-part arrangement of a segment of the Super Mario Bros Theme!
Detecting Colors with the SparkFun Tristimulus Color Sensor
Detect and classify colors based on their CIE XYZ color space values.
Display Distance Measurements On an OLED
This tutorial will take your SparkFun Qwiic Ultrasonic Distance Sensor to the next level by adding a cool little OLED display.
Fading with the MOSFET Power Switch and Buck Regulator
In this tutorial, we will slowly turn on the load and then slowly turn it off using the N-channel MOSFET.
SparkFun Arduino UNO R4 WiFi Qwiic Kit Hookup Guide
The SparkFun Arduino UNO R4 WiFi Qwiic Kit is a great way to get started with Arduino and the Qwiic-connect system - use this guide to get started!
SparkFun RTK Reference Station Hookup Guide
Setup the RTK Reference Station in minutes and start sending RTCM NTRIP corrections to your favourite caster.
Displaying Sensor Data with Bluetooth
In our previous Bluetooth tutorial called Sending Sensor Data Via Bluetooth, we showed how to display data from a triple axis accelerometer over the Arduino IDE’s serial monitor. Continuing off of the first tutorial, we are going to expand this project to include more capabilities for visualizing and interacting with your accelerometer data.
Qwiic Dynamic NFC/RFID Tag Hookup Guide
Add a configurable NFC/RFID tag to your Qwiic ecosystem by following this guide.
SparkFun Thing Plus Matter - MGM240P Hookup Guide
Get started with the SparkFun Thing Plus Matter - MGM240P with this Hookup Guide. This guide covers the hardware on this development board along with a quick intro to using the board with Silicon Labs' Simplicity Studio IDE.
SparkFun NanoBeacon Board - IN100 Hookup Guide
A quick guide to show how to configure and use your own 2.4Ghz wireless beacon with the SparkFun NanoBeacon Board - IN100.
Audio Codec Breakout - WM8960 Hookup Guide
The SparkFun Audio Codec Breakout - WM8960 is a low power, high quality stereo codec chock full of features. In this tutorial, some of these features by using an Arduino microcontroller to configure the audio codec and pass audio to the headphone or speaker channels.
Getting Started with u-blox Thingstream and PointPerfect
Interested in high precision GNSS without setting up a base station?
SparkFun Temperature Sensor - STTS22H (Qwiic) Hookup Guide
Get started with the ultralow-power, high-accuracy, qwiic-enabled SparkFun Temperature Sensor - STTS22H!
MicroMod Main Board Hookup Guide V2
The MicroMod Main Board - Single and Double are specialized carrier boards that allow you to interface a Processor Board with a Function Board(s). The modular system allows you to add an additional feature(s) to a Processor Board with the help of a Function Board(s). In this tutorial, we will focus on the basic functionality of the Main Board - Single V2.1 and Main Board - Double and V2.2.
Qwiic Kit for Raspberry Pi V2 Hookup Guide
Get started with the SGP40, BME280, VCNL4040, and microOLED via I2C using the Qwiic system and Python on a Raspberry Pi! Measure VOC Index, light, temperature, humidity, and pressure from the environment. Then display them on the microOLED, serial terminal, or the cloud with Cayenne!
SparkFun Absolute Digital Barometer - LPS28DFW (Qwiic) Hookup Guide
Get started adding water-resistant pressure sensing using the SparkFun Absolute Digital Barometer - LPS28DFW (Qwiic) following this guide.
SparkFun Indoor Air Quality Sensor - ENS160 (Qwiic) Hookup Guide
Is your air safe? Check your eCO2, TVOC, and AQI levels with the new SparkFun Indoor Air Quality Sensor - ENS160!
Sending Sensor Data over LoRa
This tutorial will show you how setup a simple peer-to-peer connection to send and receive sensor data using LoRa.
GNSS Correction Data Receiver (NEO-D9S) Hookup Guide
Add GNSS correction data to your high precision GNSS (HPG) receiver with the u-blox NEO-D9S! This tutorial will get you started with the ZED-F9P, NEO-D9S, and the ESP32 IoT RedBoard.
Getting Started with Machinechat
Organize and display your data with SparkFun's Artemis OpenLog and MachineChat's JEDIOne!
Qwiic Speaker Amp (TPA2016D2) Hookup Guide
The SparkFun Qwiic Speaker Amp includes the Texas Instruments TPA2016D2 stereo, filter-free class-D audio power amplifier. This tutorial will help you get started and configure the amplifer settings using an Arduino microcontroller.
Measuring Height with Atmospheric Pressure
Measure height using atmospheric pressure with your Qwiic MicroPressure breakout board!
MicroMod Qwiic Pro Kit Project Guide
The MicroMod Qwiic Pro Kit was designed to allow users to get started with Arduino without the need for soldering or a breadboard. We've included three inputs (a joystick, accelerometer, and proximity sensor) and one display that can be daisy chained to the MicroMod SAMD51 Processor Board.
AzureWave Thing Plus (AW-CU488) Hookup Guide
The SparkFun AzureWave Thing Plus is a Feather form-factor development board equipped with the AW-CU488. We'll highlight key features of the board and show you to get started with the development board. A few Arduino examples will be highlighted to connect to a WiFi router, calculate the Fast Fourier Transform (FFT) from an input microphone, output an analog signal to a speaker, and connect an Qwiic-enabled device.
DA16200 Thing Plus Hookup Guide
A guide to get started with the DA16200 Thing Plus.
GNSS Receiver Breakout - MAX-M10S (Qwiic) Hookup Guide
Get started using the SparkFun GNSS Receiver Breakout - MAX-M10S (Qwiic), a ultra-low power, GNSS receiver module for your asset tracking needs!
IoT RedBoard ESP32 Development Board Hookup Guide
Delve into the functionality-rich world of the IoT RedBoard ESP32 Development Board!
Monitor Sensor Data from Anywhere
Using WiFi to send sensor data from an ESP32 to a WiFi network and be able to read it from an IoT Dashboard from anywhere in the world.
Qwiic 9DoF - ISM330DHCX, MMC5983MA Hookup Guide
Find all your degrees of freedom with this little Qwiic breakout board combining the ISM330DHCX 6Dof and the MMC5983MA Magnetometer!
Qwiic Micro Magnetometer - MMC5983MA Hookup Guide
Let's figure out where we're going with the SparkFun Qwiic Micro Magnetometer - MMC5983MA!
Qwiic 6DoF - ISM330DHCX Hookup Guide
Get started with the Qwiic 6DoF ISM330DHCX Breakout Board!
Qwiic Digital Desk Sign with MicroMod
Make a Qwiic-enabled digital desk sign with a MicroMod SAMD51 Processor Board's USB Host and a USB keyboard!
SparkFun RTK Facet L-Band Hookup Guide
Setup the RTK Facet L-Band in minutes to begin gathering millimeter level geospatial coordinates.
MicroMod Alorium Sno M2 Processor Board Hookup Guide
Get started with the MicroMod Alorium Sno M2 Processor Board!
Qwiic dToF Imager (TMF882X) Hookup Guide
Getting started with the AMS dToF imagers (TMF8820 and TMF8820).
MicroMod mikroBUS™ Carrier Board Hookup Guide
This carrier board takes advantage of the MicroMod, Qwiic, and the mikroBUS™ ecosystems and allows users to take advantage of the growing number of 7 MicroMod processor boards, 83 Qwiic (add-on) boards, and +1100 drop-in Click boards™, which equates to +51M different board combinations. Click to learn more.
Qwiic Distance Sensor (VL53L1X, VL53L4CD) Hookup Guide
The Qwiic Distance Sensor - VL53L1X is a time of flight sensor that is capable of several modes, as well as having a range of 4M. It's cousin VL53L4CD is also a time of flight sensor with similar characteristics but it has a range of about 1.3M. Let's hook it up and find out just how far away that thing over there is.
Qwiic ToF Imager - VL53L5CX Hookup Guide
Hookup Guide for the Qwiic ToF Imager - VL53L5CX
GNSS Timing Breakout - ZED-F9T (Qwiic) Hookup Guide
Follow this guide to add up to 5 nanosecond timing accuracy under clear skies with no external GNSS correction with the GNSS Timing Breakout - ZED-F9T (Qwiic).
Sending Sensor Data Over WiFi
This tutorial will show you how setup a simple peer-to-peer connection to send and receive sensor data between two ESP32 WiFi boards.
SparkFun GPS-RTK Dead Reckoning ZED-F9K Hookup Guide
The u-blox ZED-F9K is a powerful GPS-RTK unit that uses a fusion of IMU, wheel ticks, a vehicle dynamics model, correction data, and GNSS measurements to provide highly accurate and continuous position for navigation in the difficult conditions. We will quickly get you set up using the Qwiic ecosystem through Arduino so that you can start reading the output!
SparkFun RTK Facet Hookup Guide
Setup the RTK Facet in minutes to begin gathering millimeter level geospatial coordinates.
MicroMod GNSS Carrier Board (ZED-F9P) Hookup Guide
Easily switch between Processor Boards using the MicroMod ecosystem and get precision down to the diameter of a dime with the ZED-F9P from u-blox using the MicroMod GNSS Carrier Board!
Artemis Global Tracker Hookup Guide
The SparkFun Artemis Global Tracker combines the Artemis processor with an Iridium 9603N satellite transceiver, ZOE-M8Q GNSS transceiver, and MS8607 PHT sensor. With a clear view of the sky, this board allows you to send and receive short data messages from anywhere in the world including remote locations far beyond the reach of WiFi and GSM networks. Follow this guide to get started with the Artemis Global Tracker.
MicroMod Main Board Hookup Guide
The MicroMod Main Board - Single and Double are specialized carrier boards that allow you to interface a Processor Board with a Function Board(s). The modular system allows you to add an additional feature(s) to a Processor Board with the help of a Function Board(s). In this tutorial, we will focus on the basic functionality of the Main Board - Single and Main Board - Double.
smôl Header Hookup Guide
Small in size, small on current draw. It's a smôl world! This guide will get you up and running with the smôl Header.
SparkFun Qwiic Alphanumeric Display Hookup Guide
A Hookup Guide to get you started with the Qwiic Alphanumeric Display.
Air Velocity Sensor Breakout - FS3000 Hookup Guide
Get started with the Air Velocity Sensor Breakout - FS3000!
Digital Temperature Sensor Breakout - AS6212 (Qwiic) Hookup Guide
Get started measuring highly accurate temperatures at extremely low power with the AS6212 temperature sensor on the SparkFun Digital Temperature Sensor Breakout - AS6212 (Qwiic).
Tsunami Super WAV Trigger Hookup Guide
This guide will get users started with the Qwiic Tsunami. We'll start by putting *.wav files and a configuration file on a microSD card, pop it into the Qwiic Tsunami, then trigger sounds across multiple outputs.
Qwiic EEPROM Hookup Guide
Running out of memory? Don't forget to check out the Qwiic EEPROM!
Qwiic LED Stick - APA102C Hookup Guide
Add some I2C RGB to your project with the SparkFun Qwiic LED Stick - APA102C
RedBoard Plus Hookup Guide
This tutorial covers the basic functionality of the RedBoard Plus. This tutorial also covers how to get started blinking an LED and using the Qwiic system.
Air Quality Sensor - SGP40 (Qwiic) Hookup Guide
Get started measuring indoor air quality with the SparkFun Air Quality Sensor - SGP40 (Qwiic) Hookup Guide.
SparkFun RTK Express Hookup Guide
Learn how to use the enclosed RTK Express product to achieve millimeter level geospatial coordinates.
Qwiic 6DoF (LSM6DSO) Breakout Hookup Guide
A hookup guide for the Qwiic 6DoF (LSM6DSO), which features a 3-axis accelerometer, 3-axis gyroscope, temperature sensor, and FIFO buffer.
Triple Axis Accelerometer Breakout - KX13x (Qwiic) Hookup Guide
Get started measuring acceleration and vibration using the Triple Axis Accelerometer Breakout - KX134 (Qwiic) & KX132 (Qwiic) following this Hookup Guide.
Qwiic Haptic Driver DA7280 Hookup Guide
The Qwiic Haptic Driver includes an itty-bitty, Linear Resonant Actuator (LRA) vibration motor and Dialog Semiconductor's DA7280 motor driver IC for applications that require haptic feedback.
Garmin LIDAR-Lite v4 (Qwiic) Hookup Guide
Connecting the Garmin LIDAR-Lite v4 to a microcontroller just got easier! Check out our hookup guide to get started.
ESP32-S2 Thing Plus Hookup Guide
Looking to use the more secure ESP32-S2? Follow this hookup guide to get started.
Qwiic MultiPort Hookup Guide
The SparkFun Qwiic MultiPort adds additional ports to boards that have only one Qwiic port on their I2C bus. Once added, you can use it as a hub to add as many I2C devices to the bus as you need! You can also use the board as an alternative to a daisy chained configuration.
SparkFun QwiicBus Hookup Guide
Build a long-range, noise-isolated I2C bus with the SparkFun QwiicBus Kit featuring the QwiicBus EndPoint and MidPoint following this Hookup Guide.
Qwiic Ultrasonic Distance Sensor (HC-SR04) Hookup Guide
Get started with the Qwiic Ultrasonic Distance Sensor!
Qwiic PIR Hookup Guide
Get started passively monitoring motion using the Panasonic EKMC and EKMB sensors with the SparkFun Qwiic PIR.
Qwiic Carrier Board Hookup Guide
The Qwiic carrier board is the latest way to rapid prototype with the included M.2 socket to swap processor boards and Qwiic connectors to easily connect I2C devices.
MicroMod Asset Tracker Carrier Board Hookup Guide
Get started with the SparkFun MicroMod Asset Tracker Carrier Board following this Hookup Guide. The Asset Tracker uses the u-blox SARA-R510M8S LTE-M / NB-IoT module to provide a host of data communication options.
Qwiic SHIM Kit for Raspberry Pi Hookup Guide
Get started with the Serial LCD with RGB backlight and 9DoF IMU (ICM-20948) via I2C using the Qwiic system and Python on a Raspberry Pi! Take sensor readings and display them in the serial terminal or SerLCD.
SparkFun expLoRaBLE Hookup Guide
Check out our latest LoRaWAN development board with Bluetooth capabilities! With this guide, we'll get you passing data to The Things Network in no time.
Soil Moisture Sensor Hookup Guide
A quick hookup guide and project to get you started with the Soil Moisture Sensor from SparkFun.
RP2040 Thing Plus Hookup Guide
Want to take a stab at advancing your programming skills? Check out the Thing Plus - RP2040, with the first microcontroller from the Raspberry Pi Foundation. This guide will get you started working with the RP2040 and programming in MicroPython and C/C++.
MicroMod RP2040 Processor Board Hookup Guide
This tutorial covers the basic functionality of the MicroMod RP2040 Processor Board and highlights the features of the dual-core ARM Cortex-M0+ processors development board. Get started with the first microcontroller from the Raspberry Pi Foundation!
Pro Micro RP2040 Hookup Guide
This tutorial covers the basic functionality of the Pro Micro RP2040 and highlights the features of the dual-core ARM Cortex-M0+ processors development board. Get started with the first microcontroller from the Raspberry Pi Foundation!
Qwiic pHAT Extension for Raspberry Pi 400 Hookup Guide
Get started interfacing your Qwiic enabled boards with your Raspberry Pi 400! SparkFun Qwiic pHAT Extension for the Raspberry Pi 400 provides you with a quick and easy solution to access all of the 400's GPIO, stack your favorite HAT right-side up, or connect a Qwiic-enabled device to the I2C bus (GND, 3.3V, SDA, and SCL).
SparkFun RTK Surveyor Hookup Guide
Learn how to use the enclosed RTK Surveyor product to achieve millimeter level geospatial coordinates.
SparkFun Qwiic 3-Axis Accelerometer (ADXL313) Hookup Guide
Let's get moving with the SparkFun Triple Axis Digital Accelerometer Breakout - ADXL313 (Qwiic), a low cost, low power, up to 13-bit resolution, 3-axis accelerometer with a 32-level FIFO stack capable of measuring up to ±4g. This hookup guide will get users started reading measurements from the ADXL313, by Analog Devices, with an Arduino microcontroller, Jetson Nano, or Raspberry Pi.
MicroMod All The Pins (ATP) Carrier Board
Access All The Pins (ATP) of the MicroMod Processor Board with the Carrier Board!
MicroMod Machine Learning Carrier Board Hookup Guide
Get hacking with this tutorial on our Machine Learning Carrier Board!
MicroMod ESP32 Processor Board Hookup Guide
A short hookup guide to get started with the SparkFun MicroMod ESP32 Processor Board.
MicroMod Data Logging Carrier Board Hookup Guide
Get started with some customizable MicroMod data logging with the Data Logging Carrier Board.
SparkFun MicroMod Input and Display Carrier Board Hookup Guide
A short Hookup Guide to get started with the SparkFun MicroMod Input and Display Carrier Board
SparkFun Qwiic Shield for Teensy Hookup Guide
A short guide for assembling and using the SparkFun Qwiic Shield for Teensy and Qwiic Shield for Teensy Extended.
SparkFun Qwiic GPIO Hookup Guide
Add up to 8 extra I/O pins to your microcontroller with the SparkFun Qwiic GPIO. Get started with the Qwiic GPIO in this Hookup Guide.
The ClockClock Project
Tell the time with this fantastic Alchitry project using clocks to make a clock!
SparkFun Qwiic Dual Solid State Relay Hookup Guide
A Hookup Guide to get you started with the SparkFun Qwiic Dual Solid State Relay.
Getting Started with the Artemis Development Kit
This guide covers the general design of the board, the installation of the recommended software used to program the Artemis DK, and some basic examples. For more advanced functionalities, we have separate software development guides for the AmbiqSDK, Arm® Mbed™ OS, and the Arduino IDE platforms that users can reference.
Artemis Development with the Arduino IDE
This is an in-depth guide on developing in the Arduino IDE for the Artemis module and any Artemis microcontroller development board. Inside, users will find setup instructions and simple examples from blinking an LED and taking ADC measurements; to more complex features like BLE and I2C.
OpenLog Artemis Hookup Guide
How to use and re-program the OpenLog Artemis, an open source datalogger. The OLA comes preprogrammed to automatically log data. The OLA can also record serial data, analog voltages, or readings from external Qwiic-enabled I2C devices. Some of these Qwiic-enabled devices include GPS/GNSS modules, pressure, altitude, humidity, temperature, air quality, environment, distance, and weight sensors.
SparkFun Qwiic MicroPressure Hookup Guide
Get started using your Qwiic MicroPressure breakout board with this hookup guide.
SparkFun Qwiic Quad Solid State Relay Kit Hookup Guide
A Hookup Guide to get you started with the SparkFun Qwiic Quad Solid State Relay Kit (say that five times fast!).
Qwiic Digital Indoor Thermometer
Qwiic-ly build a digital indoor thermometer to measure the ambient temperature of the room and display it using an OLED on an I2C bus!
SparkFun GPS-RTK Dead Reckoning ZED-F9R Hookup Guide
The u-blox ZED-F9R is a powerful GPS-RTK unit that uses a fusion of IMU, wheel ticks, a vehicle dynamics model, correction data, and GNSS measurements to provide highly accurate and continuous position for navigation in the difficult conditions. We will quickly get you set up using the Qwiic ecosystem through Arduino and Python so that you can start reading the output!
SparkFun Photodetector (MAX30101) Hookup Guide
The SparkFun Photodetector - MAX30101 (Qwiic) is the successor to the MAX30105 particle sensor, a highly sensitive optical sensor. This tutorial will get you started on retrieving the raw data from the MAX30101 sensor.
RFID Beginners Tutorial
Make a remote work logger using an RFID reader and a GPS module. Scan a card and get ID, location, and time. All the perfect data to punch in and punch out from the middle of Nowhere!
SparkFun Air Quality Sensor - SGP30 (Qwiic) Hookup Guide
A hookup guide to get started with the SparkFun Air Quality Sensor - SGP30 (Qwiic).
SparkFun Environmental Sensor Breakout - BME68x (Qwiic) Hookup Guide
A hookup guide to get started with the BME68x Environmental Sensor from Bosch. Monitor the air quality, temperature, humidity, and barometric pressure with this Qwiic sensor!
SparkFun Humidity Sensor Breakout - SHTC3 (Qwiic) Hookup Guide
A Hookup Guide to get started using the SHTC3 breakout.
SparkFun GPS Dead Reckoning NEO-M8U Hookup Guide
The u-blox NEO-M8U is a powerful GPS units that takes advantage of untethered dead reckoning (UDR) technology for navigation. The module provides continuous positioning for vehicles in urban environments and during complete signal loss (e.g. short tunnels and parking garages). We will quickly get you set up using the Qwiic ecosystem and Arduino so that you can start reading the output!
Working with Qwiic on a Jetson Nano through Jupyter Notebooks
We created a few Jupyter Notebooks to make using our Qwiic boards with your Jetson Nano even easier!
Raspberry Pi Safe Reboot and Shutdown Button
Safely reboot or shutdown your Raspberry Pi to avoid corrupting the microSD card using the built-in general purpose button on the Qwiic pHAT v2.0!
SparkFun Auto pHAT Hookup Guide
The pHAT to get your projects moving. This guide will help you get started using the Auto pHAT.
SparkFun Top pHAT Hookup Guide
The pHAT to sit above your other HATs. Does that make it the "king" of the pHATs?
This guide will help you get started using the Top pHAT with the Raspberry Pi.
Real Time Clock Module - RV-8803 (Qwiic) Hookup Guide
A Hookup Guide for the SparkFun Real Time Clock Module - RV-8803 (Qwiic). Learn how to integrate the RV-8803 into your next time-keeping project.
Assembly Guide for SparkFun JetBot AI Kit V2.0
Assembly Guide for the SparkFun JetBot AI Kit v2.0. This tutorial includes photos & comments to assemble the two-layer chassis & additional components unique to the JetBot kit.
SparkFun Qwiic Digital Temperature Sensor - TMP102 Hookup Guide
Get started using your SparkFun Digital Temperature Sensor - TMP102 (Qwiic) with this Hookup Guide!
Temperature Sensor Comparison
A comparison of analog and digital temperature sensors. Which is better?
Raspberry Pi 4 Kit Hookup Guide
Guide for hooking up your Raspberry Pi 4 Model B basic, desktop, or hardware starter kit together.
SparkFun Qwiic Thermocouple Hookup Guide
Learn how to hook up your Qwiic Thermocouple Amplifier.
SparkFun Clock Generator 5P49V60 (Qwiic) Hookup Guide
The SparkFun Clock Generator 5P49V60 (Qwiic) breakout board offers a wide range of customizable frequencies in a wide range of different signal types using a single reference clock. This hookup guide will go over all of the many available functions and gives the hardware rundown on what exactly is on this board.
Basic Servo Control for Beginners
An introductory tutorial demonstrating several ways to use and interact with servo motors!
Power Delivery Board - USB-C (Qwiic) Hookup Guide
This guide will go over how to use the USB Type-C Power Delivery Board.
Qwiic Pro Micro USB-C (ATmega32U4) Hookup Guide
An overview of the ATmega32U4-based Qwiic Pro Micro USB-C, how to install it, and how to use it with Arduino.
SparkFun Qwiic Shield for Thing Plus Hookup Guide
A short guide for assembling and using the SparkFun Qwiic Shield for Thing Plus.
SparkFun Qwiic Shield for Arduino Nano Hookup Guide
Hookup Guide for the SparkFun Qwiic Shield for Arduino Nano.
SparkFun Qwiic Button Hookup Guide
A Hookup Guide for the SparkFun Qwiic Button (Red) and SparkFun Qwiic Button Breakout. Goes over connecting the Qwiic Button to an Arduino microcontroller and using it with the Qwiic Button Arduino library.
Secure DIY Garage Door Opener
Did you know that most garage doors are at risk of a roll jam attack? Here we make a DIY garage door remote-control system that is much more secure than most commercial-ready products using the latest in ECC cryptography.
SparkFun GPS NEO-M9N Hookup Guide
The u-blox NEO-M9N is a powerful GPS unit that comes with a chip antenna, SMA connector, and u.FL connector. We will quickly get you set up using the Qwiic ecosystem and Arduino so that you can start reading the output!
Getting Started with the Autonomous Kit for the Sphero RVR
Want to get started in robotics? Look no further than the SparkFun autonomous kit for the Sphero RVR! Whether you purchased the Basic or Advanced kit, this tutorial will get you rolling...
Basic Autonomous Kit for Sphero RVR Assembly Guide
Get your Basic Autonomous Kit for Sphero RVR all hooked up with this guide!
Advanced Autonomous Kit for Sphero RVR Assembly Guide
Get your Advanced Autonomous Kit for the Sphero RVR built up with this hookup guide!
Programming the SparkFun Edge with Arduino
Running low-power machine learning examples on the SparkFun Edge can now be done using the familiar Arduino IDE. In this follow-up to the initial Edge tutorial, we'll look at how to get three examples up and running without the need to learn an entirely new SDK.
Qwiic SHIM for Raspberry Pi Hookup Guide
Ever wanted to prototype I2C components on a Pi? Now you can!
Qwiic TMP117 High Precision Digital Temperature Sensor Hookup Guide
Add a high precision, digital temperature sensor to your projects using the TMP117 over the I2C!
Qwiic Pro Kit Project Guide
The Qwiic Pro Kit was designed to allow users to get started with Arduino without the need for soldering or a breadboard. We've included three inputs (a joystick, accelerometer, and proximity sensor) and one display that can be daisy chained to the RedBoard Turbo (SAMD21) Development Board.
SparkFun Qwiic Micro (SAMD21E) Hookup Guide
An introduction to the Qwiic Micro SAMD21E. Level up your Arduino-skills with the powerful SAMD21 ARM Cortex M0+ processor!
Cryptographic Co-Processor ATECC508A (Qwiic) Hookup Guide
Learn how to use some of the standard features of the SparkFun Cryptographic Co-processor.
GPS Geo-Mapping at the Push of a Button
Let's ramp up our GPS tracking skills with KML files and Google Earth. We'll make a tracker that logs location and allows us to visualize our steps with Google Earth.
SparkFun Edge Hookup Guide
Get to know your Edge board, including both the hardware features for you to utilize as well as how to get talking to it.
Hookup Guide for the Qwiic Motor Driver
Drive things "qwiic"-ly with the SparkFun Qwiic Motor Driver!
SparkFun Pulse Oximeter and Heart Rate Monitor Hookup Guide
Find out your oxygen saturation level or check out your heart rate using the MAX30101 biometric sensor and MAX32664 Biometric Hub via I2C!
Hookup Guide for the SparkFun RedBoard Artemis
Get started with the RedBoard Artemis - all the functionality of the SparkFun Artemis module wrapped in the familiar Uno R3 footprint
Hookup Guide for the SparkFun RedBoard Artemis Nano
Get started with the powerful RedBoard Artemis Nano
Hookup Guide for the SparkFun RedBoard Artemis ATP
Get started with the RedBoard Artemis ATP - all the functionality of the SparkFun Artemis module wrapped in the Mega Arduino Footprint
XBee3 Thing Plus Hookup Guide
Get started with SparkFun's XBee3 Thing Plus - both the u.FL as well as the PCB antenna versions.
Qwiic Atmospheric Sensor (BME280) Hookup Guide
Measure temperature, humidity, barometric pressure with the SparkFun Atmospheric Sensor Breakout BME280 (Qwiic).
SparkFun AS3935 Lightning Detector Hookup Guide (v20)
Are you worried about the looming clouds in the distance, how far away is that storm exactly? Add lightning detection with the AS3935 to your next weather station or your next bike ride!
Pi Servo pHAT (v2) Hookup Guide
This hookup guide will get you started with connecting and using the Pi Servo pHAT on a Raspberry Pi.
SparkFun 9DoF IMU (ICM-20948) Breakout Hookup Guide
How to use the SparkFun 9DoF ICM-20948 breakout board for your motion sensing projects. This breakout is ideal for wearable sensors and IoT applications.
Capacitive Touch Slider (CAP1203) Hookup Guide
An easy and Qwiic way to add capacitive touch to any of your projects using the CAP1203! In this guide, we go over how to connect and set up your Capacitive Touch Slider so you can start playing with it right away.
SAMD51 Thing Plus Hookup Guide
This tutorial covers the basic functionality of the SAMD51 Thing Plus and highlights the features of the new ARM Cortex-M4F development board.
Qwiic 12-Bit ADC Hookup Guide
Need to add more analog inputs for your project? Check out the Qwiic 12-bit ADC.
Qwiic pHAT for Raspberry Pi Hookup Guide
Get started interfacing your Qwiic enabled boards with your Raspberry Pi. The Qwiic pHAT connects the I2C bus (GND, 3.3V, SDA, and SCL) on your Raspberry Pi to an array of Qwiic connectors.
Displaying Your Coordinates with a GPS Module
This Arduino tutorial will teach you how to pinpoint and display your GPS coordinates with a press of a button using hardware from our Qwiic Connect System (I2C).
Keyboard Shortcut, Qwiic Keypad
A simple project using the Qwiic Keypad and the RedBoard Turbo to create your own custom hotkey-pad.
Qwiic Keypad Hookup Guide
If you are tired of taking up GPIO pins, wiring a bunch of pull up resistors, and using firmware that scans the keys taking up valuable processing time... check out the new Qwiic Keypad.
Qwiic Scale Hookup Guide
Create your own digital scale quickly and easily using the Qwiic Scale!
SparkFun GPS Breakout (ZOE-M8Q and SAM-M8Q) Hookup Guide
The SparkFun ZOE-M8Q and SAM-M8Q are three similarly powerful GNSS boards, but with different project applications. We'll compare both GNSS receivers before getting each up and running.
Build a Qwiic Jukebox that is Toddler Approved!
Follow this tutorial to build your own custom jukebox. Note, this is designed simple and tough for use primarily with toddlers. It's also a great introduction to SparkFun's Qwiic products!
Using SparkFun Edge Board with Ambiq Apollo3 SDK
We will demonstrate how to get started with your SparkFun Edge Board by setting up the toolchain on your computer, examining an example program, and using the serial uploader tool to flash the chip.
SparkFun Qwiic RFID-IDXXLA Hookup Guide
The Qwiic RFID ID-XXLA is an I2C solution that pairs with the ID-LA modules: ID-3LA, the ID-12LA, or the ID-20LA, and utilizes 125kHz RFID chips. Let's take a look at the hardware used for this tutorial.
ESP32 Thing Plus Hookup Guide
Hookup guide for the ESP32 Thing Plus (Micro-B) using the ESP32 WROOM's WiFi/Bluetooth system-on-chip in Arduino.
Transparent Graphical OLED Breakout Hookup Guide
The future is here! Our Qwiic Transparent Graphical OLED Breakout allows you to display custom images on a transparent screen using either I2C or SPI connections.
Qwiic Proximity Sensor (VCNL4040) Hookup Guide
The SparkFun Qwiic Proximity Sensor is a great, qualitative proximity (up to 20 cm) and light sensor. This hookup guide covers a few examples to retrieve basic sensor readings.
Qwiic Joystick Hookup Guide
Looking for an easy way to implement a joystick to your next Arduino or Raspberry Pi project? This hookup guide will walk you through using the Qwiic Joystick with the Arduino IDE on a RedBoard Qwiic and in Python on a Raspberry Pi.
Qwiic Transparent OLED HUD Hookup Guide
Learn how to connect that sweet transparent OLED.
Qwiic OpenLog Hookup Guide
The updated Qwiic version of the OpenLog Hookup Guide
RedBoard Turbo Hookup Guide
An introduction to the RedBoard Turbo. Level up your Arduino-skills with the powerful SAMD21 ARM Cortex M0+ processor!
Qwiic MP3 Trigger Hookup Guide
Playing MP3s has never been easier.
GPS-RTK2 Hookup Guide
Get precision down to the diameter of a dime with the new ZED-F9P from u-blox.
RedBoard Qwiic Hookup Guide
This tutorial covers the basic functionality of the RedBoard Qwiic. This tutorial also covers how to get started blinking an LED and using the Qwiic system.
Qwiic Quad Relay Hookup Guide
SparkFun’s Qwiic Quad Relay is a product designed for switching not one but four high powered devices from your Arduino or other low powered microcontroller using I2C.
Qwiic Single Relay Hookup Guide
Get started switching those higher power loads around with the Qwiic Single Relay.
Three Quick Tips About Using U.FL
Quick tips regarding how to connect, protect, and disconnect U.FL connectors.
Qwiic UV Sensor (VEML6075) Hookup Guide
Learn how to connect your VEML6075 UV Sensor and figure out just when you should put some sunscreen on.
Qwiic Twist Hookup Guide
Take your volume knob beyond 11 with the Qwiic Twist digital RGB LED encoder via I2C!
SparkFun Pro nRF52840 Mini Hookup Guide
A hardware overview and hookup guide for the SparkFun Pro nRF52840 Mini -- a breakout for Nordic's impossibly cool Bluetooth/ARM Cortex M4 SoC.
LTE Cat M1/NB-IoT Shield Hookup Guide
The SparkFun LTE CAT M1/NB-IoT Shield equips your Arduino or Arduino-compatible microcontroller with access to data networks across the globe. This shield adds wireless, high-bandwidth cellular functionality to your IoT project!
SparkFun LoRa Gateway 1-Channel Hookup Guide
How to setup and use the LoRa Gateway 1-Channel in Arduino.
Spectral Triad (AS7265x) Hookup Guide
Learn how to wield the power of 18 channels of UV to NIR spectroscopy with AS72651 (UV), AS72652 (VIS), and AS72653 (NIR) sensors!
TFMini - Micro LiDAR Module (Qwiic) Hookup Guide
The TFMini is a ToF (Time of Flight) LiDAR sensor capable of measuring the distance to an object as close as 30 cm and as far as 12 meters! The TFMini allows you to easily integrate LiDAR into applications traditionally reserved for smaller sensors such as the SHARP GP-series infrared rangefinders. With the added Qwiic feature, you can quickly connect to the sensor via I2C!
SparkFun SAMD21 Pro RF Hookup Guide
Using the super blazing, nay blinding, fast SAMD21 whipping clock cycles at 48MHz and the RFM96 module to connect to the Things Network (and other Radio woodles).
Qwiic IR Array (MLX90640) Hookup Guide
The Melexis MLX90640 contains a 32x24 array of thermopile sensors creating, in essence, a low resolution thermal imaging camera. In this guide, we’ll go over how to connect your Qwiic Infrared Array with MLX90640 and get it communicating with Processing to produce a nice thermal image.
GPS-RTK Hookup Guide
Find out where you are! Use this easy hook-up guide to get up and running with the SparkFun high precision GPS-RTK NEO-M8P-2 breakout board.
ESP32 LoRa 1-CH Gateway, LoRaWAN, and the Things Network
Using the ESP32 LoRa 1-CH Gateway as a gateway and device, and pushing data to The Things Network.
AVR-Based Serial Enabled LCDs Hookup Guide
The AVR-based Qwiic Serial Enabled LCDs are a simple and cost effective solution to include in your project. These screens are based on the HD44780 controller, and include ATmega328P with an Arduino compatible bootloader. They accept control commands via Serial, SPI and I2C (via PTH headers or Qwiic connector). In this tutorial, we will show examples of a simple setup and go through each communication option.
Qwiic Flex Glove Controller Hookup Guide
Is your finger bent? Is your finger straight? The Qwiic Flex Glove controller board will answer this age old question for you with the flex sensor!
Qwiic MUX Hookup Guide
Have a bunch of sensors with the same I2C address? Put them on the Qwiic MUX (TCA9548A) to get them all talking on the same bus!
RedBoard Edge Hookup Guide
The RedBoard Edge is a RedBoard that's been rebuilt around the idea that projects are eventually put into an enclosure to help clean up their look.
Qwiic Differential I2C Bus Extender (PCA9615) Hookup Guide
Learn how to extend the range of your I2C communication bus with the Qwiic differential I2C bus extender (PCA9615 ) breakout board.
Qwiic Real Time Clock Module (RV-1805) Hookup Guide
Find out what time it is, even after the power's been out on your project for a while with the Qwiic Real Time Clock (RTC) module.
IoT Power Relay
Using the ESP32 to make a web-configured timed relay.
Qwiic Magnetometer (MLX90393) Hookup Guide
Figure out how magnetic fields are oriented, all without having to solder a thing.
Qwiic GRID-Eye Infrared Array (AMG88xx) Hookup Guide
The Panasonic GRID-Eye (AMG88xx) 8x8 thermopile array serves as a functional low-resolution infrared camera. This means you have a square array of 64 pixels each capable of independent temperature detection. It’s like having thermal camera (or Predator’s vision), just in really low resolution.
Qwiic VR IMU (BNO080) Hookup Guide
Figure out how things are oriented with the robust 9 degrees of freedom (DOF) BNO080 IMU. Maybe even make your own virtual reality (VR) applications if you're feeling savvy.
Qwiic Accelerometer (MMA8452Q) Hookup Guide
Freescale’s MMA8452Q is a smart, low-power, three-axis, capacitive micro-machined accelerometer with 12-bits of resolution. It’s perfect for any project that needs to sense orientation or motion. We’ve taken that accelerometer and stuck it on a Qwiic-Enabled breakout board to make interfacing with the tiny, QFN package a bit easier.
Qwiic Distance Sensor (RFD77402) Hookup Guide
The RFD77402 uses an infrared VCSEL (Vertical Cavity Surface Emitting Laser) TOF (Time of Flight) module capable of millimeter precision distance readings up to 2 meters. It’s also part of SparkFun’s Qwiic system, so you won’t have to do any soldering to figure out how far away things are.
Using the PSoC 6 Pioneer Board with the Pioneer IoT Add-on Shield
Cypress's PSoC 6 Pioneer Board is a development tool for the powerful PSoC 6 processor. In this tutorial, we'll show you how to use the PSoC 6 Pioneer Board along with the SparkFun/Digi-Key Pioneer IoT Add-on Shield to send data to a Raspberry Pi via BLE or WiFi.
Qwiic Micro OLED Hookup Guide
Get started displaying things with the Qwiic Micro OLED.
Qwiic Human Presence Sensor (AK9753) Hookup Guide
How to get started with your Qwiic enabled AK9753 Human Presence Sensor.
Qwiic Adapter Hookup Guide
Get started with your Qwiic adapter board. This adapter breaks out the I2C pins from the Qwiic connectors to pins that you can easily solder with your favorite I2C enabled device.
Qwiic HAT for Raspberry Pi Hookup Guide
Get started interfacing your Qwiic enabled boards with your Raspberry Pi. This Qwiic connects the I2C bus (GND, 3.3V, SDA, and SCL) on your Raspberry Pi to an array of Qwiic connectors.
SparkFun GPS Breakout - XA1110 (Qwiic) Hookup Guide
Figure out where in the world you are with the Qwiic SparkFun GPS Breakout - XA1110.
Qwiic Shield for Arduino & Photon Hookup Guide
Get started with our Qwiic ecosystem with the Qwiic shield for Arduino or Photon.
AS726X NIR/VIS Spectral Sensor Hookup Guide
It's now easier than ever to measure and characterize how different materials absorb and reflect different wavelengths of light. The AS726X spectral sensors allow you to detect wavelengths in the visible range (VIS) and near infrared range (NIR)!
CCS811/BME280 (Qwiic) Environmental Combo Breakout Hookup Guide
Sense various environmental conditions such as temperature, humidity, barometric pressure, eCO2 and tVOCs with the CCS811 and BME280 combo breakout board.
Sensor Kit Resource Hub
An overview of each component in the SparkFun Sensor Kit, plus links to tutorials and other resources you'll need to hook them up.
I2C
An introduction to I2C, one of the main embedded communications protocols in use today.