Qwiic
The SparkFun Qwiic Connect System is an ecosystem of I2C sensors, actuators, shields, and cables that make prototyping faster and less prone to error. Get it? It's quick Qwiic! The following tutorials tagged takes advantage of the Qwiic system.
SparkFun Absolute Digital Barometer - LPS28DFW (Qwiic) Hookup Guide
Get started adding water-resistant pressure sensing using the SparkFun Absolute Digital Barometer - LPS28DFW (Qwiic) following this guide.
SparkFun Indoor Air Quality Sensor - ENS160 (Qwiic) Hookup Guide
Is your air safe? Check your eCO2, TVOC, and AQI levels with the new SparkFun Indoor Air Quality Sensor - ENS160!
Sending Sensor Data over LoRa
This tutorial will show you how setup a simple peer-to-peer connection to send and receive sensor data using LoRa.
GNSS Correction Data Receiver (NEO-D9S) Hookup Guide
Add GNSS correction data to your high precision GNSS (HPG) receiver with the u-blox NEO-D9S! This tutorial will get you started with the ZED-F9P, NEO-D9S, and the ESP32 IoT RedBoard.
Getting Started with Machinechat
Organize and display your data with SparkFun's Artemis OpenLog and MachineChat's JEDIOne!
MicroMod Qwiic Pro Kit Project Guide
The MicroMod Qwiic Pro Kit was designed to allow users to get started with Arduino without the need for soldering or a breadboard. We've included three inputs (a joystick, accelerometer, and proximity sensor) and one display that can be daisy chained to the MicroMod SAMD51 Processor Board.
Measuring Height with Atmospheric Pressure
Measure height using atmospheric pressure with your Qwiic MicroPressure breakout board!
Qwiic Speaker Amp (TPA2016D2) Hookup Guide
The SparkFun Qwiic Speaker Amp includes the Texas Instruments TPA2016D2 stereo, filter-free class-D audio power amplifier. This tutorial will help you get started and configure the amplifer settings using an Arduino microcontroller.
AzureWave Thing Plus (AW-CU488) Hookup Guide
The SparkFun AzureWave Thing Plus is a Feather form-factor development board equipped with the AW-CU488. We'll highlight key features of the board and show you to get started with the development board. A few Arduino examples will be highlighted to connect to a WiFi router, calculate the Fast Fourier Transform (FFT) from an input microphone, output an analog signal to a speaker, and connect an Qwiic-enabled device.
DA16200 Thing Plus Hookup Guide
A guide to get started with the DA16200 Thing Plus.
GNSS Receiver Breakout - MAX-M10S (Qwiic) Hookup Guide
Get started using the SparkFun GNSS Receiver Breakout - MAX-M10S (Qwiic), a ultra-low power, GNSS receiver module for your asset tracking needs!
IoT RedBoard ESP32 Development Board Hookup Guide
Delve into the functionality-rich world of the IoT RedBoard ESP32 Development Board!
Monitor Sensor Data from Anywhere
Using WiFi to send sensor data from an ESP32 to a WiFi network and be able to read it from an IoT Dashboard from anywhere in the world.
Qwiic 9DoF - ISM330DHCX, MMC5983MA Hookup Guide
Find all your degrees of freedom with this little Qwiic breakout board combining the ISM330DHCX 6Dof and the MMC5983MA Magnetometer!
Qwiic Micro Magnetometer - MMC5983MA Hookup Guide
Let's figure out where we're going with the SparkFun Qwiic Micro Magnetometer - MMC5983MA!
Qwiic 6DoF - ISM330DHCX Hookup Guide
Get started with the Qwiic 6DoF ISM330DHCX Breakout Board!
Qwiic Digital Desk Sign with MicroMod
Make a Qwiic-enabled digital desk sign with a MicroMod SAMD51 Processor Board's USB Host and a USB keyboard!
SparkFun RTK Facet L-Band Hookup Guide
Setup the RTK Facet L-Band in minutes to begin gathering millimeter level geospatial coordinates.
MicroMod Alorium Sno M2 Processor Board Hookup Guide
Get started with the MicroMod Alorium Sno M2 Processor Board!
Qwiic dToF Imager (TMF882X) Hookup Guide
Getting started with the AMS dToF imagers (TMF8820 and TMF8820).
MicroMod mikroBUS™ Carrier Board Hookup Guide
This carrier board takes advantage of the MicroMod, Qwiic, and the mikroBUS™ ecosystems and allows users to take advantage of the growing number of 7 MicroMod processor boards, 83 Qwiic (add-on) boards, and +1100 drop-in Click boards™, which equates to +51M different board combinations. Click to learn more.
Qwiic Distance Sensor (VL53L1X, VL53L4CD) Hookup Guide
The Qwiic Distance Sensor - VL53L1X is a time of flight sensor that is capable of several modes, as well as having a range of 4M. It's cousin VL53L4CD is also a time of flight sensor with similar characteristics but it has a range of about 1.3M. Let's hook it up and find out just how far away that thing over there is.