Qwiic
The SparkFun Qwiic Connect System is an ecosystem of I2C sensors, actuators, shields, and cables that make prototyping faster and less prone to error. Get it? It's quick Qwiic! The following tutorials tagged takes advantage of the Qwiic system.
Qwiic GRID-Eye Infrared Array (AMG88xx) Hookup Guide
The Panasonic GRID-Eye (AMG88xx) 8x8 thermopile array serves as a functional low-resolution infrared camera. This means you have a square array of 64 pixels each capable of independent temperature detection. It’s like having thermal camera (or Predator’s vision), just in really low resolution.
Qwiic VR IMU (BNO080) Hookup Guide
Figure out how things are oriented with the robust 9 degrees of freedom (DOF) BNO080 IMU. Maybe even make your own virtual reality (VR) applications if you're feeling savvy.
Qwiic Accelerometer (MMA8452Q) Hookup Guide
Freescale’s MMA8452Q is a smart, low-power, three-axis, capacitive micro-machined accelerometer with 12-bits of resolution. It’s perfect for any project that needs to sense orientation or motion. We’ve taken that accelerometer and stuck it on a Qwiic-Enabled breakout board to make interfacing with the tiny, QFN package a bit easier.
Qwiic Distance Sensor (RFD77402) Hookup Guide
The RFD77402 uses an infrared VCSEL (Vertical Cavity Surface Emitting Laser) TOF (Time of Flight) module capable of millimeter precision distance readings up to 2 meters. It’s also part of SparkFun’s Qwiic system, so you won’t have to do any soldering to figure out how far away things are.
Using the PSoC 6 Pioneer Board with the Pioneer IoT Add-on Shield
Cypress's PSoC 6 Pioneer Board is a development tool for the powerful PSoC 6 processor. In this tutorial, we'll show you how to use the PSoC 6 Pioneer Board along with the SparkFun/Digi-Key Pioneer IoT Add-on Shield to send data to a Raspberry Pi via BLE or WiFi.
Qwiic Micro OLED Hookup Guide
Get started displaying things with the Qwiic Micro OLED.
Qwiic Human Presence Sensor (AK9753) Hookup Guide
How to get started with your Qwiic enabled AK9753 Human Presence Sensor.
Qwiic Adapter Hookup Guide
Get started with your Qwiic adapter board. This adapter breaks out the I2C pins from the Qwiic connectors to pins that you can easily solder with your favorite I2C enabled device.
Qwiic HAT for Raspberry Pi Hookup Guide
Get started interfacing your Qwiic enabled boards with your Raspberry Pi. This Qwiic connects the I2C bus (GND, 3.3V, SDA, and SCL) on your Raspberry Pi to an array of Qwiic connectors.
SparkFun GPS Breakout - XA1110 (Qwiic) Hookup Guide
Figure out where in the world you are with the Qwiic SparkFun GPS Breakout - XA1110.
Qwiic Shield for Arduino & Photon Hookup Guide
Get started with our Qwiic ecosystem with the Qwiic shield for Arduino or Photon.
AS726X NIR/VIS Spectral Sensor Hookup Guide
It's now easier than ever to measure and characterize how different materials absorb and reflect different wavelengths of light. The AS726X spectral sensors allow you to detect wavelengths in the visible range (VIS) and near infrared range (NIR)!
CCS811/BME280 (Qwiic) Environmental Combo Breakout Hookup Guide
Sense various environmental conditions such as temperature, humidity, barometric pressure, eCO2 and tVOCs with the CCS811 and BME280 combo breakout board.
Sensor Kit Resource Hub
An overview of each component in the SparkFun Sensor Kit, plus links to tutorials and other resources you'll need to hook them up.
I2C
An introduction to I2C, one of the main embedded communications protocols in use today.