Hookup Guide for the Qwiic Motor Driver

≡ Pages
Contributors: Ell C

Introduction

The Qwiic Motor Driver takes all the great features of the Serial Controlled Motor Driver and mini-sizes them, adding Qwiic ports for plug and play functionality. Boasting the same PSOC and 2-channel motor ports, the QWIIC Motor Driver is designed to communicate over I2C, but UART is also available.

SparkFun Qwiic Motor Driver

ROB-15451
$23.78

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

Suggested Reading

If you aren’t familiar with the following concepts, we recommend you read over these tutorials before continuing.

Serial Communication

Asynchronous serial communication concepts: packets, signal levels, baud rates, UARTs and more!

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

Motors and Selecting the Right One

Learn all about different kinds of motors and how they operate.

Logic Levels

Learn the difference between 3.3V and 5V devices and logic levels.

Bi-Directional Logic Level Converter Hookup Guide

An overview of the Bi-Directional Logic Level Converter, and some example circuits to show how it works.

Serial Controlled Motor Driver Hookup Guide

Hookup guide for the Serial Controlled Motor Driver

Hardware Overview

Let's look at some of the various features of the hardware.

Features:

  • 1.5 A peak drive per channel, 1.2 A steady state
  • Operates from 3 to 11 volts with 12v absolute max
  • 3.3V default VCC and logic
  • 127 levels of DC drive strength.
  • Controllable by I2C or TTL UART signals
  • Direction inversion on a per motor basis
  • Global Drive enable
  • Exposed small heat sink shape
  • Several I2C addresses, default UART bauds available

Front of Qwiic Motor Driver

Power

There are two separate power circuits on this board . Power for the motors is supplied through the VIN Connectors - you can provide anywhere from 3.3V to 11V to the "MAX 11V" and "GND" connections. Power for the PSOC and logic circuits is provided by the 3.3V inputs on the Qwiic connectors. Both are needed for proper functioning.

VIn inputs

Motor Power Ports: Ground (Left) - VIN(Right)

Qwiic Connectors

There are two Qwiic connectors on the board such that you can provide power or daisy-chain the boards should you choose to do so. If you're unfamiliar with our Qwiic system, head on over to our Qwiic page to see the advantages!

Qwiic connectors on either side of the board

Motor Ports

The screw pin terminals at the top of the board allow for two motor connections. They are labeled on the backside of the board.

Screw terminals for motor inputs

From left to right on the front: B2-B1-A2-A1

Function / Connection
Group Name Direction Description UART I2C
Motor Port A1 O Winding of first addressable location Motor A winding
A2 O Winding of first addressable location Motor A winding
B1 O Winding of second addressable location Motor B winding
B2 O Winding of second addressable location Motor B winding

Jumpers

Jumper Usage Table

There are 2 sets of jumpers to configure on this board. There are pull-up enables for I2C and 4 config bits that select operational mode.

Name Description Usage
I2C Jumpers I2C pull-up enable Opening these disables theI2C pull-up resistors used for I2C communication. If multiple I2C devices are being used, these pull-ups should be disabled on all but one device. If UART is being used, the pull-up resistors should be disabled.
Address Jumpers Serial and function selection The config bits are 4 bits that form a configuration nybble. A closed jumper is a '1' and an open jumper is a '0'. See config table for more information.

I2C Pull-Up Jumpers

I2C Jumpers on the lower right side of the back of the board

Address Bits

The configuration is set by encoding a number into the 4 config bits on the bottom of the board. Close a jumper to indicate a 1, or leave it open to indicate a 0.

Address jumpers on the back of the board

Use this table to see what the user port, address, and expansion port will become in each configuration:

Pattern Mode User Port User Address Expansion Port
0000 UART at 9600 UART N/A Master
0011 I2C I2C 0x58 Master
0100 I2C I2C 0x59 Master
0101 I2C I2C 0x5A Master
0110 I2C I2C 0x5B Master
0111 I2C I2C 0x5C Master
1000 I2C I2C 0x5D Master
1001 I2C I2C 0x5E Master
1010 I2C I2C 0x5F Master
1011 I2C I2C 0x60 Master
1100 I2C I2C 0x61 Master
1101 UART at 57600 UART N/A Master
1110 UART at 115200 UART N/A Master
1111 N/A Reserved N/A N/A

Bold text is the default setting for the Qwiic Motor Driver

Thermal Conduction Area

The Qwiic Motor Driver is designed to operate small robot drive motors without a heatsink; we were able to run up to about 1.1A continuous current without going above 100°C. If you find that you need a heatsink, you can use our Theragrip Thermal Tape to attach three Small Heat Sinks across the thermal conduction area on the back of the board.

Thermal conduction area on the back of the board

If you need more information on how to determine whether or not you need a heat sink, kick on over to the Serial Controlled Motor Driver Hookup Guide and scroll down to Typical Application Motors and Heat Sinking.

Small heatsinks on the back of the Qwiic Motor Driver

Small Heatsinks on the back of the Qwiic Motor Driver

Board Dimensions

All measurements are in inches. The Qwiic Motor Driver PCB measures 1x1 inch, with slight overhangs for the power and motor screw terminals.

Board Dimensions

Software Setup

Note: This code/library has been written and tested on Arduino IDE version 1.8.5. Otherwise, make sure you are using the latest stable version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

Installing Arduino

If you haven't used the Arduino IDE before, head on over to our Installing the Arduino IDE tutorial to get set up:

Installing Arduino IDE

March 26, 2013
A step-by-step guide to installing and testing the Arduino software on Windows, Mac, and Linux.

Getting the Arduino Library

The Qwiic Motor Driver uses the same Arduino Library as the Serial Controlled Motor Driver (hereafter referred to as SCMD). To get the Arduino library, either download and install it from Github or use the Arduino Library Manager.

Download the Github repository

Visit the GitHub repository to download the most recent version of the library, or click the link below:

Use the library manager or install in the Arduino IDE

In the Library Manager, search for Serial Controlled Motor Driver. For help installing the library, check out our How To Install An Arduino Library tutorial.

Installing an Arduino Library

January 11, 2013
How do I install a custom Arduino library? It's easy! This tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries not linked with the Arduino IDE, we will also go over manually installing an Arduino library.

Experiment 1: Testing the Motors

Let's start by hooking up some motors and making sure they're running. Since the Qwiic Motor Driver uses the same PSOC as the Serial Controlled Motor Driver, the same examples will work with minor modifications.

Hardware Hookup

Hardware Hookup Fritzing image Experiment 1

Click the image for a closer look

Testing the Motors

The following test is essentially the TwoMotorRobot.ino example from the SCMD library, but with a few minor changes to account for the defaults of the Qwiic Motor Driver.

Copy and paste the following code into your Arduino browser and upload.

language:c
//This example drives a robot in left and right arcs, driving in an overall wiggly course.
//  It demonstrates the variable control abilities. When used with a RedBot chassis,
//  each turn is about 90 degrees per drive.
//
//  Pin 8 can be grounded to disable motor movement, for debugging.

#include <Arduino.h>
#include <stdint.h>
#include "SCMD.h"
#include "SCMD_config.h" //Contains #defines for common SCMD register names and values
#include "Wire.h"

SCMD myMotorDriver; //This creates the main object of one motor driver and connected peripherals.

void setup()
{
  pinMode(8, INPUT_PULLUP); //Use to halt motor movement (ground)

  Serial.begin(9600);
  Serial.println("Starting sketch.");

  //***** Configure the Motor Driver's Settings *****//
  //  .commInter face is I2C_MODE 
  myMotorDriver.settings.commInterface = I2C_MODE;

  //  set address if I2C configuration selected with the config jumpers
  myMotorDriver.settings.I2CAddress = 0x5D; //config pattern is "1000" (default) on board for address 0x5D

  //  set chip select if SPI selected with the config jumpers
  myMotorDriver.settings.chipSelectPin = 10;

  //*****initialize the driver get wait for idle*****//
  while ( myMotorDriver.begin() != 0xA9 ) //Wait until a valid ID word is returned
  {
    Serial.println( "ID mismatch, trying again" );
    delay(500);
  }
  Serial.println( "ID matches 0xA9" );

  //  Check to make sure the driver is done looking for peripherals before beginning
  Serial.print("Waiting for enumeration...");
  while ( myMotorDriver.ready() == false );
  Serial.println("Done.");
  Serial.println();

  //*****Set application settings and enable driver*****//

  //Uncomment code for motor 0 inversion
  //while( myMotorDriver.busy() );
  //myMotorDriver.inversionMode(0, 1); //invert motor 0

  //Uncomment code for motor 1 inversion
  while ( myMotorDriver.busy() ); //Waits until the SCMD is available.
  myMotorDriver.inversionMode(1, 1); //invert motor 1

  while ( myMotorDriver.busy() );
  myMotorDriver.enable(); //Enables the output driver hardware

}

#define LEFT_MOTOR 0
#define RIGHT_MOTOR 1
void loop()
{
  //pass setDrive() a motor number, direction as 0(call 0 forward) or 1, and level from 0 to 255
  myMotorDriver.setDrive( LEFT_MOTOR, 0, 0); //Stop motor
  myMotorDriver.setDrive( RIGHT_MOTOR, 0, 0); //Stop motor
  while (digitalRead(8) == 0); //Hold if jumper is placed between pin 8 and ground

  //***** Operate the Motor Driver *****//
  //  This walks through all 34 motor positions driving them forward and back.
  //  It uses .setDrive( motorNum, direction, level ) to drive the motors.

  //Smoothly move one motor up to speed and back (drive level 0 to 255)
  for (int i = 0; i < 256; i++)
  {
    myMotorDriver.setDrive( LEFT_MOTOR, 0, i);
    myMotorDriver.setDrive( RIGHT_MOTOR, 0, 20 + (i / 2));
    delay(5);
  }
  for (int i = 255; i >= 0; i--)
  {
    myMotorDriver.setDrive( LEFT_MOTOR, 0, i);
    myMotorDriver.setDrive( RIGHT_MOTOR, 0, 20 + (i / 2));
    delay(5);
  }
  //Smoothly move the other motor up to speed and back
  for (int i = 0; i < 256; i++)
  {
    myMotorDriver.setDrive( LEFT_MOTOR, 0, 20 + (i / 2));
    myMotorDriver.setDrive( RIGHT_MOTOR, 0, i);
    delay(5);
  }
  for (int i = 255; i >= 0; i--)
  {
    myMotorDriver.setDrive( LEFT_MOTOR, 0, 20 + (i / 2));
    myMotorDriver.setDrive( RIGHT_MOTOR, 0, i);
    delay(5);
  }
}

What You Should See

The code goes through and establishes communication with the motor driver and then runs each motor in arcs, resulting in a "wiggly pattern".

Things to note:

  • Serial.begin is periodically run until the returned ID word is valid.
  • Setup waits for isReady() to become true before going on to the drive section
  • One motor is inverted by command at setup. Do it here so you don't have to mess with it later.
  • enable() is called to connect the drivers to the PWM generators.
  • LEFT_MOTOR and RIGHT_MOTOR are defined to ease use of the setDrive( ... ) function.

See the Arduino Library Reference section of the Serial Controlled Motor Driver Hookup Guide for more information on the functions defined in the Arduino library.

Experiment 2: Interactive Commands with UART

This example demonstrates the basic commands, plus some direct register access possible with only a UART available. This type of program could be easily run from a script from a more classic PC where I2C isn't available.

Interactive UART

Requirements

  • Computer serial terminal set to 9600 baud.
  • Terminal set to send CR and LF (Carriage return and line feed).
  • Config jumpers set to '0000', or all open.
  • I2C PU jumper fully open
  • FTDI Basic or Serial Basic - either will work but ensure you have the 3.3V version

Address Jumper 3 and I2C Pullup Jumpers are cut

Make sure the Address Jumper 3 and I2C Pullup Jumpers are cut as you see here.

Connect the FTDI to the Qwiic Motor Driver as you see in the Fritzing diagram below. Attach two motors to the driver, one between A1 and A2, and the other between B1 and B2.

Example 2 Fritzing image

Click the image for a closer look

Example Commands

When you're ready, make sure you have the correct COM port selected in your Arduino IDE, open a Serial Monitor, and send the following commands:

"R01"

This will read the ID register and return 0xA9

"M0F50"

This will tell motor 0 to drive at half speed, forward -- But nothing will happen yet!

"E"

This will enable all drivers. Motor 0 should begin spinning at half speed.

"M1R100"

This will tell motor 1 to drive at full speed in reverse. Now both should be spinning opposite directions.

"D"

D will disable both motors, which will stop spinning.

See the section UART Commands in the Serial Controlled Motor Driver Hookup Guide for a full command listing.

Troubleshooting

Resources and Going Further

Need inspiration? Check out some of the Qwiic or motor related tutorials!

SparkFun Edge Hookup Guide

Get to know your Edge board, including both the hardware features for you to utilize as well as how to get talking to it.

Garmin LIDAR-Lite v4 (Qwiic) Hookup Guide

Connecting the Garmin LIDAR-Lite v4 to a microcontroller just got easier! Check out our hookup guide to get started.

Temperature Sensor Comparison

A comparison of analog and digital temperature sensors. Which is better?

Qwiic Speaker Amp (TPA2016D2) Hookup Guide

The SparkFun Qwiic Speaker Amp includes the Texas Instruments TPA2016D2 stereo, filter-free class-D audio power amplifier. This tutorial will help you get started and configure the amplifer settings using an Arduino microcontroller.

Actobotics Basic Differential Platform

Get started with Actobotics with this simple vehicle. Then expand and customize it for your own evil robot empire.

Servo Trigger Hookup Guide

How to use the SparkFun Servo Trigger to control a vast array of Servo Motors, without any programming!

Shapeoko Coaster Project

A step-by-step guide to cutting and engraving a coaster with the Shapeoko.

Haptic Motor Driver Hook-Up Guide

Good vibes only. Getting started with the Haptic Motor Driver.

Or check out this blog post for some ideas.