WiFi
SparkFun Arduino UNO R4 WiFi Qwiic Kit Hookup Guide
The SparkFun Arduino UNO R4 WiFi Qwiic Kit is a great way to get started with Arduino and the Qwiic-connect system - use this guide to get started!
SparkFun RTK Reference Station Hookup Guide
Setup the RTK Reference Station in minutes and start sending RTCM NTRIP corrections to your favourite caster.
Getting Started with u-blox Thingstream and PointPerfect
Interested in high precision GNSS without setting up a base station?
Qwiic Kit for Raspberry Pi V2 Hookup Guide
Get started with the SGP40, BME280, VCNL4040, and microOLED via I2C using the Qwiic system and Python on a Raspberry Pi! Measure VOC Index, light, temperature, humidity, and pressure from the environment. Then display them on the microOLED, serial terminal, or the cloud with Cayenne!
Wireless Timing Project
Time for racing, let's make a wireless timing device using ESP32 wireless communication.
AzureWave Thing Plus (AW-CU488) Hookup Guide
The SparkFun AzureWave Thing Plus is a Feather form-factor development board equipped with the AW-CU488. We'll highlight key features of the board and show you to get started with the development board. A few Arduino examples will be highlighted to connect to a WiFi router, calculate the Fast Fourier Transform (FFT) from an input microphone, output an analog signal to a speaker, and connect an Qwiic-enabled device.
DA16200 Thing Plus Hookup Guide
A guide to get started with the DA16200 Thing Plus.
Getting Started with the DA16200 FreeRTOS SDK
Interested in the DA16200 FreeRTOS SDK? This guide covers setting up the SDK in the Eclipse IDE and how to program our boards with the DA16200 module.
IoT RedBoard ESP32 Development Board Hookup Guide
Delve into the functionality-rich world of the IoT RedBoard ESP32 Development Board!
ESP32 Thing Plus (USB-C) Hookup Guide
Meet the updated ESP32 Thing Plus (USB-C) development board. We have included some extra bells and whistles that users will appreciate, so check out out hookup guide for all the details!
Monitor Sensor Data from Anywhere
Using WiFi to send sensor data from an ESP32 to a WiFi network and be able to read it from an IoT Dashboard from anywhere in the world.
The 970-HA-JOKES Payphone Project
A payphone turned into a bit of fun.
SparkFun RTK Facet L-Band Hookup Guide
Setup the RTK Facet L-Band in minutes to begin gathering millimeter level geospatial coordinates.
Qwiic ToF Imager - VL53L5CX Hookup Guide
Hookup Guide for the Qwiic ToF Imager - VL53L5CX
Sending Sensor Data Over WiFi
This tutorial will show you how setup a simple peer-to-peer connection to send and receive sensor data between two ESP32 WiFi boards.
Getting Started with the Raspberry Pi Zero 2 W
Learn how to setup, configure and use the latest version of the smallest Raspberry Pi out there, the Raspberry Pi Zero 2 W.
SparkFun RTK Facet Hookup Guide
Setup the RTK Facet in minutes to begin gathering millimeter level geospatial coordinates.
MicroMod WiFi Function Board - ESP32 Hookup Guide
The MicroMod ESP32 Function Board adds additional wireless options to MicroMod Processor Boards that do not have that capability. This special function board acts as a coprocessor that takes advantage of Espressif's ESP32 WROOM to add WiFi and Bluetooth® to your applications.
MicroMod WiFi Function Board - DA16200 Hookup Guide
Add IoT functionality to any MicroMod project with the MicroMod WiFi function Board - DA16200!
smôl ESP32 Hookup Guide
Small in size, small on current draw. It's a smôl world! This guide will get you up and running with the smôl ESP32 Processor Board.
Dialog ULP WiFi DA16200 R3 Shield Hookup Guide
Add WiFi to your project with this hookup guide for our Dialog's Ultra Low Power DA16200 R3 shield!
ESP32-S2 Thing Plus Hookup Guide
Looking to use the more secure ESP32-S2? Follow this hookup guide to get started.
MicroMod ESP32 Processor Board Hookup Guide
A short hookup guide to get started with the SparkFun MicroMod ESP32 Processor Board.
MicroMod Machine Learning Carrier Board Hookup Guide
Get hacking with this tutorial on our Machine Learning Carrier Board!
Nintendo Switch Macro Recording on the Raspberry Pi
Learn how to record and playback controller 'macros' for your Nintendo Switch using a Raspberry Pi, SparkFun Top pHAT, and Joycontrol.
How to Make a Magic Mirror with Raspberry Pi
Need a great project for your Raspberry Pi 4 kit? Use it to create a command center to display the weather, clock, your calendar, or even a news feed!
Adding WiFi to the NVIDIA Jetson
Step by step instructions for setting up and installing the Edimax N150 USB WiFi/BLE adapter on your NVIDIA Jetson Nano
Assembly Guide for SparkFun JetBot AI Kit V2.0
Assembly Guide for the SparkFun JetBot AI Kit v2.0. This tutorial includes photos & comments to assemble the two-layer chassis & additional components unique to the JetBot kit.
Raspberry Pi 4 Kit Hookup Guide
Guide for hooking up your Raspberry Pi 4 Model B basic, desktop, or hardware starter kit together.
Getting Started with the Autonomous Kit for the Sphero RVR
Want to get started in robotics? Look no further than the SparkFun autonomous kit for the Sphero RVR! Whether you purchased the Basic or Advanced kit, this tutorial will get you rolling...
Basic Autonomous Kit for Sphero RVR Assembly Guide
Get your Basic Autonomous Kit for Sphero RVR all hooked up with this guide!
Advanced Autonomous Kit for Sphero RVR Assembly Guide
Get your Advanced Autonomous Kit for the Sphero RVR built up with this hookup guide!
ESP32 Relay Web Server
The goal of this project is to have a website hosted on an ESP32 that controls any relay controlled device connected to a local network and keeps a dynamically updated state of those devices.
SparkFun ESP32 DMX to LED Shield
Learn how to utilize your DMX to LED Shield in a variety of different ways.
ESP32 Thing Plus Hookup Guide
Hookup guide for the ESP32 Thing Plus (Micro-B) using the ESP32 WROOM's WiFi/Bluetooth system-on-chip in Arduino.
AST-CAN485 WiFi Shield Hookup Guide
Hookup Guide for the AST-CAN485 WiFi Shield.
Three Quick Tips About Using U.FL
Quick tips regarding how to connect, protect, and disconnect U.FL connectors.
SparkFun WiFi IR Blaster Hookup Guide
How to assemble the WiFi IR Blaster and program it using Arduino. You'll be controlling IR devices from the web in no time!
SparkFun LoRa Gateway 1-Channel Hookup Guide
How to setup and use the LoRa Gateway 1-Channel in Arduino.
Introduction to MQTT
An introduction to MQTT, one of the main communication protocols used with the Internet of Things (IoT).
ESP32 LoRa 1-CH Gateway, LoRaWAN, and the Things Network
Using the ESP32 LoRa 1-CH Gateway as a gateway and device, and pushing data to The Things Network.
WiFi Controlled Robot
This tutorial will show you how to make a robot that streams a webcam to a custom website that can be remotely controlled.
Setting up a Raspberry Pi 3 as an Access Point
This guide will show you how to configure a Raspberry Pi as an access point and connect it to your local Ethernet network to share Internet to other WiFi devices.
Using Artnet DMX and the ESP32 to Drive Pixels
In this tutorial, we'll find out how to use Resolume Arena, a popular video jockey software, to control custom-made ArtNet DMX fixtures.
Using the PSoC 6 Pioneer Board with the Pioneer IoT Add-on Shield
Cypress's PSoC 6 Pioneer Board is a development tool for the powerful PSoC 6 processor. In this tutorial, we'll show you how to use the PSoC 6 Pioneer Board along with the SparkFun/Digi-Key Pioneer IoT Add-on Shield to send data to a Raspberry Pi via BLE or WiFi.
Using Flask to Send Data to a Raspberry Pi
In this tutorial, we'll show you how to use the Flask framework for Python to send data from ESP8266 WiFi nodes to a Raspberry Pi over an internal WiFi network.
Getting Started with the Raspberry Pi Zero Wireless
Learn how to setup, configure and use the smallest Raspberry Pi yet, the Raspberry Pi Zero - Wireless.
ESP32 Environment Sensor Shield Hookup Guide
SparkFun's ESP32 Environment Sensor Shield provides sensors and hookups for monitoring environmental conditions. This tutorial will show you how to connect your sensor suite to the Internet and post weather data online.
ESP32 Thing Power Control Shield Hookup Guide
This tutorial shows you how to get started with the ESP32 Thing Power Control Shield.
Logging Data to Google Sheets with the Tessel 2
This project covers how to log data to Google Sheets two ways: using IFTTT with a web connection or a USB pen drive and "sneakernet" without.
Internet of Things Experiment Guide
The SparkFun ESP8266 Thing Dev Board is a powerful development platform that lets you connect your hardware projects to the Internet. In this guide, we show you how to combine some simple components to remotely log temperature data, send yourself texts and control lights from afar.
ESP32 Thing Hookup Guide
An introduction to the ESP32 Thing's hardware features, and a primer on using the WiFi system-on-chip in Arduino.
Sunrise Machine with the Tessel 2
Are you to sleepy to enjoy a sunrise on a brisk morning? Yeah...us too! No worries, with a Webcam, a Tessel 2 and a bit of code you can sleep in and catch the sunrise at your leisure with the Sunrise Machine.
ReconBot with the Tessel 2
Build a robot with the Tessel 2 that you can control from a browser on your phone or laptop.
Environmental Monitoring with the Tessel 2
Build an air-conditioner monitoring device to collect environment information and store it in the cloud.
Getting Started with the Tessel 2
Get your Tessel 2 up and running by blinking and LED, the Hello World of embedded electronics.
Connectivity of the Internet of Things
An overview of the different protocols that can be used for the development of Internet of Things (IoT)-based projects.
Experiment Guide for the Johnny-Five Inventor's Kit
Use the Tessel 2 and the Johnny Five Inventors kit to explore the world of JavaScript enabled hardware through 14 awesome experiments!
Hazardous Gas Monitor
Build a portable gas monitor to check for dangerous levels of hazardous gases.
Sparcade: Edison as a Web Server for Browser Games
Turn the Intel® Edison into an access point that serves a simple browser-based game. High scores from the game are displayed on a character LCD.
Blynk Board Washer/Dryer Alarm
How to configure the Blynk Board and app to notify you when your washer or dryer is done shaking.
Getting Started with the SparkFun Blynk Board
How to provision a Blynk Board - get it connected to Wi-Fi and Blynk, so you can start Blynking!
Blynk Board Project Guide
A series of Blynk projects you can set up on the Blynk Board without ever re-programming it.
ESP8266 Powered Propane Poofer
Learn how Nick Poole built a WiFi controlled fire-cannon using the ESP8266 Thing Dev Board!
LED Cloud-Connected Cloud
Make an RGB colored cloud light! You can also control it from your phone, or hook up to the weather!
SparkFun Inventor's Kit for Edison Experiment Guide
Learn how to harness the power of the Intel® Edison using JavaScript to post data to the cloud, control electronics from smartphones, and host web pages that interact with circuits.
ESP8266 Thing Development Board Hookup Guide
An overview of SparkFun's ESP8266 Thing Development Board - a development board for the Internet of Things.
SparkFun Inventor's Kit for Photon Experiment Guide
Dive into the world of the Internet of Things with the SparkFun Inventor's Kit for Photon.
ESP8266 WiFi Shield Hookup Guide
Interface your Arduino with an ESP8266 to give it inexpensive access to your WiFi network and the Internet!
Photon IMU Shield Hookup Guide
Learn how to use the SparkFun Photon IMU Shield for your Photon device which houses an on-board LSM9DS1 system-in-a-chip that houses a 3-axis accelerometer, 3-axis gyroscope, and 3-axis magnetometer.
Photon Battery Shield Hookup Guide
The Photon Battery Shield has everything your Photon needs to run off, charge, and monitor a LiPo battery. Read through this hookup guide to get started using it.
Photon OLED Shield Hookup Guide
The Photon OLED Shield has everything you need to add a small yet crisp OLED screen to your Photon projects. This hookup guide will show you how to get started.
Electric Imp Breakout Hookup Guide
An electric imp HUG! Provides an overview of the imp card and breakout. Both hardware and firmware subjects are covered.
ESP8266 Thing Hookup Guide
An overview of SparkFun's ESP8266 Thing - a development board for the Internet of...Things. This tutorial explains the circuitry driving the board, and how to get it up and running in an Arduino environment.
General Guide to SparkFun Blocks for Intel® Edison
A general guide for using SparkFun Blocks for Intel® Edison in your next project!
Loading Debian (Ubilinux) on the Edison
How to load a Debian distribution (specifically Ubilinux) onto the Edison.
Edison Getting Started Guide
An introduction to the Intel® Edison. Then a quick walk through on interacting with the console, connecting to WiFi, and doing...stuff.
HID Control of a Web Page
Learn how to move a slider on a webpage and make a motor spin. We connect HTML and HID to read sensors and interface with the physical world.
WiFly Shield Hookup Guide
How to get the WiFly Shield up and running.
XBee WiFi Hookup Guide
An overview of Digi's WiFi XBees, and a quick how-to on getting them connected and interfacing with the cloud.