Photon Battery Shield Hookup Guide
Introduction
Free your Photon from its USB cable by powering it through the Photon Battery Shield. The Battery Shield has everything your Photon needs to run off, charge, and monitor a LiPo battery.
The Shield features two unique IC's: an MCP73831 charge controller and a MAX17043 LiPo fuel gauge. With them, you'll be able to charge your battery through USB and monitor its voltage and state-of-charge.
Covered In This Tutorial
The purpose of this hookup guide is to familiarize you with the hardware and software of the Photon Battery Shield. It's split into the following sections:
- Battery Shield Overview -- A quick overview of the components and features of the Photon Battery Shield.
 - Using and Charging a LiPo Battery -- Some tips and tricks for running off, and charging a LiPo battery with the Shield.
 - Using the MAX17043 LiPo Fuel Gauge -- Example code -- including a Particle library -- demonstrating how to read the voltage and state-of-charge outputs, plus other features of the MAX17043 IC.
 
Required Materials
The Photon Battery Shield equips your Photon with just about everything it should need to use a LiPo battery -- it even includes headers! Of course you'll need the Battery Shield and a Photon.
SparkFun Photon Battery Shield
DEV-13626Particle Photon (Headers)
WRL-13774The one thing the Battery Shield doesn't include is a battery. Our compatible LiPo batteries come in a variety of shapes and capacities -- the larger the battery, the longer it will last. Any of the following will work:
Lithium Ion Battery - 850mAh
PRT-00341Lithium Ion Battery - 2000mAh
PRT-08483Polymer Lithium Ion Battery - 400mAh
PRT-10718If you want to use a battery of your own, just make sure it's a single-cell (3.7V nominal, ~4.2V max) lithium-polymer (LiPo) or lithium-ion (Li+). Optimally, choose one that is terminated with a 2-pin PH-series JST connector, otherwise you may need to do some wire splicing.
If you don't already have one (or just want to stock up), you may also need a Micro-B USB Cable, which will come in handy when you need to recharge the battery. If you don't want to plug that cable into a computer, a USB Wall Charger is useful to have on hand.
Suggested Reading
Using the Photon Battery Shield doesn't require a whole lot of pre-existing knowledge. If you want to learn more about the foundational concepts in this tutorial, here are some guides we recommend:
- How to Power a Project -- Hopefully you've already figured this out, since you're reading a Battery Shield tutorial. This tutorial does have an enlightening section on battery power.
 - Battery Technologies -- Specifically, check out the section on Lithium Polymer batteries.
 - How Lithium Polymer Batteries are Made -- Learn everything you always wanted to know about what goes on behind the scenes at a battery factory.
 - I2C Communication -- I2C is a popular low-level, two-wire communication standard. This is what we'll use to communicate with the MAX17043 fuel gauge IC.
 
Battery Technologies
How to Power a Project
I2C
How Lithium Polymer Batteries are Made
Battery Shield Overview
Let's do a quick rundown of the Photon Battery Shield's hardware features. Here are some highlights of the board's main components:
- LiPo Connector (PH-Series JST) -- The battery goes here. This connector is polarized, so it'll only plug in the right way.
 - Photon Socket -- Each Photon comes pre-soldered with male headers, so all of our shields come pre-populated with female connectors on their top-side.
 - Photon Pin Breakouts -- Need more access to the Photon's I/O? These pin break-outs have that covered. These break outs are in the same place on each of our Photon Shields -- should you need to interface them together that way.
 - Photon Polarity Indicator -- Nothing's going to work if your Photon isn't plugged in correctly. These angled edges should match up to those on the Photon's PCB.
 - Charge LED Indicator -- This red LED will light up whenever the LiPo battery is being charged.
 
Flipping the Shield over reveals a few, less commonly-used features of the board:
- "Stackable" Male Pins -- Whether you want to plug the battery shield into more Photon shields, or use it in a breadboard, these male pins should do the job. If you don't need this feature, the pins can all be quickly beheaded by some flush cutters.
 - SMD Barrel Jack footprint -- This footprint allows you to add an SMD Barrel Jack to the Battery Shield's underside. This'll allow you to charge the battery with a 5V Wall Adapter, or even a Small Solar Panel. Just make sure your power source isn't higher than 5.5V.
 - I2C Pull-up Resistor Enable/Disable -- The Photon Battery Shield includes a pair of 10kΩ pull-up resistors on the SDA and SCL lines (D0 and D1). If you've got more I2C devices to connect, you may need to disable those. These jumpers are closed by default, but can be opened with a couple slices of a hobby knife.
 - Alert Interrupt Jumper -- The MAX17043 features a programmable interrupt output, which can fire whenever your battery gets below a set percentage of charge. This pin can be connected to the Photon's D6 pin by adding a blob of solder between these two pads. Note that this jumper is open by default, as other shields make use of D6.
 
Using and Charging a LiPo Battery
Before plugging your battery in, grab your Photon, and plug it into the battery shield. Make sure you line up the Photon's angled edges with the matching white silkscreen on the shield. The Photon's USB connector should be pointing out the same direction as the black JST connector.
Next, grab your LiPo battery and mate its white JST connector with the black one on the shield. These connectors are polarized, so you can only plug it in the right way.
If the battery had any charge, your Photon should turn on, and its RGB LED should begin being colorful. If it was already commissioned, your Photon should connect to your WiFi network. You can even load up the Particle Build IDE and truly start loading code over-the-air.
Charging the Battery through USB
Eventually your LiPo's power capacity will be drained, and it'll be time to charge it back up. To avoid any extra USB connectors, the Photon Battery Shield was designed to use the Photon's USB connector as a charge-source.
With the LiPo and Photon still connected to the Battery Shield, simply plug a Micro-B USB cable into your Photon (the other end of the USB cable can be plugged into a computer or USB wall adapter).
Once USB is attached, the red charge LED indicator should illuminate -- it'll remain lit up until the battery is fully charged.
(Optional) Charging the Battery through Barrel Jack
The Battery Shield provides additional options for charging your LiPo in an unpopulated barrel jack footprint. If you need to charge the LiPo sans-Photon, this may be the best option for you.
To add this feature, you'll need our Surface-Mount Barrel Jack, and some soldering tools. If you're a novice solderer, don't be scared off by the "SMD" soldering -- these joints are about as easy as it gets. Check out or soldering tutorial for some guidance.
The barrel jack's input should face out towards the edge of the board. Make sure you solder all four pads:
To charge a LiPo through this jack, you'll need a 5V power source -- our 5V Wall Adapter should do the trick. Or, if you really want to avoid wires, you can use our small, 0.45W solar panel, which will source up to 5V when it's nice and sunny.
If you don't want to solder the barrel jack on, but still have a 5V power source available, you can supply that voltage to the "VIN" and "GND" pins on the shield's header. This is a more advanced charge technique, and only recommended for more experienced users.
Using the MAX17043 LiPo Fuel Gauge
One of the most unique features of the Photon Battery Shield is the integrated MAX17043 LiPo fuel gauge. The MAX17043 sits between the battery and your Photon -- it uses a calibrated ADC to measure the battery voltage. Comparing that measured voltage against their "ModelGauge" algorithm, the IC can produce a state-of-charge (SOC) estimate, to give you an idea of what percentage remains of the battery charge.
Loading the SparkFunMAX17043 Library
The MAX17043 communicates over I2C, so coding an interface between the Photon and the fuel gauge can be a little tricky. Luckily, we've done the hard work for you! We've written a Particle library for the MAX17043. You can load it up in the Particle IDE by going to the "Libraries" tab, and searching for SparkFunMAX17043.
If you're using the desktop version of the IDE, Particle Dev, and still want to use the library, you can grab the latest version from our GitHub repository.
Running the MAX17043_Simple Example
After finding the library, navigate to "MAX17043_Simple.cpp" and click Use This Example -- the Build IDE will create a clone of this sketch in your "Code" tab.
You shouldn't have to change anything, just make sure your Photon is selected in the "Devices" tab, and click "Flash".
Once your Photon is running the code, there are two ways to view its data. One is to open a serial terminal (see our Serial Terminal Basics tutorial if you need help with this). Find your Photon's serial port number ("COM#" on Windows "/dev/tty.usbmodemXXXX" on Mac) and set the baud rate to 9600. The battery's voltage, state-of-charge, and alert status will stream by.
Since USB is plugged in, the voltage and percentage should steadily increase as the battery charges.
Alternatively, if you want to monitor the battery discharge, you can use the Photon's Internet-connectivity to view the battery voltage and charge status. First, though, you'll need to identify your Photon's device ID as well as your account's access token. The device ID can be found in Particle Build by clicking the '>' next to your device name.
Your access token can be found under the "Settings" tab.
Armed with those long strings of hex characters, open a new browser tab and navigate to:
https://api.particle.io/v1/devices/DEVICE_ID/voltage?access_token=ACCESS_TOKEN
Make sure to sub in the proper values for DEVICE_ID and ACCESS_TOKEN. If everything was entered correctly, you should see something like this:
Among the data in that JSON response is a "result" key, which shows the current voltage reading. You can also view the state-of-charge, and alert status by navigating to:
https://api.particle.io/v1/devices/DEVICE_ID/soc?access_token=ACCESS_TOKEN
and
https://api.particle.io/v1/devices/DEVICE_ID/alert?access_token=ACCESS_TOKEN
Yay Spark Variables!
Using the SparkFunMAX17043 Library
The SparkFunMAX17043 library is simple. There's some initialization required. Make sure to include the library, and in your setup() call lipo.begin().
language:c
#include "SparkFunMAX17043/SparkFunMAX17043.h" // Include the SparkFun MAX17043 library
void setup()
{
    // Set up the MAX17043 LiPo fuel gauge:
    lipo.begin(); // Initialize the MAX17043 LiPo fuel gauge
    // Quick start restarts the MAX17043 in hopes of getting a more accurate
    // guess for the SOC.
    lipo.quickStart();
}
Calling lipo.quickStart() will re-calibrate the MAX17043's ADC, and usually results in more accurate readings.
If you're using the library in Particle Build, make sure you go to the SPARKFUNMAX17043 library in the "Libraries" tab, select INCLUDE IN APP, and add it to your desired code file.
Reading Voltage and SoC
Two functions are used to read the MAX17043's voltage and state-of-charge values:
language:c
// lipo.getVoltage() returns a voltage value (e.g. 3.93)
voltage = lipo.getVoltage();
// lipo.getSOC() returns the estimated state of charge (e.g. 79%)
soc = lipo.getSOC();
Both functions return a float variable. lipo.getVoltage() should usually be between 0.0 and about 4.2. lipo.getSOC() should be somewhere between 0.0 and 100.0.
Using the Alert Interrupt
One of the MAX17043's nifty features is a programmable alert interrupt. You can tell it to trigger a flag whenever the state-of-charge falls below a certain threshold.
To set up the alert, use lipo.setThreshold([percentage]). For example:
language:c
lipo.setThreshold(15); // Set Alert threshold to 15%
...will set the alert threshold to 15%.
The alert status can be read in both software and hardware. To get the alert status in software, call lipo.getAlert(). This function will return 0 if the alert is not triggered, and 1 if it is.
As mentioned in the Battery Shield Overview section, a jumper on the bottom of the board can optionally be closed to connect the MAX17043's alert pin to Photon pin D6. This alert is active-low -- meaning it'll be HIGH when it's not triggered and LOW when the SoC has fallen below threshold.
Once an alert has been triggered, you'll need to clear it before it can fire again. That's what lipo.clearAlert() will do for you. Even if the SoC rises above the threshold, you'll still need to manually clear the alert.
Resources and Going Further
If you need any resources detailing the Photon Battery Shield, here are some schematics, datasheets, and other links you may find handy:
- Photon Battery Shield GitHub Repo
 - Photon Battery Shield Schematic
 - Particle Documentation Pages -- go here to set up and configure your Photon (or other Particle devices)
 - Particle Community Forum -- anything that you couldn't find in the docs should be easily found in the community forum. If you are having trouble, search this forum first, as many of the answers are there already.
 - MAX17043 LiPo Fuel Gauge Datasheet
 - MCP73831 Charge Controller Datasheet
 
If you are interested in putting your Photon into sleep mode to conserve more battery power, check out the Particle Docs links below:
- Photon System Modes - Playing with different modes allows you to have control over when the Photon is and isn't connected to the web.
 - Photon System Sleep Function - The sleep function puts the Photon to sleep while it isn't performing any actions to conserve power.
 
Now that you've become familiarized with the Photon Battery Shield, what project are you going to make with it? Need some inspiration? Check out the below SparkFun tutorials for some ideas:
HID Control of a Web Page
Are You Okay? Widget
ESP8266 Thing Hookup Guide
The Battery Shield pairs very well with any of our other Photon Shields; check out our hookup guides for those shields: