Audio

How to Play Multiple Buzzers at Once

October 18, 2024
This tutorial demonstrates the SparkFun Qwiic Buzzer's ability to control multiple buzzers simultaneously by playing a 3-part arrangement of a segment of the Super Mario Bros Theme!

Analog MEMS Microphone (VM2020) Hookup Guide

February 9, 2023
Get started with the SparkFun analog MEMS microphone breakout board! In this tutorial, we will be connecting the differential MEMS microphone to an Arduino using the WM8960 audio codec.

Audio Codec Breakout - WM8960 Hookup Guide

January 26, 2023
The SparkFun Audio Codec Breakout - WM8960 is a low power, high quality stereo codec chock full of features. In this tutorial, some of these features by using an Arduino microcontroller to configure the audio codec and pass audio to the headphone or speaker channels.

Qwiic Speaker Amp (TPA2016D2) Hookup Guide

September 29, 2022
The SparkFun Qwiic Speaker Amp includes the Texas Instruments TPA2016D2 stereo, filter-free class-D audio power amplifier. This tutorial will help you get started and configure the amplifer settings using an Arduino microcontroller.

AzureWave Thing Plus (AW-CU488) Hookup Guide

September 22, 2022
The SparkFun AzureWave Thing Plus is a Feather form-factor development board equipped with the AW-CU488. We'll highlight key features of the board and show you to get started with the development board. A few Arduino examples will be highlighted to connect to a WiFi router, calculate the Fast Fourier Transform (FFT) from an input microphone, output an analog signal to a speaker, and connect an Qwiic-enabled device.

The 970-HA-JOKES Payphone Project

July 11, 2022
A payphone turned into a bit of fun.

Analog MEMS Microphone Breakout - SPH8878LR5H-1 Hookup Guide

March 17, 2022
Get started with sound monitoring using the SparkFun analog MEMS microphone breakout board with Arduino!

Tinker Kit Circuit Guide

September 16, 2021
This guide takes you through the basics of building 11 different circuits with the SparkFun Tinker Kit and how to program them using the Arduino IDE.

Tsunami Super WAV Trigger Hookup Guide

August 25, 2021
This guide will get users started with the Qwiic Tsunami. We'll start by putting *.wav files and a configuration file on a microSD card, pop it into the Qwiic Tsunami, then trigger sounds across multiple outputs.

Red Hat Instrument Kit Hookup Guide

August 19, 2021
Get started with the Red Hat Instrument kit!

QuickLogic Thing Plus (EOS S3) Hookup Guide

July 22, 2021
This guide provides users with functional descriptions, configuration options for the QuickLogic Thing Plus EOS S3. It also serves as a “Getting Started” and “How To” guide.

MicroMod Artemis Processor Board Hookup Guide

October 21, 2020
Get started with the Artemis MicroMod Processor Board in this tutorial!

Spectrum Shield Hookup Guide (v2)

May 4, 2020
Want your project to react to music? Then the SparkFun Spectrum Shield is the product for you! Get going in no time with this Hookup Guide.

SparkFun Inventor's Kit Experiment Guide - v4.1

August 8, 2019
The SparkFun Inventor's Kit (SIK) Experiment Guide contains all of the information needed to build all five projects, encompassing 16 circuits, in the latest version of the kit, v4.1.2 and v4.1.

SparkFun gator:microphone Hookup Guide

June 13, 2019
The gator:microphone is an I2C sensor for detecting sound with an electret microphone. This tutorial will get you started using the gator:microphone with the micro:bit platform.

Build a Qwiic Jukebox that is Toddler Approved!

March 29, 2019
Follow this tutorial to build your own custom jukebox. Note, this is designed simple and tough for use primarily with toddlers. It's also a great introduction to SparkFun's Qwiic products!

SparkFun gator:bit v2 Hookup Guide

January 31, 2019
The gator:bit v2 is a breakout board for the BBC micro:bit. The gator:bit exposes almost every pin on the micro:bit to clippable pad with circuit protection. It also has as built-in addressable LEDs and a built-in buzzer.

Qwiic MP3 Trigger Hookup Guide

January 24, 2019
Playing MP3s has never been easier.

TSH82 Configurable OpAmp Hookup Guide

November 2, 2018
The TSH82 Configurable OpAmp board offers the designer a great balance of performance and flexibility. We'll show you how to get the very best out of your board!

I2S Audio Breakout Hookup Guide

September 6, 2018
Hookup guide for the MAX98357A I2S audio breakout board.

micro:bit Educator Lab Pack Experiment Guide

May 8, 2018
A quickstart guide for the micro:bit educator lab pack.

Little Soundie Audio Player Hookup Guide

April 26, 2018
Add sound effects to your project, prop or costume with Little Soundie Audio Player.

Papa Soundie Audio Player Hookup Guide

April 26, 2018
Add sound effects to your project, prop or costume with Papa Soundie Audio Player.

Noisy Cricket Stereo Amplifier - 1.5W Hookup Guide

April 26, 2018
A hookup guide for the Noisy Cricket Stereo Amplifier - 1.5W.

MIDI BLE Tutorial

February 22, 2018
Developing a bidirectional MIDI-BLE link with the nRF52832 Breakout.

Wireless Audio Bluetooth Adapter w/ BC127

December 14, 2017
Build a custom wireless audio Bluetooth adapter using BlueCreation's BC127 and add it to your old speaker system!

Clap On Lamp

November 28, 2017
Modify a simple desk lamp to respond to a double clap (or other sharp noise) using parts from the SparkFun Inventor's Kit v4.0.

Vibe-O-Matic 3000

November 28, 2017
We attempt to emulate a car seat to ease a baby to sleep.

SparkFun Inventor's Kit Experiment Guide - v4.0

November 15, 2017
The SparkFun Inventor's Kit (SIK) Experiment Guide contains all of the information needed to build all five projects, encompassing 16 circuits, in the latest version of the kit, v4.0a.

SparkFun Inventor's Kit for micro:bit Experiment Guide

July 21, 2017
This guide contains all the information you will need to explore the twelve circuits of the SparkFun Inventors Kit for micro:bit.

Spectacle Sound Kit Hookup Guide

May 4, 2017
All the information you need to use the Spectacle Sound Kit in one place.

Spectacle Audio Board Hookup Guide

May 4, 2017
All the information you need to use the Spectacle Audio Board in one place.

Spectacle Example: Super Mario Bros. Diorama

May 4, 2017
A study in building an animated diorama (with sound!) using Spectacle electronics.

Spectacle Light and Sound Kit Hookup Guide

May 4, 2017
All the information you need to use the Spectacle Light and Sound Kit in one place.

Introduction to Operational Amplifiers with LTSpice

April 18, 2017
Picking up where we left off in "Getting Started with LTSpice," we delve a little deeper into LTSpice through an introduction of Operational Amplifiers (OpAmps).

THAT InGenius and OutSmarts Breakout Hookup Guide

March 30, 2017
Learn about the benefits of balanced signal transmission, and how to apply the THAT InGenius and OutSmarts breakouts.

TeensyView Hookup Guide

March 16, 2017
A guide to using the TeensyView OLED board to display text and graphics.

Bark Back Interactive Pet Monitor

March 8, 2017
Monitor and interact with pets through this dog bark detector project based on the Raspberry Pi!

Tsunami Hookup Guide

February 16, 2017
Hit the ground running with Tsunami, the Super Wav Trigger.

MEMS Microphone Hookup Guide

January 27, 2017
Get started with the SparkFun analog MEMS microphone breakout board with Arduino! Create a volume unit meter with the ADMP401 or ICS-40180 to react to sound before building your sound visualizer!

Vox Imperium: Stormtrooper Voice Changer

October 25, 2016
Add some flair to your Imperial uniform by changing your voice using a Teensy 3.2 and Prop Shield.

Proto Pedal Example: Analog Equalizer Project

September 22, 2016
Building a gyrator-based analog equalizer using the Proto Pedal.

Proto Pedal Chassis Hookup Guide

September 22, 2016
Prepare the Proto Pedal Chassis by drilling holes for controls and painting it.

Proto Pedal Assembly and Theory Guide

September 22, 2016
Getting started with the SparkFun Proto Pedal. We'll assemble the board, then discuss some of the details of the circuit.

Proto Pedal Example: Programmable Digital Pedal

September 22, 2016
Building a pedal around the Teensy 3.2 and Teensy Audio shield. Changing the effect in the pedal is as easy as uploading a new sketch!

Electret Mic Breakout Board Hookup Guide

June 23, 2016
An introduction to working with the Electret Mic Breakout Board.

Hazardous Gas Monitor

June 17, 2016
Build a portable gas monitor to check for dangerous levels of hazardous gases.

Interactive LED Music Visualizer

May 31, 2016
Use an Arduino and the SparkFun Sound Detector to create visualizations on Addressable RGB LED strips.

SIK Keyboard Instrument

April 15, 2016
We can use the parts and concepts in the SparkFun Invetor's Kit to make a primitive keyboard instrument.

BadgerHack: Synth Add-On Kit

February 16, 2016
Make a tiny synth with BadgerStick.

MP3 Trigger Hookup Guide V24

January 21, 2016
Incorporate sound into your next project easily with the MP3 Trigger.

Sound Reactive EL Wire Costume

December 31, 2015
Learn how to make your EL wire costumes sound reactive in this project tutorial.

Touch Potentiometer Hookup Guide

October 22, 2015
Learn how to use the SparkFun Touch Potentiometer to control lighting, volume or other inputs in your daily life.

MIDI Tutorial

October 8, 2015
Understanding the Musical Instrument Digital Interface.

MIDI Shield Hookup Guide

October 8, 2015
How to assemble the SparkFun MIDI Shield, plus several example projects.

SparkFun Inventor's Kit for Photon Experiment Guide

September 3, 2015
Dive into the world of the Internet of Things with the SparkFun Inventor's Kit for Photon.

Making Music with the FreeSoC2

August 14, 2015
Create a synth keyboard with the FreeSoC2 from SparkFun.

Si4703 FM Radio Receiver Hookup Guide

August 13, 2015
Add some tunes to your project with the Si4703 FM Radio Receiver Breakout.

Experiment Guide for RedBot with Shadow Chassis

May 28, 2015
This Experiment Guide offers nine experiments to get you started with the SparkFun RedBot. This guide is designed for those who are familiar with our SparkFun Inventor's Kit and want to take their robotics knowledge to the next level.

Hackers in Residence: The Sound Visualizer Pt. 2

May 7, 2015
An addition to a previous project, this time using a PC and a custom Java app to create your own music visualizer using a RGB LED matrix.

Bare Conductive Musical Painting

May 5, 2015
Learn how to make a musical painting using the Bare Conductive Touch Board and Conductive Paint.

Rotary Switch Potentiometer Hookup Guide

April 30, 2015
How to use the Rotary Switch Potentiometer breakout board, with some sample applications.

MP3 Player Shield Hookup Guide V15

April 6, 2015
How to get your Arduino groovin' using the MP3 Player Shield.

Hackers in Residence: The Sound Visualizer

March 23, 2015
A fun project that uses a Raspberry Pi and a custom Java app to create your own sound visualizer using a RGB LED matrix.

RedBoard Santa Trap

December 25, 2014
A fun holiday project to try for anyone looking to catch Santa on Christmas!

Cackling Apple Head Witch

October 30, 2014
Make your own cackling apple head witch to scare all of the trick or treaters this Halloween!

SparkPunk Sequencer Theory and Applications Guide

August 14, 2014
Examine the inner workings of the SparkPunk Sequencer, then explore some modifications and alternate applications.

SparkPunk Sequencer Hookup Guide

August 14, 2014
How to assemble and use the SparkPunk Sequencer kit.

Hackers in Residence - The ElectricBone

June 25, 2014
Drum machines and keyboards have been the standard for making digital music, but how do you make electronic music if you're trained to play the trombone? One of our Hackers in Residence, Carlos Mello, took it upon himself to find a solution to that very question.

SparkPunk Hookup Guide

June 12, 2014
How to assemble and modify the SparkPunk Sound Generator kit.

WAV Trigger Hookup Guide V11

May 30, 2014
An introduction to being able to trigger music and sound effects based on buttons, sensors, or switches using the WAV Trigger board.

MiniGen Hookup Guide

May 22, 2014
Using the MiniGen, SparkFun's Arduino Pro Mini signal generator shield

Interactive Hanging LED Array

April 10, 2014
Learn how we converted 72 lightbulbs into an interactive LED array for our conference room.

Binary Blaster Assembly Guide

March 13, 2014
Learn how to assemble and play the Binary Blaster Game from SparkFun Electronics.

Build an Auduino Step Sequencer

March 6, 2014
Make a Step Sequencer using an Arduino, the Auduino firmware, and a handful of hardware.

Sound Detector Hookup Guide

February 27, 2014
The Sound Detector is a microphone with a binary output. This guide explains how it works and how you can use it in your projects.

Understanding the BC127 Bluetooth Module

January 31, 2014
SparkFun has two boards using the BC127; here's what you need to know to use them.

Dot/Bar Display Driver Hookup Guide

January 16, 2014
How to hook up the LM3914 or LM3916 to drive a 10-LED display with a lone analog signal.

My Drunk Kitchen Apron

September 5, 2013
A fun project that uses the LilyPad MP3 trigger. This apron will dispense helpful kitchen advice and humor from the host of My Drunk Kitchen, Hannah Harto!

RN-52 Bluetooth Hookup Guide

August 29, 2013
A hookup guide to get you started with the RN-52 Audio Bluetooth Module Breakout Board.

Si4707 Hookup Guide

May 29, 2013
Instructions on hooking up to and communicating with the Si4707 Weather Band Radio Breakout using an Arduino.

Getting Started with the LilyPad MP3 Player

May 8, 2013
The LilyPad MP3 Player is an amazing little board that contains almost everything you need to play audio files. You can use it to create all kinds of noisy projects, from MP3 hoodies to talking teddy bears. Your imagination is the only limit! This tutorial will help you get started.

The Uncertain 7-Cube

March 8, 2013
The Uncertain 7-Cube is a non-committal, less-than-helpful, but also entirely honest fortune teller. Simply ask it a yes or no question, give it a nudge, and the 7-Cube will dutifully inform you that it doesn’t have all the facts and doesn’t feel comfortable making a guess.

MP3 Player Shield Music Box

January 21, 2013
Music Box Project based on the Dr. Who TARDIS.

Old Tutorials

Looking for the old, archived tutorials? Head on over to the archived tutorials on the main SparkFun site.
Please be aware that the tutorials you find there are no longer actively maintained.