ATtiny
Thing Plus Dual-Port Logging Shield Hookup Guide
This tutorial shows you how to hook up and use the SparkFun Thing Plus Dual-Port Logging Shield.
SparkFun Qwiic Dual Solid State Relay Hookup Guide
A Hookup Guide to get you started with the SparkFun Qwiic Dual Solid State Relay.
SparkFun Qwiic Quad Solid State Relay Kit Hookup Guide
A Hookup Guide to get you started with the SparkFun Qwiic Quad Solid State Relay Kit (say that five times fast!).
SparkFun Qwiic Button Hookup Guide
A Hookup Guide for the SparkFun Qwiic Button (Red) and SparkFun Qwiic Button Breakout. Goes over connecting the Qwiic Button to an Arduino microcontroller and using it with the Qwiic Button Arduino library.
Qwiic Keypad Hookup Guide
If you are tired of taking up GPIO pins, wiring a bunch of pull up resistors, and using firmware that scans the keys taking up valuable processing time... check out the new Qwiic Keypad.
SparkFun Qwiic RFID-IDXXLA Hookup Guide
The Qwiic RFID ID-XXLA is an I2C solution that pairs with the ID-LA modules: ID-3LA, the ID-12LA, or the ID-20LA, and utilizes 125kHz RFID chips. Let's take a look at the hardware used for this tutorial.
Qwiic Joystick Hookup Guide
Looking for an easy way to implement a joystick to your next Arduino or Raspberry Pi project? This hookup guide will walk you through using the Qwiic Joystick with the Arduino IDE on a RedBoard Qwiic and in Python on a Raspberry Pi.
Qwiic MP3 Trigger Hookup Guide
Playing MP3s has never been easier.
Qwiic Quad Relay Hookup Guide
SparkFun’s Qwiic Quad Relay is a product designed for switching not one but four high powered devices from your Arduino or other low powered microcontroller using I2C.
Qwiic Single Relay Hookup Guide
Get started switching those higher power loads around with the Qwiic Single Relay.
Qwiic Twist Hookup Guide
Take your volume knob beyond 11 with the Qwiic Twist digital RGB LED encoder via I2C!
Pi AVR Programmer HAT Hookup Guide
In this tutorial, we will use a Raspberry Pi 3 and the Pi AVR Programmer HAT to program an ATMega328P target. We are going to first program the Arduino bootloader over SPI, and then upload an Arduino sketch over a USB serial COM port.
Atto84 Hookup Guide
A bare minimum Arduino compatible breakout using a ATtiny84 for integration into your small projects!
Night Sky Halloween Costume
Make a beautiful night sky costume using the LilyPad LEDs and the LilyTiny.
Twinkle Zodiac Constellation
Create a quick and easy piece of e-textile art based on a Zodiac sign using a LilyTiny, LilyPad LEDs, battery holder, conductive thread, and coin cell battery.
Roshamglo Hookup Guide
This tutorial provides everything you need to know to get started with the Roshamglo badge.
Hack Your Roshamglo Badge
Learn how to customize and program your Roshamglo badge.
Roshamglo Project: TV-B-Gone
Turn your Roshamglo board into a (nearly) universal TV power button.
How to Install an ATtiny Bootloader With Virtual USB
With this, you will be able to upload Arduino sketches directly to the ATtiny84 over USB without needing to use a programming device (such as another Arduino or FTDI chip).
Electronic E-craft Terrarium
A guest tutorial on an Electronic Terrarium from the Performative Sculpture class of Parsons DT.
Light Up Pennant with E-Textiles
Show your school spirit, geek pride, or fandom with a light up pennant using the LilyTwinkle or LilyPad Arduino.
Wake-on-Shake Hookup Guide
A basic hookup guide for getting started with the SparkFun Wake-on-Shake. The board gives you the ability to put your project into hibernation until bumped or shaken awake using the ADXL362 accelerometer. This means you can design projects meant to stay inert for long periods of time, possibly even several years, depending on the battery type used to power the project.
LilyTiny Plush Monster
Craft a stuffed monster while exploring the LilyTiny preprogrammed microcontroller. This is a project based on the Plush Monster Activity created at MIT's High-Low Tech Lab by Emily Lovell, Jie Qi, and Natalie Freed.
Twinkling Trick or Treat Bag
Make a light up goodie bag with conductive thread, LEDs, and the LilyTwinkle!
Re-Programming the LilyTiny / LilyTwinkle
A quick tutorial showing how to reprogram the ATtiny85 IC found on the LilyTiny or LilyTwinkle boards.
Installing a Bootloader on the MicroView
Fix your bootloader-less MicroView! This tutorial covers how to: disassemble the MicroView, wire it up to an assortment of programmers, program the bootloader, and test it out.
Pocket AVR Programmer Hookup Guide
Skip the bootloader and load your program directly onto an AVR with the AVR Pocket Programmer.
Tiny AVR Programmer Hookup Guide
A how-to on the Tiny AVR Programmer. How to install drivers, hook it up, and program your favorite Tiny AVRs using AVRDUDE!
LDK Experiment 6: Microcontroller Circuits
Learn how to build a simple microcontroller circuit using the pre-programmed LilyTiny Board
Firefly Jar Assembly Guide
Make a soft circuit firefly jar with conductive thread, LEDs, and the LilyTwinkle!
The Uncertain 7-Cube
The Uncertain 7-Cube is a non-committal, less-than-helpful, but also entirely honest fortune teller. Simply ask it a yes or no question, give it a nudge, and the 7-Cube will dutifully inform you that it doesn’t have all the facts and doesn’t feel comfortable making a guess.
Soft Circuits: LED Feelings Pizza
Here we will learn how to say how you feel with pizza. Electric pizza.