Weather

Monitor your environment and log it to the cloud by building your own personal weather station! Or pull data from a server to check out the forecast in your area. Check out the following tutorials to start reading temperature, humidity, pressure, UV, ambient light, hazardous gases, water levels, wind speed and direction, soil moisture, TVOC, eCO2, and even lightning in your environment!

SparkFun Thing Plus - NINA-B306 Hookup Guide

March 23, 2023
A quick guide to get started using the SparkFun Thing Plus - NINA-B306. This Thing Plus is loaded with the Arm Cortex-M4 processor in the NINA-B306 along with on-board motion and environmental sensors in the ISM330DHCX 6DoF and BME280 pressure and temperature sensor.

Qwiic Kit for Raspberry Pi V2 Hookup Guide

December 29, 2022
Get started with the SGP40, BME280, VCNL4040, and microOLED via I2C using the Qwiic system and Python on a Raspberry Pi! Measure VOC Index, light, temperature, humidity, and pressure from the environment. Then display them on the microOLED, serial terminal, or the cloud with Cayenne!

SparkFun Absolute Digital Barometer - LPS28DFW (Qwiic) Hookup Guide

December 8, 2022
Get started adding water-resistant pressure sensing using the SparkFun Absolute Digital Barometer - LPS28DFW (Qwiic) following this guide.

SparkFun Indoor Air Quality Sensor - ENS160 (Qwiic) Hookup Guide

November 11, 2022
Is your air safe? Check your eCO2, TVOC, and AQI levels with the new SparkFun Indoor Air Quality Sensor - ENS160!

Qwiic Pressure Sensor (BMP581) Hookup Guide

July 14, 2022
Get started with the SparkFun Pressure Sensor - BMP581 (Qwiic) following this Hookup Guide

Qwiic Pressure Sensor (BMP384) Hookup Guide

June 2, 2022
Get started with the SparkFun Pressure Sensor - BMP384 (Qwiic) following this guide.

Artemis Global Tracker Hookup Guide

December 9, 2021
The SparkFun Artemis Global Tracker combines the Artemis processor with an Iridium 9603N satellite transceiver, ZOE-M8Q GNSS transceiver, and MS8607 PHT sensor. With a clear view of the sky, this board allows you to send and receive short data messages from anywhere in the world including remote locations far beyond the reach of WiFi and GSM networks. Follow this guide to get started with the Artemis Global Tracker.

MicroMod Environmental Function Board Hookup Guide

November 11, 2021
The SparkFun MicroMod Environmental Function Board adds additional sensing options to the MicroMod Processor Boards. This function board includes three sensors to monitor air quality (SGP40), humidity & temperature (SHTC3), and CO2 concentrations (STC31) in your indoor environment. To make it even easier to use, all communication is over the MicroMod's I2C bus! In this tutorial, we will go over how to connect the board and read the sensors.

Digital Temperature Sensor Breakout - AS6212 (Qwiic) Hookup Guide

September 9, 2021
Get started measuring highly accurate temperatures at extremely low power with the AS6212 temperature sensor on the SparkFun Digital Temperature Sensor Breakout - AS6212 (Qwiic).

MicroMod Weather Carrier Board Hookup Guide

January 14, 2021
A quick guide to help to create your own MicroMod weather station using the MicroMod Weather Carrier Board and Processor of your choice.

Qwiic Digital Indoor Thermometer

July 15, 2020
Qwiic-ly build a digital indoor thermometer to measure the ambient temperature of the room and display it using an OLED on an I2C bus!

How to Make a Magic Mirror with Raspberry Pi

June 17, 2020
Need a great project for your Raspberry Pi 4 kit? Use it to create a command center to display the weather, clock, your calendar, or even a news feed!

SparkFun Air Quality Sensor - SGP30 (Qwiic) Hookup Guide

June 5, 2020
A hookup guide to get started with the SparkFun Air Quality Sensor - SGP30 (Qwiic).

SparkFun Environmental Sensor Breakout - BME68x (Qwiic) Hookup Guide

May 14, 2020
A hookup guide to get started with the BME68x Environmental Sensor from Bosch. Monitor the air quality, temperature, humidity, and barometric pressure with this Qwiic sensor!

Wireless Remote Weather Station with micro:bit

May 11, 2020
Monitor the weather without being exposed to it through wireless communication between two micro:bits using the radio blocks! This is useful if your weather station is installed in a location that is difficult to retrieve data from the OpenLog. We will also explore a few different ways to send and receive data.

SparkFun Humidity Sensor Breakout - SHTC3 (Qwiic) Hookup Guide

May 7, 2020
A Hookup Guide to get started using the SHTC3 breakout.

Qwiic TMP117 High Precision Digital Temperature Sensor Hookup Guide

November 14, 2019
Add a high precision, digital temperature sensor to your projects using the TMP117 over the I2C!

SparkFun gator:UV Hookup Guide

September 5, 2019
The gator:UV is an I2C based UV sensor. This tutorial will get you started using the gator:UV with the micro:bit platform.

Qwiic Atmospheric Sensor (BME280) Hookup Guide

August 21, 2019
Measure temperature, humidity, barometric pressure with the SparkFun Atmospheric Sensor Breakout BME280 (Qwiic).

SparkFun AS3935 Lightning Detector Hookup Guide (v20)

July 25, 2019
Are you worried about the looming clouds in the distance, how far away is that storm exactly? Add lightning detection with the AS3935 to your next weather station or your next bike ride!

Qwiic Ambient Light Sensor (VEML6030) Hookup Guide

July 18, 2019
The VEML6030 is a high accuracy ambient light sensor with 16-bit resolution. This I2C sensor can detect light similar to the human eye response. Start detecting light levels in your environment!

SparkFun gator:environment Hookup Guide

June 13, 2019
The gator:environment combines two I2C sensors for temperature, humidity, pressure, eCO2, and eTVOC values. This tutorial will get you started using the gator:environment with the micro:bit platform.

SparkFun gator:soil Hookup Guide

June 13, 2019
The gator:soil is analog soil moisture sensor. This tutorial will get you started using the gator:soil with the micro:bit platform.

SparkFun gator:particle Hookup Guide

June 13, 2019
The gator:particle is an I2C heart-rate monitor and pulse oximeter that can be used as a particle sensor. This tutorial will get you started using the gator:particle with the micro:bit platform.

RHT03 (DHT22) Humidity and Temperature Sensor Hookup Guide

March 12, 2019
Measure relative humidity and temperature or your environment with the RHT03 (a.k.a DHT22) low cost sensor on a single wire digital interface connected to an Arduino!

Qwiic UV Sensor (VEML6075) Hookup Guide

December 20, 2018
Learn how to connect your VEML6075 UV Sensor and figure out just when you should put some sunscreen on.

Spectral Triad (AS7265x) Hookup Guide

November 8, 2018
Learn how to wield the power of 18 channels of UV to NIR spectroscopy with AS72651 (UV), AS72652 (VIS), and AS72653 (NIR) sensors!

CCS811/BME280 (Qwiic) Environmental Combo Breakout Hookup Guide

September 8, 2017
Sense various environmental conditions such as temperature, humidity, barometric pressure, eCO2 and tVOCs with the CCS811 and BME280 combo breakout board.

micro:climate Kit Experiment Guide

July 21, 2017
A weather station kit that is built on top of the inexpensive, easy-to-use micro:bit and Microsoft MakeCode.

Weather Meter Hookup Guide

July 20, 2017
How to assemble your very own weather meter!

ESP32 Environment Sensor Shield Hookup Guide

July 6, 2017
SparkFun's ESP32 Environment Sensor Shield provides sensors and hookups for monitoring environmental conditions. This tutorial will show you how to connect your sensor suite to the Internet and post weather data online.

CCS811 Air Quality Breakout Hookup Guide

April 27, 2017
This tutorial shows you how to get data from a CCS811 breakout board with the I2C interface.

Arduino Weather Shield Hookup Guide V12

March 2, 2017
Read humidity, pressure and luminosity quickly and easily. Add wind speed, direction and rain gauge for full weather station capabilities.

TMP102 Digital Temperature Sensor Hookup Guide

February 2, 2017
How to connect and use the SparkFun Digital Temperature Sensor Breakout - TMP102 with an Arduino.

HIH-4030 Humidity Sensor Hookup Guide

December 6, 2016
Measure relative humidity with SparkFun's HIH-4030 Humidity Sensor Breakout.

MAX30105 Particle and Pulse Ox Sensor Hookup Guide

December 1, 2016
The SparkFun MAX30105 Particle Sensor is a flexible and powerful sensor enabling sensing of distance, heart rate, particle detection, even the blinking of an eye. Get ready. Set. Shine!

Environmental Monitoring with the Tessel 2

October 13, 2016
Build an air-conditioner monitoring device to collect environment information and store it in the cloud.

Experiment Guide for the Johnny-Five Inventor's Kit

June 28, 2016
Use the Tessel 2 and the Johnny Five Inventors kit to explore the world of JavaScript enabled hardware through 14 awesome experiments!

Hazardous Gas Monitor

June 17, 2016
Build a portable gas monitor to check for dangerous levels of hazardous gases.

Photon Remote Water Level Sensor

June 2, 2016
Learn how to build a remote water level sensor for a water storage tank and how to automate a pump based off the readings!

Si7021 Humidity and Temperature Sensor Hookup Guide

May 5, 2016
The Si7021 humidity and temperature sensor is an easy to use, digital, low-cost sensor to aid you in all your environment sensing needs.

Blynk Board Project Guide

March 25, 2016
A series of Blynk projects you can set up on the Blynk Board without ever re-programming it.

LED Cloud-Connected Cloud

February 22, 2016
Make an RGB colored cloud light! You can also control it from your phone, or hook up to the weather!

SparkFun BME280 Breakout Hookup Guide

October 22, 2015
A guide for connecting the BME280 sensor to a microcontroller, and for using the SparkFun Arduino library.

SparkFun Inventor's Kit for Photon Experiment Guide

September 3, 2015
Dive into the world of the Internet of Things with the SparkFun Inventor's Kit for Photon.

MS5803-14BA Pressure Sensor Hookup Guide

July 24, 2014
Breakout of MS5803-14BA Pressure Sensor to measure the absolute pressure of the fluid around them to determine altitude, water depth, or any other tasks that require an accurate pressure reading. This includes air, water, and anything else that acts like a viscous fluid.

ML8511 UV Sensor Hookup Guide

March 13, 2014
Get up and running quickly with this simple to use UV sensor.

T5403 Barometric Pressure Sensor Hookup Guide

March 6, 2014
T5403 Barometric Pressure Sensor Hookup Guide

MPL3115A2 Pressure Sensor Hookup Guide

December 5, 2013
Getting started with the MPL3115A2 Pressure Sensor.

Si4707 Hookup Guide

May 29, 2013
Instructions on hooking up to and communicating with the Si4707 Weather Band Radio Breakout using an Arduino.

Creating a Humidor Control Box

March 13, 2013
Because some of our boards need to be re-humidified after reflow, we decided to make our own humidor. This tutorial will focus on how to model a project in 3D and then fabricate it using a CNC routing machine.