Si7021 Humidity and Temperature Sensor Hookup Guide

≡ Pages
Contributors: Joel_E_B

Introduction

The Si7021 is a low-cost, easy to use, highly accurate, digital temperature and humidity sensor. All you need is two lines for I2C communication, and you’ll have relative humidity readings and accurate temperature readings as well! This sensor is ideal for environmental sensing and data logging, perfect for a weather station or humidor control system.

SparkFun Humidity and Temperature Sensor Breakout - Si7021

SEN-13763
Retired

The Si7021 also comes equipped with a hydrophobic PTFE filter covering the inlet on the sensor. This filter blocks contaminants but allows water vapor to pass through, keeping your sensor safe from water damage while still proving accurate sensor readings.

Required Materials

To follow along with this hookup guide, you will need the following:

Suggested Reading

Before embarking upon this tutorial, you may find the following links useful:

Pull-up Resistors

A quick introduction to pull-up resistors - whey they're important, and how/when to use them.

Installing an Arduino Library

How do I install a custom Arduino library? It's easy! This tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries not linked with the Arduino IDE, we will also go over manually installing an Arduino library.

Logic Levels

Learn the difference between 3.3V and 5V devices and logic levels.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

Board Overview

Let's go over the Si7021 Breakout in detail.

alt text

Si7021 Details:

  • Uses the I2C interface
  • Typical humidity accuracy of ±2%
  • Typical temperature accuracy of ±0.3C
  • Operates from 0 to 100% humidity but this sensor isn’t recommended for harsh environments where it could come in contact with water (such as rain)
  • 3.3V sensor - use inline logic level converters or 10kΩ resistors to limit 5V signals
  • Only one Si7021 sensor can reside on the I2C bus at a time

Pull-up Resistors

This breakout board has built-in 4.7KΩ pull up resistors for I2C communications. If you're hooking up multiple I2C devices on the same bus, you may want to disable/enable the pull-up resistors for one or more boards. On the Si7021, the pull-ups are enabled by default. To disable them, simply use some solder wick to remove the solder on the jumper labeled PU. This will disconnect the resistors from VCC and from the I2C bus.

PTFE Filter

The tiny white cover on the IC is known as a Polytetrafluorethylene (PTFE) Membrane Filter. It keeps moisture out but allows humidity in. This filter is very low-profile, hydrophobic and oleophobic, and excludes particulates down to 0.35 microns in size.

Heads up! Do not remove this white filter, mistaking it for some IC tape that was left on by mistake. Removing the filter may result in a shortened life span of the device or failure in highly humid areas.

From the Si7021 datasheet:

"Because the sensor operates on the principal of measuring a change in capacitance, any changes to the dielectric constant of the polymer film will be detected as a change in relative humidity. Therefore, it is important to minimize the probability of contaminants coming into contact with the sensor. Dust and other particles as well as liquids can affect the RH reading."

alt text

Image courtesy of Silicon Labs datasheet

Hooking It Up

Wiring up the Si7021 is very easy! We recommend soldering four male headers to the breakout board. You can also solder wires if your application needs.

Power

This board runs at 3.3V. Be sure to power the board from the 3.3V pin! Because I2C is an open drain signal, there's no need to worry about level shifting the signal; the 3.3V signal will be adequate to communicate with the Arduino and the signal will never reach a dangerous level for the pins on the Si7021.

Connections: Breakout to Arduino

Method 1

There are two ways to connect an Si7021 to an Arduino. The first is using pins A4 and A5 on classic Arduino boards. This breakout was designed using our standard I2C pinout, allowing the sensor to be connected directly to an Arduino without using a breadboard or wires.

  • GND → A2
  • VCC → A3
  • SDA → A4
  • SCL → A5

This would look like the following:

Fritzing

Heads up! This method will only work with Arduino boards that run at 3.3V such as the 3.3V Arduino Pro, the 3.3V Arduino Pro Mini, the SparkFun SAMD21 Mini Breakout and the SparkFun SAMD21 Dev Breakout.

Also, if using this wiring scheme, be sure to assign pins A2 and A3 as GND and VCC, respectively, in your code.

If you need to use this device with a 5V microcontoller, you will need to use a Logic Level Converter.

Method 2

This method is for those with newer model Arduino boards that have the SDA and SCL lines broken out. We'll be hooking up VCC and GND to the normal power pins and two data lines for I2C communication. Connect the SDA and SCL lines directly to the SDA and SCL lines broken out on the Arduino headers.

  • VCC → 3.3V
  • GND → GND
  • SDA → SDA
  • SCL → SCL

This would look something like the following:

alt text

Si7021 Library and Example Code

To get started, use the example code and library files below.

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE.

If you have not previously installed an Arduino library, please check out our installation guide.

You can download the library from the link below. Check out our Installing an Arduino Library tutorial for more help.

Once the library is installed, open Arduino, and expand the examples menu. You should see the Si7021 example.

menu

The examples menu expanded to show Si7021 example

language:c
/******************************************************************************
  SparkFun Si7021 Breakout Example
  Joel Bartlett @ SparkFun Electronics
  Original Creation Date: May 18, 2015
  Updated May 4, 2016
  This sketch prints the temperature and humidity the Serial port.

  The library used in this example can be found here:
  https://github.com/sparkfun/Si7021_Breakout/tree/master/Libraries

  Hardware Connections:
      HTU21D ------------- Photon
      (-) ------------------- GND
      (+) ------------------- 3.3V (VCC)
       CL ------------------- D1/SCL
       DA ------------------- D0/SDA

  Development environment specifics:
    IDE: Particle Dev
    Hardware Platform: SparkFun RedBoard
                       Arduino IDE 1.6.5

  This code is beerware; if you see me (or any other SparkFun
  employee) at the local, and you've found our code helpful,
  please buy us a round!
  Distributed as-is; no warranty is given.
*******************************************************************************/
#include "SparkFun_Si7021_Breakout_Library.h"
#include <Wire.h>

float humidity = 0;
float tempf = 0;


int power = A3;
int GND = A2;

//Create Instance of HTU21D or SI7021 temp and humidity sensor and MPL3115A2 barrometric sensor
Weather sensor;

//---------------------------------------------------------------
void setup()
{
    Serial.begin(9600);   // open serial over USB at 9600 baud

    pinMode(power, OUTPUT);
    pinMode(GND, OUTPUT);

    digitalWrite(power, HIGH);
    digitalWrite(GND, LOW);

    //Initialize the I2C sensors and ping them
    sensor.begin();

}
//---------------------------------------------------------------
void loop()
{
    //Get readings from all sensors
    getWeather();
    printInfo();
    delay(1000);

}
//---------------------------------------------------------------
void getWeather()
{
  // Measure Relative Humidity from the HTU21D or Si7021
  humidity = sensor.getRH();

  // Measure Temperature from the HTU21D or Si7021
  tempf = sensor.getTempF();
  // Temperature is measured every time RH is requested.
  // It is faster, therefore, to read it from previous RH
  // measurement with getTemp() instead with readTemp()
}
//---------------------------------------------------------------
void printInfo()
{
//This function prints the weather data out to the default Serial Port

  Serial.print("Temp:");
  Serial.print(tempf);
  Serial.print("F, ");

  Serial.print("Humidity:");
  Serial.print(humidity);
  Serial.println("%");
}

Once you've uploaded the code, connect using this serial terminal to see the output.

Si7021 Functions:

Weather::getRH() - Returns current Relative Humidity measurement.

Weather::readTemp() - Returns temperature in Celsius from previous RH measurement.

Weather::getTemp() - Returns current temp in Celsius.

Weather::readTempF() - Returns temperature in Fahrenheit from previous RH measurement.

Weather::getTempF() - Returns current temp in Fahrenheit.

Weather::changeResolution() - Allows the user to change the humidity and temperature resolution. The vast majority of users do not need to change the resolution. By default the sensor will be in its highest resolution settings. This function is useful if you need to decrease the amount of time between readings or to save power. See the datasheet for more information. As an example, to change the resolution to 11 bit RH and 11 bit temperature, you would call myHumidity.SetResolution(0b10000001); to set bit 7 and bit 0.

alt text

Resolution table can be found on page 25 of the datasheet.

Resources and Going Further

With that, you should now have a functional humidity and temperature sensing system. Check the links below for more information.

Need some inspiration? Check out these other tutorials:

Hazardous Gas Monitor

Build a portable gas monitor to check for dangerous levels of hazardous gases.

SparkFun gator:environment Hookup Guide

The gator:environment combines two I2C sensors for temperature, humidity, pressure, eCO2, and eTVOC values. This tutorial will get you started using the gator:environment with the micro:bit platform.

Qwiic TMP117 High Precision Digital Temperature Sensor Hookup Guide

Add a high precision, digital temperature sensor to your projects using the TMP117 over the I2C!

SparkFun Thing Plus - NINA-B306 Hookup Guide

A quick guide to get started using the SparkFun Thing Plus - NINA-B306. This Thing Plus is loaded with the Arm Cortex-M4 processor in the NINA-B306 along with on-board motion and environmental sensors in the ISM330DHCX 6DoF and BME280 pressure and temperature sensor.

Or check out this blog post for ideas.