Hookup

This type of tutorial shows people how to get a specific product hooked up and working.

SparkFun Qwiic Shield for Teensy Hookup Guide

October 15, 2020
A short guide for assembling and using the SparkFun Qwiic Shield for Teensy and Qwiic Shield for Teensy Extended.

SparkFun Qwiic GPIO Hookup Guide

October 8, 2020
Add up to 8 extra I/O pins to your microcontroller with the SparkFun Qwiic GPIO. Get started with the Qwiic GPIO in this Hookup Guide.

SparkFun Qwiic Dual Solid State Relay Hookup Guide

September 24, 2020
A Hookup Guide to get you started with the SparkFun Qwiic Dual Solid State Relay.

Getting Started with the Artemis Development Kit

September 10, 2020
This guide covers the general design of the board, the installation of the recommended software used to program the Artemis DK, and some basic examples. For more advanced functionalities, we have separate software development guides for the AmbiqSDK, Arm® Mbed™ OS, and the Arduino IDE platforms that users can reference.

Installing Board Definitions in the Arduino IDE

September 9, 2020
How do I install a custom Arduino board/core? It's easy! This tutorial will go over how to install an Arduino board definition using the Arduino Board Manager. We will also go over manually installing third-party cores, such as the board definitions required for many of the SparkFun development boards.

SparkFun ProDriver and Mini Stepper Motor Driver Hookup Guide

September 3, 2020
The SparkFun ProDriver and Mini Stepper Motor Driver boards utilize Toshiba's TC78H670FTG stepper motor driver. The ProDriver features latch pin terminals, which are easier to connect than the "Easy" Drivers. Meanwhile, the Mini Stepper Motor Driver come in smaller PCB footprint, that is pin compatible with breadboards. To get started, follow this hookup guide and you will be spinning stepper motors, in no time.

OpenLog Artemis Hookup Guide

August 20, 2020
How to use and re-program the OpenLog Artemis, an open source datalogger. The OLA comes preprogrammed to automatically log data. The OLA can also record serial data, analog voltages, or readings from external Qwiic-enabled I2C devices. Some of these Qwiic-enabled devices include GPS/GNSS modules, pressure, altitude, humidity, temperature, air quality, environment, distance, and weight sensors.

Jetson Nano + Sphero RVR Mash-up (PART 2)

July 29, 2020
We took two of our biggest robotics partnerships from the previous year and shazamed them together into one robot to rule them all!

SparkFun Qwiic MicroPressure Hookup Guide

July 23, 2020
Get started using your Qwiic MicroPressure breakout board with this hookup guide.

SparkFun Qwiic Quad Solid State Relay Kit Hookup Guide

July 16, 2020
A Hookup Guide to get you started with the SparkFun Qwiic Quad Solid State Relay Kit (say that five times fast!).

SparkFun GPS-RTK Dead Reckoning ZED-F9R Hookup Guide

July 9, 2020
The u-blox ZED-F9R is a powerful GPS-RTK unit that uses a fusion of IMU, wheel ticks, a vehicle dynamics model, correction data, and GNSS measurements to provide highly accurate and continuous position for navigation in the difficult conditions. We will quickly get you set up using the Qwiic ecosystem through Arduino and Python so that you can start reading the output!

SparkFun Photodetector (MAX30101) Hookup Guide

June 25, 2020
The SparkFun Photodetector - MAX30101 (Qwiic) is the successor to the MAX30105 particle sensor, a highly sensitive optical sensor. This tutorial will get you started on retrieving the raw data from the MAX30101 sensor.

SparkFun Air Quality Sensor - SGP30 (Qwiic) Hookup Guide

June 5, 2020
A hookup guide to get started with the SparkFun Air Quality Sensor - SGP30 (Qwiic).

SparkFun Environmental Sensor Breakout - BME68x (Qwiic) Hookup Guide

May 14, 2020
A hookup guide to get started with the BME68x Environmental Sensor from Bosch. Monitor the air quality, temperature, humidity, and barometric pressure with this Qwiic sensor!

SparkFun Humidity Sensor Breakout - SHTC3 (Qwiic) Hookup Guide

May 7, 2020
A Hookup Guide to get started using the SHTC3 breakout.

Spectrum Shield Hookup Guide (v2)

May 4, 2020
Want your project to react to music? Then the SparkFun Spectrum Shield is the product for you! Get going in no time with this Hookup Guide.

SparkFun GPS Dead Reckoning NEO-M8U Hookup Guide

April 30, 2020
The u-blox NEO-M8U is a powerful GPS units that takes advantage of untethered dead reckoning (UDR) technology for navigation. The module provides continuous positioning for vehicles in urban environments and during complete signal loss (e.g. short tunnels and parking garages). We will quickly get you set up using the Qwiic ecosystem and Arduino so that you can start reading the output!

Jetson Nano + Sphero RVR Mash-up (PART 1)

April 23, 2020
We took two of our biggest robotics partnerships from the previous year and shazamed them together into one robot to rule them all!

Working with Qwiic on a Jetson Nano through Jupyter Notebooks

April 23, 2020
We created a few Jupyter Notebooks to make using our Qwiic boards with your Jetson Nano even easier!

Real Time Clock Module - RV-8803 (Qwiic) Hookup Guide

April 2, 2020
A Hookup Guide for the SparkFun Real Time Clock Module - RV-8803 (Qwiic). Learn how to integrate the RV-8803 into your next time-keeping project.

Assembly Guide for SparkFun JetBot AI Kit V2.0

March 27, 2020
Assembly Guide for the SparkFun JetBot AI Kit v2.0. This tutorial includes photos & comments to assemble the two-layer chassis & additional components unique to the JetBot kit.

SparkFun Qwiic Digital Temperature Sensor - TMP102 Hookup Guide

March 26, 2020
Get started using your SparkFun Digital Temperature Sensor - TMP102 (Qwiic) with this Hookup Guide!

Raspberry Pi 4 Kit Hookup Guide

March 14, 2020
Guide for hooking up your Raspberry Pi 4 Model B basic, desktop, or hardware starter kit together.

SparkFun Qwiic Thermocouple Hookup Guide

March 12, 2020
Learn how to hook up your Qwiic Thermocouple Amplifier.
Viewing 572 Hookup Tutorials. View All Tutorials.