Hookup
This type of tutorial shows people how to get a specific product hooked up and working.
LED Light Bar Hookup
A quick overview of SparkFun's LED light bars, and some examples to show how to hook them up.
Using the BlueSMiRF
How to get started using the BlueSMiRF and Bluetooth Mate Silvers.
TXB0104 Level Shifter Hookup Guide
How to use the TXB0104 chip.
Using the Arduino Pro Mini 3.3V
This tutorial is your guide to all things Arduino Pro Mini. It explains what it is, what it's not, and how to get started using it.
ProtoSnap LilyPad Development Simple Hookup Guide
Interested in getting into LilyPad? Or maybe it's Arduino that tickles your fancy? Just want to add a little white-blinky-LED zest to your vest? All of the above? The ProtoSnap LilyPad Simple is a great tool to explore any of these subjects.
RN-52 Bluetooth Hookup Guide
A hookup guide to get you started with the RN-52 Audio Bluetooth Module Breakout Board.
Using the Serial 7-Segment Display
How to quickly and easily set up the Serial 7-Segment Display and the Serial 7-Segment Display Shield.
MetaWatch Teardown and Arduino Hookup
Tearing down the nifty Bluetooth-enabled MetaWatch. Then building an Arduino sketch to control it.
WS2812 Breakout Hookup Guide
How to create a pixel string with the WS2812 and WS2812B addressable LEDs!
LDK Experiment 4: Make Your Own Button
How to create your own e-textiles buttons.
Si4707 Hookup Guide
Instructions on hooking up to and communicating with the Si4707 Weather Band Radio Breakout using an Arduino.
Firefly Jar Assembly Guide
Make a soft circuit firefly jar with conductive thread, LEDs, and the LilyTwinkle!
Getting Started with the LilyPad MP3 Player
The LilyPad MP3 Player is an amazing little board that contains almost everything you need to play audio files. You can use it to create all kinds of noisy projects, from MP3 hoodies to talking teddy bears. Your imagination is the only limit! This tutorial will help you get started.
Connecting Arduino to Processing
Send serial data from Arduino to Processing and back - even at the same time!
Using OpenSegment
How to hook up and use the OpenSegment display shield. The OpenSegment is the big brother to the Serial 7-Segment Display. They run on the same firmware, however the OpenSegment is about twice as big.
IR Communication
This tutorial explains how common infrared (IR) communication works, as well as shows you how to set up a simple IR transmitter and receiver with an Arduino.
LDK Experiment 1: Lighting Up a Basic Circuit
The first experiment in the LilyPad Design Kit series. In this exercise, you will learn how a basic e-textiles circuit works, and light up a sewable LED using a coin cell battery holder and conductive thread.
LilyPad Development Board Hookup Guide
The LilyPad Development Board is a sewable electronics prototyping board that you can use to learn circuits and programming with Arduino, then break apart to make an interactive fabric or wearable project.
Simon Says Assembly Guide
No matter what flavor of the Simon Says Through-hole Soldering Kit you've purchased, this tutorial is here to guide you through the entire build process.
Simon Says Experiments
So you've built up a Simon Says kit? What next? This tutorial will get you up and running with Arduino software, guide you through a few example sketches, and send you on your way to create your own. Careful, this stuff is highly addictive. :)