Arduino
This popular development board is great for beginners and advanced users alike. It comes in a variety of flavors and is extensible with "shields" for adding special functionality. Find tutorials here to learn how to do cool stuff using the Arduino platform.
Sort by:
Recently Added
Viewing 409 Arduino Tutorials.
View All Tutorials.
Electret Mic Breakout Board Hookup Guide
An introduction to working with the Electret Mic Breakout Board.
Battery Babysitter Hookup Guide
An introduction and getting started guide for the Battery Babysitter - a flexible LiPo battery charger and monitor.
Beefcake Relay Control Hookup Guide
This is a guide for assembling and basic use of the Beefcake Relay Control board
GPS Differential Vector Pointer
Use GPS to have two objects, a base and a target, point towards one another. This can be used to aim a directional antenna (or in the case of this project, a laser) from one object to the other object at a distance that is only limited by your ability to provide the base station with the target's GPS location.
How to Build a Remote Kill Switch
Learn how to build a wireless controller to kill power when things go... sentient.
Interactive LED Music Visualizer
Use an Arduino and the SparkFun Sound Detector to create visualizations on Addressable RGB LED strips.
Hobby Servo Tutorial
Servos are motors that allow you to accurately control the rotation of the output shaft, opening up all kinds of possibilities for robotics and other projects.
Getting Started with the SparkFun Inventor's Kit for Google's Science Journal App
This is a quick guide to using the Google Science Journal app with the Arduino 101 that's included and pre-programmed in the SIK for Google's Science Journal App.
Measuring Internal Resistance of Batteries
Classroom STEM activity that has students build a battery from a lemon, measure the open and closed circuit voltages, and determine the battery's internal resistance.
SoftPot Hookup Guide
Equip your Arduino project with a sliding soft potentiometer to monitor position or adding linear control to your project.
Sensor Kit Resource Hub
An overview of each component in the SparkFun Sensor Kit, plus links to tutorials and other resources you'll need to hook them up.
Force Sensitive Resistor Hookup Guide
How to hook a force-sensitive resistor up to an Arduino to measure pressure variances.
RFM69HCW Hookup Guide
The RFM69HCW is an inexpensive transceiver that you can use to create all kinds of wireless projects. This tutorial will help you get started.
SIK Experiment Guide for the Arduino 101/Genuino 101 Board
This guide contains all the information you will need to explore the 21 circuits of the SparkFun Inventor's Kit for the Arduino 101/Genuino 101 Board.
SIK Keyboard Instrument
We can use the parts and concepts in the SparkFun Invetor's Kit to make a primitive keyboard instrument.
OpenLog Hookup Guide
An introduction to working with the OpenLog data logger.
Blynk Board Arduino Development Guide
How to get your computer set up with Arduino and the Blynk Board hardware definitions -- so you can start creating Blynk projects of your own!
Blynk Board Bridge Widget Demo
A Blynk project that demonstrates how to use the Bridge widget to get two (or more) Blynk Boards to communicate.
SparkFun LED Array (8x7) Hookup Guide
Getting started with the Charlieplexed 8x7 LED array.
MicroSD Breakout With Level Shifter Hookup Guide
How to use the level translating µSD device.
LED Cloud-Connected Cloud
Make an RGB colored cloud light! You can also control it from your phone, or hook up to the weather!
PicoBuck Hookup Guide v12
The PicoBuck board is a high-efficiency three-channel constant-current LED driver.
SparkFun USB to Serial UART Boards Hookup Guide
How to use the SparkFun FTDI based boards to program an Arduino and access another serial device over the hardware serial port, without unplugging anything!
BadgerHack: Synth Add-On Kit
Make a tiny synth with BadgerStick.
Sort by:
Recently Added
Viewing 409 Arduino Tutorials.
View All Tutorials.