Light

Experiment Guide for the Johnny-Five Inventor's Kit

June 28, 2016
Use the Tessel 2 and the Johnny Five Inventors kit to explore the world of JavaScript enabled hardware through 14 awesome experiments!

GPS Differential Vector Pointer

May 31, 2016
Use GPS to have two objects, a base and a target, point towards one another. This can be used to aim a directional antenna (or in the case of this project, a laser) from one object to the other object at a distance that is only limited by your ability to provide the base station with the target's GPS location.

PIR Motion Sensor Hookup Guide

May 5, 2016
An overview of passive infrared (PIR) motion detecting sensors, and how to hook them up to an Arduino.

Photocell Hookup Guide

May 5, 2016
Hook a light-sensing photocell up to an Arduino to create an ambient light monitor.

QRD1114 Optical Detector Hookup Guide

May 5, 2016
Use this IR LED/phototransistor fusion to sense objects in close proximity or even the color of a surface!

Sensor Kit Resource Hub

May 5, 2016
An overview of each component in the SparkFun Sensor Kit, plus links to tutorials and other resources you'll need to hook them up.

Boss Alarm

March 30, 2016
Build a Boss Alarm that alerts you of anyone walking into your office and automatically changes your computer screen.

Blynk Board Project Guide

March 25, 2016
A series of Blynk projects you can set up on the Blynk Board without ever re-programming it.

LED Cloud-Connected Cloud

February 22, 2016
Make an RGB colored cloud light! You can also control it from your phone, or hook up to the weather!

BadgerHack: Gaming Add-On Kit

February 16, 2016
Make a Breakout clone with the BadgerHack Gaming Add-On Kit.

LilyPad Light Sensor Hookup Guide

November 19, 2015
How to hook up the LilyPad Light Sensor as well as some project ideas and example code.

Touch Potentiometer Hookup Guide

October 22, 2015
Learn how to use the SparkFun Touch Potentiometer to control lighting, volume or other inputs in your daily life.

SX1509 I/O Expander Breakout Hookup Guide

September 24, 2015
Learn how you can use the SX1509 to control 16 LEDs or up to 64 buttons with just two pins.

LilyPad Pixel Board Hookup Guide

September 16, 2015
Add changing colors to your wearable projects using LilyPad Pixel Boards.

LED Robot Pop Up Card

August 19, 2015
Craft a paper circuit pop up card with a cycling RGB LED, battery, and copper tape.

LED Butterfly Pop Up Card

August 19, 2015
Craft an illuminated butterfly pop up card with copper tape, two LEDs, and a battery.

Large Digit Driver Hookup Guide

June 25, 2015
Getting started guide for the Large Digit display driver board. This tutorial explains how to solder the module (backpack) onto the back of the large 7-segment LED display and run example code from an Arduino.

Origami Paper Circuits

May 26, 2015
A quick tutorial to get you started in the world of light up origami flowers.

The Great Big Guide to Paper Circuits

May 22, 2015
Let's take a look at different materials we can use to combine paper crafting and electronics.

Hackers in Residence: The Sound Visualizer Pt. 2

May 7, 2015
An addition to a previous project, this time using a PC and a custom Java app to create your own music visualizer using a RGB LED matrix.

Light Up Silk Flower Corsage

April 20, 2015
Combine a silk flower with a built-in RGB LED and some LilyPad Switches to create a customizable accessory.

FLIR Lepton Hookup Guide

March 26, 2015
See the invisible world of infrared radiation using the FLIR Dev Kit and Raspberry Pi.

Hackers in Residence: The Sound Visualizer

March 23, 2015
A fun project that uses a Raspberry Pi and a custom Java app to create your own sound visualizer using a RGB LED matrix.

VL6180 Hookup Guide

February 12, 2015
Get started with your VL6180 based sensor or the VL6180 breakout board.