Tutorials

Electret Mic Breakout Board Hookup Guide

June 23, 2016
An introduction to working with the Electret Mic Breakout Board.

Battery Babysitter Hookup Guide

June 23, 2016
An introduction and getting started guide for the Battery Babysitter - a flexible LiPo battery charger and monitor.

Hazardous Gas Monitor

June 17, 2016
Build a portable gas monitor to check for dangerous levels of hazardous gases.

ASCII

June 13, 2016
A brief history of how ASCII came to be, how it's useful to computers, and some helpful tables to convert numbers to characters.

Beefcake Relay Control Hookup Guide

June 2, 2016
This is a guide for assembling and basic use of the Beefcake Relay Control board

Photon Remote Water Level Sensor

June 2, 2016
Learn how to build a remote water level sensor for a water storage tank and how to automate a pump based off the readings!

Interactive LED Music Visualizer

May 31, 2016
Use an Arduino and the SparkFun Sound Detector to create visualizations on Addressable RGB LED strips.

GPS Differential Vector Pointer

May 31, 2016
Use GPS to have two objects, a base and a target, point towards one another. This can be used to aim a directional antenna (or in the case of this project, a laser) from one object to the other object at a distance that is only limited by your ability to provide the base station with the target's GPS location.

How to Build a Remote Kill Switch

May 31, 2016
Learn how to build a wireless controller to kill power when things go... sentient.

Continuous Rotation Servo Trigger Hookup Guide

May 26, 2016
How to use the SparkFun Continuous Rotation Servo Trigger with continuous rotation servos, without any programming!

Servo Trigger Programming Guide

May 26, 2016
Looking under the hood of the Servo Trigger -- using the development environment and some finer details of the firmware.

Hobby Servo Tutorial

May 26, 2016
Servos are motors that allow you to accurately control the rotation of the output shaft, opening up all kinds of possibilities for robotics and other projects.

Getting Started with the SparkFun Inventor's Kit for Google's Science Journal App

May 24, 2016
This is a quick guide to using the Google Science Journal app with the Arduino 101 that's included and pre-programmed in the SIK for Google's Science Journal App.

Sparcade: Edison as a Web Server for Browser Games

May 19, 2016
Turn the Intel® Edison into an access point that serves a simple browser-based game. High scores from the game are displayed on a character LCD.

IOIO-OTG Hookup Guide

May 18, 2016
Get started using the IOIO-OTG with your Android device or PC.

Sensor Kit Resource Hub

May 5, 2016
An overview of each component in the SparkFun Sensor Kit, plus links to tutorials and other resources you'll need to hook them up.

SoftPot Hookup Guide

May 5, 2016
Equip your Arduino project with a sliding soft potentiometer to monitor position or adding linear control to your project.

Si7021 Humidity and Temperature Sensor Hookup Guide

May 5, 2016
The Si7021 humidity and temperature sensor is an easy to use, digital, low-cost sensor to aid you in all your environment sensing needs.

Flex Sensor Hookup Guide

May 5, 2016
An overview of the flex sensor - a bendable variable resistor. Plus, example circuits and Arduino code to get you started!

QRD1114 Optical Detector Hookup Guide

May 5, 2016
Use this IR LED/phototransistor fusion to sense objects in close proximity or even the color of a surface!

Force Sensitive Resistor Hookup Guide

May 5, 2016
How to hook a force-sensitive resistor up to an Arduino to measure pressure variances.

Photocell Hookup Guide

May 5, 2016
Hook a light-sensing photocell up to an Arduino to create an ambient light monitor.

Piezo Vibration Sensor Hookup Guide

May 5, 2016
How to combine a piezo sensor, high-value resistor, and an Arduino to create a vibration sensor.

Reed Switch Hookup Guide

May 5, 2016
Magnetically-actuated reed switches are the perfect component for non-contact proximity sensors. This tutorial provides a quick overview and example hook up.