Arduino

This popular development board is great for beginners and advanced users alike. It comes in a variety of flavors and is extensible with "shields" for adding special functionality. Find tutorials here to learn how to do cool stuff using the Arduino platform.

SparkFun Qwiic GPIO Hookup Guide

October 8, 2020
Add up to 8 extra I/O pins to your microcontroller with the SparkFun Qwiic GPIO. Get started with the Qwiic GPIO in this Hookup Guide.

SparkFun Qwiic Dual Solid State Relay Hookup Guide

September 24, 2020
A Hookup Guide to get you started with the SparkFun Qwiic Dual Solid State Relay.

Qwiic GPS Clock

September 14, 2020
What time is it? Time for you to... Qwiic-ly build a GPS clock and output it to a display! This project provides you with the current date and time using GPS satellites. Read the date and time as a digital or analog clock. Or even configure the clock for military, your time zone, or automatically adjust the time for daylight savings time!

Getting Started with the Artemis Development Kit

September 10, 2020
This guide covers the general design of the board, the installation of the recommended software used to program the Artemis DK, and some basic examples. For more advanced functionalities, we have separate software development guides for the AmbiqSDK, Arm® Mbed™ OS, and the Arduino IDE platforms that users can reference.

Artemis Development with the Arduino IDE

September 10, 2020
This is an in-depth guide on developing in the Arduino IDE for the Artemis module and any Artemis microcontroller development board. Inside, users will find setup instructions and simple examples from blinking an LED and taking ADC measurements; to more complex features like BLE and I2C.

Installing Board Definitions in the Arduino IDE

September 9, 2020
How do I install a custom Arduino board/core? It's easy! This tutorial will go over how to install an Arduino board definition using the Arduino Board Manager. We will also go over manually installing third-party cores, such as the board definitions required for many of the SparkFun development boards.

SparkFun ProDriver and Mini Stepper Motor Driver Hookup Guide

September 3, 2020
The SparkFun ProDriver and Mini Stepper Motor Driver boards utilize Toshiba's TC78H670FTG stepper motor driver. The ProDriver features latch pin terminals, which are easier to connect than the "Easy" Drivers. Meanwhile, the Mini Stepper Motor Driver come in smaller PCB footprint, that is pin compatible with breadboards. To get started, follow this hookup guide and you will be spinning stepper motors, in no time.

SparkFun Qwiic Quad Solid State Relay Kit Hookup Guide

July 16, 2020
A Hookup Guide to get you started with the SparkFun Qwiic Quad Solid State Relay Kit (say that five times fast!).

Qwiic Digital Indoor Thermometer

July 15, 2020
Qwiic-ly build a digital indoor thermometer to measure the ambient temperature of the room and display it using an OLED on an I2C bus!

SparkFun GPS-RTK Dead Reckoning ZED-F9R Hookup Guide

July 9, 2020
The u-blox ZED-F9R is a powerful GPS-RTK unit that uses a fusion of IMU, wheel ticks, a vehicle dynamics model, correction data, and GNSS measurements to provide highly accurate and continuous position for navigation in the difficult conditions. We will quickly get you set up using the Qwiic ecosystem through Arduino and Python so that you can start reading the output!

ESP32 OTA Updates over BLE from a React Web Application

July 2, 2020
Learn how to flash firmware Over-the-Air using a BLE React WebApp and ESP32

SparkFun Photodetector (MAX30101) Hookup Guide

June 25, 2020
The SparkFun Photodetector - MAX30101 (Qwiic) is the successor to the MAX30105 particle sensor, a highly sensitive optical sensor. This tutorial will get you started on retrieving the raw data from the MAX30101 sensor.

RFID Beginners Tutorial

June 15, 2020
Make a remote work logger using an RFID reader and a GPS module. Scan a card and get ID, location, and time. All the perfect data to punch in and punch out from the middle of Nowhere!

SparkFun Air Quality Sensor - SGP30 (Qwiic) Hookup Guide

June 5, 2020
A hookup guide to get started with the SparkFun Air Quality Sensor - SGP30 (Qwiic).

SparkFun Environmental Sensor Breakout - BME68x (Qwiic) Hookup Guide

May 14, 2020
A hookup guide to get started with the BME68x Environmental Sensor from Bosch. Monitor the air quality, temperature, humidity, and barometric pressure with this Qwiic sensor!

SparkFun Humidity Sensor Breakout - SHTC3 (Qwiic) Hookup Guide

May 7, 2020
A Hookup Guide to get started using the SHTC3 breakout.

Spectrum Shield Hookup Guide (v2)

May 4, 2020
Want your project to react to music? Then the SparkFun Spectrum Shield is the product for you! Get going in no time with this Hookup Guide.

SparkFun GPS Dead Reckoning NEO-M8U Hookup Guide

April 30, 2020
The u-blox NEO-M8U is a powerful GPS units that takes advantage of untethered dead reckoning (UDR) technology for navigation. The module provides continuous positioning for vehicles in urban environments and during complete signal loss (e.g. short tunnels and parking garages). We will quickly get you set up using the Qwiic ecosystem and Arduino so that you can start reading the output!

Arduino Shields v2

April 20, 2020
An update to our classic Arduino Shields Tutorial! All things Arduino shields. What they are and how to assemble them.

Real Time Clock Module - RV-8803 (Qwiic) Hookup Guide

April 2, 2020
A Hookup Guide for the SparkFun Real Time Clock Module - RV-8803 (Qwiic). Learn how to integrate the RV-8803 into your next time-keeping project.

Temperature Sensor Comparison

March 18, 2020
A comparison of analog and digital temperature sensors. Which is better?

SparkFun Qwiic Thermocouple Hookup Guide

March 12, 2020
Learn how to hook up your Qwiic Thermocouple Amplifier.

SparkFun Clock Generator 5P49V60 (Qwiic) Hookup Guide

February 28, 2020
The SparkFun Clock Generator 5P49V60 (Qwiic) breakout board offers a wide range of customizable frequencies in a wide range of different signal types using a single reference clock. This hookup guide will go over all of the many available functions and gives the hardware rundown on what exactly is on this board.

Basic Servo Control for Beginners

February 25, 2020
An introductory tutorial demonstrating several ways to use and interact with servo motors!
Viewing 408 Arduino Tutorials. View All Tutorials.