Arduino
This popular development board is great for beginners and advanced users alike. It comes in a variety of flavors and is extensible with "shields" for adding special functionality. Find tutorials here to learn how to do cool stuff using the Arduino platform.
Qwiic Ambient Light Sensor (VEML6030) Hookup Guide
The VEML6030 is a high accuracy ambient light sensor with 16-bit resolution. This I2C sensor can detect light similar to the human eye response. Start detecting light levels in your environment!
SparkFun 9DoF IMU (ICM-20948) Breakout Hookup Guide
How to use the SparkFun 9DoF ICM-20948 breakout board for your motion sensing projects. This breakout is ideal for wearable sensors and IoT applications.
Artemis Development with Arduino
Get our powerful Artemis based boards (Artemis Nano, BlackBoard Artemis, and BlackBoard Artemis ATP) blinking in less than 5 minutes using the SparkFun Artemis Arduino Core!
Designing with the SparkFun Artemis
Let's chat about layout and design considerations when using the Artemis module.
TPL5110 Nano Power Timer Hookup Guide
The TPL5110 Nano Power Timer is ideal for applications that require low power, and especially those projects that are running off of a LiPo battery. The Nano Power Timer will turn on your project after the set amount of time, continuously.
Capacitive Touch Slider (CAP1203) Hookup Guide
An easy and Qwiic way to add capacitive touch to any of your projects using the CAP1203! In this guide, we go over how to connect and set up your Capacitive Touch Slider so you can start playing with it right away.
Basic Character LCD Hookup Guide
Liquid crystal displays (LCDs) are a great way to output a string of words or sensor data to a display for visual feedback. In this tutorial, we'll learn about LCDs, how to print a string of words to a 16x2 basic character LCD and create custom characters.
SAMD51 Thing Plus Hookup Guide
This tutorial covers the basic functionality of the SAMD51 Thing Plus and highlights the features of the new ARM Cortex-M4F development board.
ARM Programming
How to program SAMD21 or SAMD51 boards (or other ARM processors).
Qwiic 12-Bit ADC Hookup Guide
Need to add more analog inputs for your project? Check out the Qwiic 12-bit ADC.
Using Home Assistant to Expand Your Home Automations
An introduction to Home Assistant, an open source home automation hub.
Displaying Your Coordinates with a GPS Module
This Arduino tutorial will teach you how to pinpoint and display your GPS coordinates with a press of a button using hardware from our Qwiic Connect System (I2C).
Wireless Gesture Controlled Robot
Control the RedBot wirelessly based on the movement of your hand using an accelerometer, Arduino, and XBees!
Keyboard Shortcut, Qwiic Keypad
A simple project using the Qwiic Keypad and the RedBoard Turbo to create your own custom hotkey-pad.
Qwiic Keypad Hookup Guide
If you are tired of taking up GPIO pins, wiring a bunch of pull up resistors, and using firmware that scans the keys taking up valuable processing time... check out the new Qwiic Keypad.
LED Gumball Machine
Hacking gumball machines to make the world a happier, blinkier place.
Wireless Glove Controller
Build a wireless glove controller with Arduinos to trigger an LED using XBees!
TFT LCD Breakout 1.8in 128x160 Hookup Guide
This TFT LCD Breakout is a versatile, colorful, and easy way to experiment with graphics or create a user interface for your project.
Qwiic Scale Hookup Guide
Create your own digital scale quickly and easily using the Qwiic Scale!
SparkFun GPS Breakout (ZOE-M8Q and SAM-M8Q) Hookup Guide
The SparkFun ZOE-M8Q and SAM-M8Q are three similarly powerful GNSS boards, but with different project applications. We'll compare both GNSS receivers before getting each up and running.
Build a Qwiic Jukebox that is Toddler Approved!
Follow this tutorial to build your own custom jukebox. Note, this is designed simple and tough for use primarily with toddlers. It's also a great introduction to SparkFun's Qwiic products!
SparkFun ESP32 DMX to LED Shield
Learn how to utilize your DMX to LED Shield in a variety of different ways.
SparkFun Qwiic RFID-IDXXLA Hookup Guide
The Qwiic RFID ID-XXLA is an I2C solution that pairs with the ID-LA modules: ID-3LA, the ID-12LA, or the ID-20LA, and utilizes 125kHz RFID chips. Let's take a look at the hardware used for this tutorial.
RHT03 (DHT22) Humidity and Temperature Sensor Hookup Guide
Measure relative humidity and temperature or your environment with the RHT03 (a.k.a DHT22) low cost sensor on a single wire digital interface connected to an Arduino!