Tutorials
Rotary Dial Kit Assembly Guide
Put together your Rotary Dial Kit and light it up with our Arduino example code!
Current Sensor Breakout (ACS723) Hookup Guide
Learn how to measure the current consumption of your project using the ACS723 Current Sensor.
Nuclear Battery Assembly Guide
How to put together your BYOT (Bring Your Own Tritium) Nuclear Battery Kit!
LilyPad Light Sensor V2 Hookup Guide
How to hook up the LilyPad Light Sensor as well as some project ideas and example code.
LilyPad USB Plus Hookup Guide
The LilyPad USB Plus is a sewable microcontroller that you can use with Arduino.
HX1 APRS Transmitter Hookup Guide
The HX1 is a low-power amateur radio transmitter that can be used to send data to the Automatic Packet Reporting System (APRS) network.
RedBoard Edge Hookup Guide
The RedBoard Edge is a RedBoard that's been rebuilt around the idea that projects are eventually put into an enclosure to help clean up their look.
Flexible Grayscale OLED Hookup Guide
Figure out how to get images displaying on your new flexible OLED screen.
Qwiic Differential I2C Bus Extender (PCA9615) Hookup Guide
Learn how to extend the range of your I2C communication bus with the Qwiic differential I2C bus extender (PCA9615 ) breakout board.
Qwiic Real Time Clock Module (RV-1805) Hookup Guide
Find out what time it is, even after the power's been out on your project for a while with the Qwiic Real Time Clock (RTC) module.
PIC-Based Serial Enabled Character LCD Hookup Guide
The PIC-based serial enabled character LCD backpack is a simple and cost effective solution for interfacing to character Liquid Crystal Displays (LCDs) based on the HD44780 controller. The backpack simplifies the number of wires needed and allows your project to display all kinds of text and numbers.
Variable Load Hookup Guide - Revised
This tutorial will show you how to assemble and use SparkFun's Variable Load board. It can be used to test stability of the power supply under various loads, battery lifetime, safety cutoffs, and other design elements of power supplies under test.
Adapting LilyPad Development Board Projects to the LilyPad ProtoSnap Plus
An overview of the updates made in the redesign of the LilyPad Development Board to the LilyPad ProtoSnap Plus and how to adapt code written for the old board to the new one.
IoT Power Relay
Using the ESP32 to make a web-configured timed relay.
SparkFun Arduino ProtoShield Hookup Guide
The SparkFun Arduino ProtoShield PCB and ProtoShield kit lets you customize your own Arduino shield using whatever custom circuit you can come up with! This tutorial will go over its features, hardware assembly, and how to use the shield with an Arduino R3 footprint.
LIDAR-Lite v3 Hookup Guide
A tutorial for connecting the Garmin LIDAR-Lite v3 or the LIDAR-Lite v3HP to an Arduino to measure distance.
12V/5V Power Supply Hookup Guide
In this tutorial, we will replace the 12V/5V (2A) power supply's molex connector with two male barrel jacks adapters.
IoT Weight Logging Scale
This tutorial will show you how to make a scale that logs your weight to a custom website on the Internet. The principles can be extrapolated to any type of data.
micro:bit Educator Lab Pack Experiment Guide
A quickstart guide for the micro:bit educator lab pack.
Qwiic GRID-Eye Infrared Array (AMG88xx) Hookup Guide
The Panasonic GRID-Eye (AMG88xx) 8x8 thermopile array serves as a functional low-resolution infrared camera. This means you have a square array of 64 pixels each capable of independent temperature detection. It’s like having thermal camera (or Predator’s vision), just in really low resolution.
Qwiic Magnetometer (MLX90393) Hookup Guide
Figure out how magnetic fields are oriented, all without having to solder a thing.
WiFi Controlled Robot
This tutorial will show you how to make a robot that streams a webcam to a custom website that can be remotely controlled.
Qwiic VR IMU (BNO080) Hookup Guide
Figure out how things are oriented with the robust 9 degrees of freedom (DOF) BNO080 IMU. Maybe even make your own virtual reality (VR) applications if you're feeling savvy.
Getting Started with 3D Printing Using Tinkercad
Tinkercad is a great, easy-to-use online modeling software that can have you 3D printing quickly. This tutorial will walk you through designing a simple project enclosure.