Qwiic
The SparkFun Qwiic Connect System is an ecosystem of I2C sensors, actuators, shields, and cables that make prototyping faster and less prone to error. Get it? It's quick Qwiic! The following tutorials tagged takes advantage of the Qwiic system.
Power Delivery Board - USB-C (Qwiic) Hookup Guide
This guide will go over how to use the USB Type-C Power Delivery Board.
Qwiic Pro Micro USB-C (ATmega32U4) Hookup Guide
An overview of the ATmega32U4-based Qwiic Pro Micro USB-C, how to install it, and how to use it with Arduino.
SparkFun Qwiic Shield for Thing Plus Hookup Guide
A short guide for assembling and using the SparkFun Qwiic Shield for Thing Plus.
SparkFun Qwiic Shield for Arduino Nano Hookup Guide
Hookup Guide for the SparkFun Qwiic Shield for Arduino Nano.
SparkFun Qwiic Button Hookup Guide
A Hookup Guide for the SparkFun Qwiic Button (Red) and SparkFun Qwiic Button Breakout. Goes over connecting the Qwiic Button to an Arduino microcontroller and using it with the Qwiic Button Arduino library.
Secure DIY Garage Door Opener
Did you know that most garage doors are at risk of a roll jam attack? Here we make a DIY garage door remote-control system that is much more secure than most commercial-ready products using the latest in ECC cryptography.
SparkFun GPS NEO-M9N Hookup Guide
The u-blox NEO-M9N is a powerful GPS unit that comes with a chip antenna, SMA connector, and u.FL connector. We will quickly get you set up using the Qwiic ecosystem and Arduino so that you can start reading the output!
Getting Started with the Autonomous Kit for the Sphero RVR
Want to get started in robotics? Look no further than the SparkFun autonomous kit for the Sphero RVR! Whether you purchased the Basic or Advanced kit, this tutorial will get you rolling...
Basic Autonomous Kit for Sphero RVR Assembly Guide
Get your Basic Autonomous Kit for Sphero RVR all hooked up with this guide!
Advanced Autonomous Kit for Sphero RVR Assembly Guide
Get your Advanced Autonomous Kit for the Sphero RVR built up with this hookup guide!
Programming the SparkFun Edge with Arduino
Running low-power machine learning examples on the SparkFun Edge can now be done using the familiar Arduino IDE. In this follow-up to the initial Edge tutorial, we'll look at how to get three examples up and running without the need to learn an entirely new SDK.
Qwiic SHIM for Raspberry Pi Hookup Guide
Ever wanted to prototype I2C components on a Pi? Now you can!
Qwiic TMP117 High Precision Digital Temperature Sensor Hookup Guide
Add a high precision, digital temperature sensor to your projects using the TMP117 over the I2C!
Qwiic Pro Kit Project Guide
The Qwiic Pro Kit was designed to allow users to get started with Arduino without the need for soldering or a breadboard. We've included three inputs (a joystick, accelerometer, and proximity sensor) and one display that can be daisy chained to the RedBoard Turbo (SAMD21) Development Board.
SparkFun Qwiic Micro (SAMD21E) Hookup Guide
An introduction to the Qwiic Micro SAMD21E. Level up your Arduino-skills with the powerful SAMD21 ARM Cortex M0+ processor!
Cryptographic Co-Processor ATECC508A (Qwiic) Hookup Guide
Learn how to use some of the standard features of the SparkFun Cryptographic Co-processor.
GPS Geo-Mapping at the Push of a Button
Let's ramp up our GPS tracking skills with KML files and Google Earth. We'll make a tracker that logs location and allows us to visualize our steps with Google Earth.
SparkFun Edge Hookup Guide
Get to know your Edge board, including both the hardware features for you to utilize as well as how to get talking to it.
Hookup Guide for the Qwiic Motor Driver
Drive things "qwiic"-ly with the SparkFun Qwiic Motor Driver!
SparkFun Pulse Oximeter and Heart Rate Monitor Hookup Guide
Find out your oxygen saturation level or check out your heart rate using the MAX30101 biometric sensor and MAX32664 Biometric Hub via I2C!
Hookup Guide for the SparkFun RedBoard Artemis ATP
Get started with the RedBoard Artemis ATP - all the functionality of the SparkFun Artemis module wrapped in the Mega Arduino Footprint
Hookup Guide for the SparkFun RedBoard Artemis
Get started with the RedBoard Artemis - all the functionality of the SparkFun Artemis module wrapped in the familiar Uno R3 footprint
Hookup Guide for the SparkFun RedBoard Artemis Nano
Get started with the powerful RedBoard Artemis Nano
XBee3 Thing Plus Hookup Guide
Get started with SparkFun's XBee3 Thing Plus - both the u.FL as well as the PCB antenna versions.