Logging

MicroMod Main Board Hookup Guide V2

January 5, 2023
The MicroMod Main Board - Single and Double are specialized carrier boards that allow you to interface a Processor Board with a Function Board(s). The modular system allows you to add an additional feature(s) to a Processor Board with the help of a Function Board(s). In this tutorial, we will focus on the basic functionality of the Main Board - Single V2.1 and Main Board - Double and V2.2.

Qwiic Kit for Raspberry Pi V2 Hookup Guide

December 29, 2022
Get started with the SGP40, BME280, VCNL4040, and microOLED via I2C using the Qwiic system and Python on a Raspberry Pi! Measure VOC Index, light, temperature, humidity, and pressure from the environment. Then display them on the microOLED, serial terminal, or the cloud with Cayenne!

Getting Started with Machinechat

October 7, 2022
Organize and display your data with SparkFun's Artemis OpenLog and MachineChat's JEDIOne!

Monitor Sensor Data from Anywhere

August 10, 2022
Using WiFi to send sensor data from an ESP32 to a WiFi network and be able to read it from an IoT Dashboard from anywhere in the world.

Thing Plus Dual-Port Logging Shield Hookup Guide

June 16, 2022
This tutorial shows you how to hook up and use the SparkFun Thing Plus Dual-Port Logging Shield.

MicroMod Main Board Hookup Guide

November 11, 2021
The MicroMod Main Board - Single and Double are specialized carrier boards that allow you to interface a Processor Board with a Function Board(s). The modular system allows you to add an additional feature(s) to a Processor Board with the help of a Function Board(s). In this tutorial, we will focus on the basic functionality of the Main Board - Single and Main Board - Double.

MicroMod Environmental Function Board Hookup Guide

November 11, 2021
The SparkFun MicroMod Environmental Function Board adds additional sensing options to the MicroMod Processor Boards. This function board includes three sensors to monitor air quality (SGP40), humidity & temperature (SHTC3), and CO2 concentrations (STC31) in your indoor environment. To make it even easier to use, all communication is over the MicroMod's I2C bus! In this tutorial, we will go over how to connect the board and read the sensors.

SparkFun RTK Express Hookup Guide

June 21, 2021
Learn how to use the enclosed RTK Express product to achieve millimeter level geospatial coordinates.

MicroMod Asset Tracker Carrier Board Hookup Guide

February 25, 2021
Get started with the SparkFun MicroMod Asset Tracker Carrier Board following this Hookup Guide. The Asset Tracker uses the u-blox SARA-R510M8S LTE-M / NB-IoT module to provide a host of data communication options.

MicroMod Weather Carrier Board Hookup Guide

January 14, 2021
A quick guide to help to create your own MicroMod weather station using the MicroMod Weather Carrier Board and Processor of your choice.

SparkFun RTK Surveyor Hookup Guide

December 3, 2020
Learn how to use the enclosed RTK Surveyor product to achieve millimeter level geospatial coordinates.

MicroMod Data Logging Carrier Board Hookup Guide

October 21, 2020
Get started with some customizable MicroMod data logging with the Data Logging Carrier Board.

OpenLog Artemis Hookup Guide

August 20, 2020
How to use and re-program the OpenLog Artemis, an open source datalogger. The OLA comes preprogrammed to automatically log data. The OLA can also record serial data, analog voltages, or readings from external Qwiic-enabled I2C devices. Some of these Qwiic-enabled devices include GPS/GNSS modules, pressure, altitude, humidity, temperature, air quality, environment, distance, and weight sensors.

Wireless Remote Weather Station with micro:bit

May 11, 2020
Monitor the weather without being exposed to it through wireless communication between two micro:bits using the radio blocks! This is useful if your weather station is installed in a location that is difficult to retrieve data from the OpenLog. We will also explore a few different ways to send and receive data.

GPS Geo-Mapping at the Push of a Button

September 27, 2019
Let's ramp up our GPS tracking skills with KML files and Google Earth. We'll make a tracker that logs location and allows us to visualize our steps with Google Earth.

SparkFun gator:log Hookup Guide

September 5, 2019
The gator:log is a serial communication based data logger. This tutorial will get you started using the gator:log with the micro:bit platform.

SparkFun gator:RTC Hookup Guide

September 5, 2019
The gator:RTC is an I2C based, real-time clock (RTC) for keeping time while your micro:bit isn't powered. This tutorial will get you started using the gator:RTC with the micro:bit platform.

Qwiic OpenLog Hookup Guide

February 7, 2019
The updated Qwiic version of the OpenLog Hookup Guide

Spectral Triad (AS7265x) Hookup Guide

November 8, 2018
Learn how to wield the power of 18 channels of UV to NIR spectroscopy with AS72651 (UV), AS72652 (VIS), and AS72653 (NIR) sensors!

Python GUI Guide: Introduction to Tkinter

August 13, 2018
Tkinter is the standard graphical user interface package that comes with Python. This tutorial will show you how to create basic windowed applications as well as complete full-screen dashboard examples complete with live graph updates from matplotlib.

Graph Sensor Data with Python and Matplotlib

July 23, 2018
Use matplotlib to create a real-time plot of temperature data collected from a TMP102 sensor connected to a Raspberry Pi.

Python Programming Tutorial: Getting Started with the Raspberry Pi

June 27, 2018
This guide will show you how to write programs on your Raspberry Pi using Python to control hardware.

Raspberry Pi Zero Helmet Impact Force Monitor

March 8, 2018
How much impact can the human body handle? This tutorial will teach you how to build your very own impact force monitor using a helmet, Raspberry Pi Zero, and accelerometer!

Reading and Writing Serial EEPROMs

August 11, 2017
EEPROM is a great way to add extra memory to your microcontroller project. Wait 'til you see how easy it is to use!

micro:climate Kit Experiment Guide

July 21, 2017
A weather station kit that is built on top of the inexpensive, easy-to-use micro:bit and Microsoft MakeCode.

Mini GPS Shield Hookup Guide

December 15, 2016
A hookup guide for the SparkFun Mini GPS Shield.

Logging Data to Google Sheets with the Tessel 2

December 12, 2016
This project covers how to log data to Google Sheets two ways: using IFTTT with a web connection or a USB pen drive and "sneakernet" without.

9DoF Razor IMU M0 Hookup Guide

December 1, 2016
How to use and re-program the 9DoF Razor IMU M0, a combination of ATSAMD21 ARM Cortex-M0 microprocessor and MPU-9250 9DoF-in-a-chip.

Internet of Things Experiment Guide

November 23, 2016
The SparkFun ESP8266 Thing Dev Board is a powerful development platform that lets you connect your hardware projects to the Internet. In this guide, we show you how to combine some simple components to remotely log temperature data, send yourself texts and control lights from afar.

Hazardous Gas Monitor

June 17, 2016
Build a portable gas monitor to check for dangerous levels of hazardous gases.

Photon Remote Water Level Sensor

June 2, 2016
Learn how to build a remote water level sensor for a water storage tank and how to automate a pump based off the readings!

OpenLog Hookup Guide

April 7, 2016
An introduction to working with the OpenLog data logger.

Blynk Board Project Guide

March 25, 2016
A series of Blynk projects you can set up on the Blynk Board without ever re-programming it.

MicroSD Breakout With Level Shifter Hookup Guide

February 25, 2016
How to use the level translating µSD device.

GPS Logger Shield Hookup Guide

February 11, 2016
How to assemble and hookup the SparkFun GPS Logger Shield. Never lose track of your Arduino again!

SparkFun BME280 Breakout Hookup Guide

October 22, 2015
A guide for connecting the BME280 sensor to a microcontroller, and for using the SparkFun Arduino library.

MicroSD Shield and SD Breakout Hookup Guide

March 25, 2015
Adding external storage in the form of an SD or microSD card can be a great addition to any project. Learn how in this hookup guide for the microSD shield and SD breakout boards.

Logomatic Hookup Guide

May 29, 2014
Basic introduction and hook-up guide for the SparkFun Logomatic.

Vernier Shield Hookup Guide

February 14, 2014
A guide to using the Vernier Shield