Tutorials
AST-CAN485 WiFi Shield Hookup Guide
Hookup Guide for the AST-CAN485 WiFi Shield.
Qwiic OpenLog Hookup Guide
The updated Qwiic version of the OpenLog Hookup Guide
Computer Vision and Projection Mapping in Python
Use computer vision to detect faces and project images on top of them.
Adding More SERCOM Ports for SAMD Boards
How to setup extra SPI, UART, and I2C serial ports on a SAMD-based boards.
SparkFun gator:bit v2 Hookup Guide
The gator:bit v2 is a breakout board for the BBC micro:bit. The gator:bit exposes almost every pin on the micro:bit to clippable pad with circuit protection. It also has as built-in addressable LEDs and a built-in buzzer.
Motion Controlled Wearable LED Dance Harness
Control LEDs based on your movement using an accelerometer! Make your LEDs breathe by fading in and out when laying on the floor, turn off the LEDs when moving to your side, or make the LEDs blink in a headstand!
LuMini 8x8 Matrix Hookup Guide
The LuMini 8x8 Matrix (APA102-2020) are the highest resolution LED matrix available.
RedBoard Turbo Hookup Guide
An introduction to the RedBoard Turbo. Level up your Arduino-skills with the powerful SAMD21 ARM Cortex M0+ processor!
Qwiic MP3 Trigger Hookup Guide
Playing MP3s has never been easier.
Wireless Remote Control with micro:bit
In this tutorial, we will utilize the MakeCode radio blocks to have the one micro:bit transmit a signal to a receiving micro:bit on the same channel. Eventually, we will control a micro:bot wirelessly using parts from the arcade:kit!
LumiDrive Hookup Guide
The LumiDrive LED Driver is SparkFun’s foray into all things Python on micro-controllers. With the SparkFun LumiDrive you will be able to control and personalize a whole strand of APA102s directly from the board itself.
LuMini Ring Hookup Guide
The LuMini Rings (APA102-2020) are the highest resolution LED rings available.
LilyPad Vibe Board Hookup Guide
The LilyPad Vibe Board is a small vibration motor that can be sewn into projects with conductive thread and controlled by a LilyPad Arduino. The board can be used as a physical indicator on clothing and costumes for haptic feedback.
GPS-RTK2 Hookup Guide
Get precision down to the diameter of a dime with the new ZED-F9P from u-blox.
RedBoard Qwiic Hookup Guide
This tutorial covers the basic functionality of the RedBoard Qwiic. This tutorial also covers how to get started blinking an LED and using the Qwiic system.
Qwiic Single Relay Hookup Guide
Get started switching those higher power loads around with the Qwiic Single Relay.
Qwiic Quad Relay Hookup Guide
SparkFun’s Qwiic Quad Relay is a product designed for switching not one but four high powered devices from your Arduino or other low powered microcontroller using I2C.
Three Quick Tips About Using U.FL
Quick tips regarding how to connect, protect, and disconnect U.FL connectors.
Qwiic UV Sensor (VEML6075) Hookup Guide
Learn how to connect your VEML6075 UV Sensor and figure out just when you should put some sunscreen on.
SparkFun Serial Basic CH340C Hookup Guide
SparkFun Serial Basic Breakout takes advantage of USB-C and is an easy-to-use USB-to-Serial adapter based on the CH340C IC from WCH. With USB-C you can get up to three times the power delivery over the previous USB generation and has the convenient feature of being reversable.
Qwiic Twist Hookup Guide
Take your volume knob beyond 11 with the Qwiic Twist digital RGB LED encoder via I2C!
LS20031 5Hz (66 Channel) GPS Receiver Hookup Guide
In this tutorial, we will solder headers to the surface mount pads of the LS20031 GPS receiver and read the output using an Arduino!
Processor Interrupts with Arduino
What is an interrupt? In a nutshell, there is a method by which a processor can execute its normal program while continuously monitoring for some kind of event, or interrupt. There are two types of interrupts: hardware and software interrupts. For the purposes of this tutorial, we will focus on hardware interrupts.
Efficient Arduino Programming with Arduino CLI and Visual Studio Code
How to eschew the Arduino IDE for a combination of and Arduino command-line tool (Arduino CLI) and a professional code editor (Visual Studio Code).