Tutorials
Qwiic Ambient Light Sensor (VEML6030) Hookup Guide
The VEML6030 is a high accuracy ambient light sensor with 16-bit resolution. This I2C sensor can detect light similar to the human eye response. Start detecting light levels in your environment!
LilyPad RGB LED Hookup Guide
Learn how to hook up the LilyPad RGB LED and use a common cathode RGB LED in e-textile projects.
EL Wire Pants
In this tutorial, we will sew standard electroluminescent (EL) wire to a pair of pants.
Pi Servo pHAT (v2) Hookup Guide
This hookup guide will get you started with connecting and using the Pi Servo pHAT on a Raspberry Pi.
SparkFun 9DoF IMU (ICM-20948) Breakout Hookup Guide
How to use the SparkFun 9DoF ICM-20948 breakout board for your motion sensing projects. This breakout is ideal for wearable sensors and IoT applications.
Artemis Development with Arduino
Get our powerful Artemis based boards (Artemis Nano, BlackBoard Artemis, and BlackBoard Artemis ATP) blinking in less than 5 minutes using the SparkFun Artemis Arduino Core!
Designing with the SparkFun Artemis
Let's chat about layout and design considerations when using the Artemis module.
SparkFun gator:environment Hookup Guide
The gator:environment combines two I2C sensors for temperature, humidity, pressure, eCO2, and eTVOC values. This tutorial will get you started using the gator:environment with the micro:bit platform.
SparkFun gator:particle Hookup Guide
The gator:particle is an I2C heart-rate monitor and pulse oximeter that can be used as a particle sensor. This tutorial will get you started using the gator:particle with the micro:bit platform.
SparkFun gator:soil Hookup Guide
The gator:soil is analog soil moisture sensor. This tutorial will get you started using the gator:soil with the micro:bit platform.
SparkFun gator:microphone Hookup Guide
The gator:microphone is an I2C sensor for detecting sound with an electret microphone. This tutorial will get you started using the gator:microphone with the micro:bit platform.
TPL5110 Nano Power Timer Hookup Guide
The TPL5110 Nano Power Timer is ideal for applications that require low power, and especially those projects that are running off of a LiPo battery. The Nano Power Timer will turn on your project after the set amount of time, continuously.
LiPo Charger Plus Hookup Guide
This tutorial shows you how to hook up and use the SparkFun LiPo Charger Plus board.
Capacitive Touch Slider (CAP1203) Hookup Guide
An easy and Qwiic way to add capacitive touch to any of your projects using the CAP1203! In this guide, we go over how to connect and set up your Capacitive Touch Slider so you can start playing with it right away.
Basic Character LCD Hookup Guide
Liquid crystal displays (LCDs) are a great way to output a string of words or sensor data to a display for visual feedback. In this tutorial, we'll learn about LCDs, how to print a string of words to a 16x2 basic character LCD and create custom characters.
SAMD51 Thing Plus Hookup Guide
This tutorial covers the basic functionality of the SAMD51 Thing Plus and highlights the features of the new ARM Cortex-M4F development board.
ARM Programming
How to program SAMD21 or SAMD51 boards (or other ARM processors).
Qwiic 12-Bit ADC Hookup Guide
Need to add more analog inputs for your project? Check out the Qwiic 12-bit ADC.
Qwiic pHAT for Raspberry Pi Hookup Guide
Get started interfacing your Qwiic enabled boards with your Raspberry Pi. The Qwiic pHAT connects the I2C bus (GND, 3.3V, SDA, and SCL) on your Raspberry Pi to an array of Qwiic connectors.
Buck-Boost Hookup Guide
This tutorial shows you how to hook up and use the SparkFun Buck-Boost board.
Using Home Assistant to Expand Your Home Automations
An introduction to Home Assistant, an open source home automation hub.
Displaying Your Coordinates with a GPS Module
This Arduino tutorial will teach you how to pinpoint and display your GPS coordinates with a press of a button using hardware from our Qwiic Connect System (I2C).
Keyboard Shortcut, Qwiic Keypad
A simple project using the Qwiic Keypad and the RedBoard Turbo to create your own custom hotkey-pad.
Qwiic Keypad Hookup Guide
If you are tired of taking up GPIO pins, wiring a bunch of pull up resistors, and using firmware that scans the keys taking up valuable processing time... check out the new Qwiic Keypad.