Tutorials
Cryptographic Co-Processor ATECC508A (Qwiic) Hookup Guide
Learn how to use some of the standard features of the SparkFun Cryptographic Co-processor.
ATX Power Connector (4-Pin) Breakout Hookup Guide
Do you need to power a project with 12V and 5V from one wall adapter? The ATX power connector breaks out the standard 4-pin computer peripheral port for your 12V and 5V devices!
APA102 Addressable LED Hookup Guide
Connect, power, and control your APA102 addressable LED strip!
Fuse Breakout Board Hookup Guide
Protect your project by adding a fuse in your circuit to save it from molten destruction.
GPS Geo-Mapping at the Push of a Button
Let's ramp up our GPS tracking skills with KML files and Google Earth. We'll make a tracker that logs location and allows us to visualize our steps with Google Earth.
SparkFun Edge Hookup Guide
Get to know your Edge board, including both the hardware features for you to utilize as well as how to get talking to it.
Getting Started with the A111 Pulsed Radar Sensor
Get started with the Acconeer A111 SDK with a Raspberry Pi! The tiny A111 pulsed coherent radar (PCR) adds high-precision, cutting-edge distance measurement for speed-, material-, motion-, or gesture-sensing projects! We’re not talking about simple ultrasonic, or even infrared sensors here, but 60GHz radar!
Hookup Guide for the Qwiic Motor Driver
Drive things "qwiic"-ly with the SparkFun Qwiic Motor Driver!
Hookup Guide for the SparkFun Artemis Thing Plus
Get started with our SparkFun Artemis Thing Plus - our popular Thing Plus footprint with the powerful Artemis module for ultimate functionality.
SparkFun Pulse Oximeter and Heart Rate Monitor Hookup Guide
Find out your oxygen saturation level or check out your heart rate using the MAX30101 biometric sensor and MAX32664 Biometric Hub via I2C!
ESP32 Relay Web Server
The goal of this project is to have a website hosted on an ESP32 that controls any relay controlled device connected to a local network and keeps a dynamically updated state of those devices.
SparkFun gator:UV Hookup Guide
The gator:UV is an I2C based UV sensor. This tutorial will get you started using the gator:UV with the micro:bit platform.
SparkFun gator:RTC Hookup Guide
The gator:RTC is an I2C based, real-time clock (RTC) for keeping time while your micro:bit isn't powered. This tutorial will get you started using the gator:RTC with the micro:bit platform.
SparkFun gator:log Hookup Guide
The gator:log is a serial communication based data logger. This tutorial will get you started using the gator:log with the micro:bit platform.
Hookup Guide for the SparkFun RedBoard Artemis ATP
Get started with the RedBoard Artemis ATP - all the functionality of the SparkFun Artemis module wrapped in the Mega Arduino Footprint
Hookup Guide for the SparkFun RedBoard Artemis
Get started with the RedBoard Artemis - all the functionality of the SparkFun Artemis module wrapped in the familiar Uno R3 footprint
Hookup Guide for the SparkFun RedBoard Artemis Nano
Get started with the powerful RedBoard Artemis Nano
XBee3 Thing Plus Hookup Guide
Get started with SparkFun's XBee3 Thing Plus - both the u.FL as well as the PCB antenna versions.
Qwiic Atmospheric Sensor (BME280) Hookup Guide
Measure temperature, humidity, barometric pressure with the SparkFun Atmospheric Sensor Breakout BME280 (Qwiic).
SparkFun Inventor's Kit Experiment Guide - v4.1
The SparkFun Inventor's Kit (SIK) Experiment Guide contains all of the information needed to build all five projects, encompassing 16 circuits, in the latest version of the kit, v4.1.2 and v4.1.
How to Install CH340 Drivers
How to install CH340 drivers (if you need them) on Windows, Mac OS X, and Linux.
SparkFun AS3935 Lightning Detector Hookup Guide (v20)
Are you worried about the looming clouds in the distance, how far away is that storm exactly? Add lightning detection with the AS3935 to your next weather station or your next bike ride!
PCA9306 Logic Level Translator Hookup Guide (v2)
A quick primer to get you going with the PCA9306 Logic Level Converter - a dedicated I2C translator.
Qwiic Ambient Light Sensor (VEML6030) Hookup Guide
The VEML6030 is a high accuracy ambient light sensor with 16-bit resolution. This I2C sensor can detect light similar to the human eye response. Start detecting light levels in your environment!