Tutorials
Qwiic Differential I2C Bus Extender (PCA9615) Hookup Guide
Learn how to extend the range of your I2C communication bus with the Qwiic differential I2C bus extender (PCA9615 ) breakout board.
Qwiic Real Time Clock Module (RV-1805) Hookup Guide
Find out what time it is, even after the power's been out on your project for a while with the Qwiic Real Time Clock (RTC) module.
Flexible Grayscale OLED Hookup Guide
Figure out how to get images displaying on your new flexible OLED screen.
PIC-Based Serial Enabled Character LCD Hookup Guide
The PIC-based serial enabled character LCD backpack is a simple and cost effective solution for interfacing to character Liquid Crystal Displays (LCDs) based on the HD44780 controller. The backpack simplifies the number of wires needed and allows your project to display all kinds of text and numbers.
Variable Load Hookup Guide - Revised
This tutorial will show you how to assemble and use SparkFun's Variable Load board. It can be used to test stability of the power supply under various loads, battery lifetime, safety cutoffs, and other design elements of power supplies under test.
Adapting LilyPad Development Board Projects to the LilyPad ProtoSnap Plus
An overview of the updates made in the redesign of the LilyPad Development Board to the LilyPad ProtoSnap Plus and how to adapt code written for the old board to the new one.
IoT Power Relay
Using the ESP32 to make a web-configured timed relay.
SparkFun Arduino ProtoShield Hookup Guide
The SparkFun Arduino ProtoShield PCB and ProtoShield kit lets you customize your own Arduino shield using whatever custom circuit you can come up with! This tutorial will go over its features, hardware assembly, and how to use the shield with an Arduino R3 footprint.
LIDAR-Lite v3 Hookup Guide
A tutorial for connecting the Garmin LIDAR-Lite v3 or the LIDAR-Lite v3HP to an Arduino to measure distance.
12V/5V Power Supply Hookup Guide
In this tutorial, we will replace the 12V/5V (2A) power supply's molex connector with two male barrel jacks adapters.
IoT Weight Logging Scale
This tutorial will show you how to make a scale that logs your weight to a custom website on the Internet. The principles can be extrapolated to any type of data.
micro:bit Educator Lab Pack Experiment Guide
A quickstart guide for the micro:bit educator lab pack.
Qwiic GRID-Eye Infrared Array (AMG88xx) Hookup Guide
The Panasonic GRID-Eye (AMG88xx) 8x8 thermopile array serves as a functional low-resolution infrared camera. This means you have a square array of 64 pixels each capable of independent temperature detection. It’s like having thermal camera (or Predator’s vision), just in really low resolution.
Qwiic Magnetometer (MLX90393) Hookup Guide
Figure out how magnetic fields are oriented, all without having to solder a thing.
WiFi Controlled Robot
This tutorial will show you how to make a robot that streams a webcam to a custom website that can be remotely controlled.
Getting Started with 3D Printing Using Tinkercad
Tinkercad is a great, easy-to-use online modeling software that can have you 3D printing quickly. This tutorial will walk you through designing a simple project enclosure.
Qwiic VR IMU (BNO080) Hookup Guide
Figure out how things are oriented with the robust 9 degrees of freedom (DOF) BNO080 IMU. Maybe even make your own virtual reality (VR) applications if you're feeling savvy.
Papa Soundie Audio Player Hookup Guide
Add sound effects to your project, prop or costume with Papa Soundie Audio Player.
Noisy Cricket Stereo Amplifier - 1.5W Hookup Guide
A hookup guide for the Noisy Cricket Stereo Amplifier - 1.5W.
Little Soundie Audio Player Hookup Guide
Add sound effects to your project, prop or costume with Little Soundie Audio Player.
Headless Raspberry Pi Setup
Configure a Raspberry Pi without a keyboard, mouse, or monitor.
Setting up a Raspberry Pi 3 as an Access Point
This guide will show you how to configure a Raspberry Pi as an access point and connect it to your local Ethernet network to share Internet to other WiFi devices.
LilyPad Tri-Color LED Hookup Guide
Learn how to hook up the LilyPad Tri-Color LED and use a common anode RGB LED in e-textile projects.
Interactive 3D Printed LED Diamond Prop
In this tutorial, we will learn about how to create an interactive theatrical prop for a performance by 3D printing a translucent diamond prop using a non-addressable RGB LED strip and AT42QT1011 capacitive touch sensing.