Projects
Need inspiration? Find it here! These tutorials feature special projects broken down into steps to illustrate how you can use various concepts, skills, and technologies to build awesome stuff.
MicroView Digital Compass
Build a portable digital compass using the SparkFun MicroView and the MAG3110 Magnetometer Breakout.
Sunrise Machine with the Tessel 2
Are you to sleepy to enjoy a sunrise on a brisk morning? Yeah...us too! No worries, with a Webcam, a Tessel 2 and a bit of code you can sleep in and catch the sunrise at your leisure with the Sunrise Machine.
Environmental Monitoring with the Tessel 2
Build an air-conditioner monitoring device to collect environment information and store it in the cloud.
ReconBot with the Tessel 2
Build a robot with the Tessel 2 that you can control from a browser on your phone or laptop.
IoT Industrial Scale
What does a baby elephant weigh? How much impact force does a jump have? Answer these questions and more by building your very own IoT industrial scale using the SparkFun OpenScale.
TB6612FNG Hookup Guide
Basic hookup guide for the TB6612FNG H-bridge motor driver to get your robot to start moving!
Proto Pedal Example: Analog Equalizer Project
Building a gyrator-based analog equalizer using the Proto Pedal.
Proto Pedal Example: Programmable Digital Pedal
Building a pedal around the Teensy 3.2 and Teensy Audio shield. Changing the effect in the pedal is as easy as uploading a new sketch!
Pokémon Go Patches with EL Panels
Add a cloth stencil over EL panels to create glowing logos and designs.
OpenScale Applications and Hookup Guide
OpenScale allows you to have a permanent scale for industrial and biological applications. Learn how to use the OpenScale board to read and configure load cells.
Electret Mic Breakout Board Hookup Guide
An introduction to working with the Electret Mic Breakout Board.
Hazardous Gas Monitor
Build a portable gas monitor to check for dangerous levels of hazardous gases.
Photon Remote Water Level Sensor
Learn how to build a remote water level sensor for a water storage tank and how to automate a pump based off the readings!
Interactive LED Music Visualizer
Use an Arduino and the SparkFun Sound Detector to create visualizations on Addressable RGB LED strips.
How to Build a Remote Kill Switch
Learn how to build a wireless controller to kill power when things go... sentient.
GPS Differential Vector Pointer
Use GPS to have two objects, a base and a target, point towards one another. This can be used to aim a directional antenna (or in the case of this project, a laser) from one object to the other object at a distance that is only limited by your ability to provide the base station with the target's GPS location.
Sparcade: Edison as a Web Server for Browser Games
Turn the Intel® Edison into an access point that serves a simple browser-based game. High scores from the game are displayed on a character LCD.
Measuring Internal Resistance of Batteries
Classroom STEM activity that has students build a battery from a lemon, measure the open and closed circuit voltages, and determine the battery's internal resistance.
SIK Keyboard Instrument
We can use the parts and concepts in the SparkFun Invetor's Kit to make a primitive keyboard instrument.
Paper Circuit Pin
This quick craft project shows you how to create a circuit using copper tape instead of wire to light up an LED and make a wearable piece of e-craft art.
Blynk Board Washer/Dryer Alarm
How to configure the Blynk Board and app to notify you when your washer or dryer is done shaking.
Boss Alarm
Build a Boss Alarm that alerts you of anyone walking into your office and automatically changes your computer screen.
Blynk Board Bridge Widget Demo
A Blynk project that demonstrates how to use the Bridge widget to get two (or more) Blynk Boards to communicate.
Blynk Board Project Guide
A series of Blynk projects you can set up on the Blynk Board without ever re-programming it.